WrapGeometryBuilder Class¶
-
class
NXOpen.Features.
WrapGeometryBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.WrapGeometry
builderTo create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateWrapGeometryBuilder()
Default values.
Property Value AddOffset.Value 0 (millimeters part), 0 (inches part) Associative 1 CloseGaps Sharp DistTol 2.54 IsInterpart 0 SplitOffset.Value 0 (millimeters part), 0 (inches part) New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
AddOffset | Returns the Additional offset. |
Associative | Returns or sets the Remove parms switch |
CloseGaps | Returns or sets the Method used to close the gaps after offset of the wrap |
DistTol | Returns or sets the Distance tolerance used to facet the solids. |
Geometry | Returns the geometry to be wrapped (solid, sheet, curve, point) |
IsInterpart | Returns or sets the Setting that determines if this feature have interpart references |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
PlanesList | Returns the Planes to split the geometry, tightens the wrap along this plane |
SplitOffset | Returns the Offset applied to both sides of the splitting planes. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
WrapGeometryBuilderCloseGapType Enumeration | Represents the close gap type |
Property Detail¶
AddOffset¶
-
WrapGeometryBuilder.
AddOffset
¶ Returns the Additional offset.
Will expand the wrap.
-------------------------------------
Getter Method
Signature
AddOffset
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
Associative¶
-
WrapGeometryBuilder.
Associative
¶ Returns or sets the Remove parms switch
-------------------------------------
Getter Method
Signature
Associative
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Associative
Parameters: associative (bool) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
CloseGaps¶
-
WrapGeometryBuilder.
CloseGaps
¶ Returns or sets the Method used to close the gaps after offset of the wrap
-------------------------------------
Getter Method
Signature
CloseGaps
Returns: Return type: NXOpen.Features.WrapGeometryBuilderCloseGapType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CloseGaps
Parameters: closeGaps ( NXOpen.Features.WrapGeometryBuilderCloseGapType
) –New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
DistTol¶
-
WrapGeometryBuilder.
DistTol
¶ Returns or sets the Distance tolerance used to facet the solids.
Also used for default offset calculation.
-------------------------------------
Getter Method
Signature
DistTol
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DistTol
Parameters: distTol (float) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Geometry¶
-
WrapGeometryBuilder.
Geometry
¶ Returns the geometry to be wrapped (solid, sheet, curve, point)
-------------------------------------
Getter Method
Signature
Geometry
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX6.0.0.
License requirements: None.
IsInterpart¶
-
WrapGeometryBuilder.
IsInterpart
¶ Returns or sets the Setting that determines if this feature have interpart references
-------------------------------------
Getter Method
Signature
IsInterpart
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsInterpart
Parameters: isInterpart (bool) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
PlanesList¶
-
WrapGeometryBuilder.
PlanesList
¶ Returns the Planes to split the geometry, tightens the wrap along this plane
-------------------------------------
Getter Method
Signature
PlanesList
Returns: Return type: NXOpen.PlaneList
New in version NX6.0.0.
License requirements: None.
SplitOffset¶
-
WrapGeometryBuilder.
SplitOffset
¶ Returns the Offset applied to both sides of the splitting planes.
-------------------------------------
Getter Method
Signature
SplitOffset
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
WrapGeometryBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.