WrapGeometryBuilderCloseGapType Enumeration

NXOpen.Features.WrapGeometryBuilder.CloseGapType is an alias for NXOpen.Features.WrapGeometryBuilderCloseGapType

class NXOpen.Features.WrapGeometryBuilderCloseGapType

Bases: object

Represents the close gap type

Enum Members

Enum Member Enum Member Description
Sharp
Beveled
NoOffset
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.