WindshieldDatumBuilder Class¶
-
class
NXOpen.Features.VehicleDesign.
WindshieldDatumBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.VehicleDesign.WindshieldDatum
builder used to create or edit a Windshield Datum.To create a new instance of this class, use
NXOpen.Features.VehicleDesignCollection.CreateWindshieldDatumBuilder()
Default values.
Property Value AssoToggle 1 BottomAngle.Value 5 EyeType EyeFeature HorizontalAngle.Value 17 RayLength.Value 3000 (millimeters part), 0 (inches part) ShowPoints 1 ShowRays 1 TopAngle.Value 7 UseStandardLoading 1 VisionType Standard New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
AssoToggle | Returns or sets the associative option that determines whether to create feature or not. |
BottomAngle | Returns the bottom inclined angle. |
EyeFeature | Returns the eye feature; select eec feature when eye type specified. |
EyeType | Returns or sets the eye type to determine which type of v points to be used. |
HorizontalAngle | Returns the horizontal inclined angle. |
LoadingName | Returns or sets the name of the used loading in the Windshield Datum. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
PointV1 | Returns or sets the point v1; select one point when eye type specified. |
PointV2 | Returns or sets the point v2; select one point when eye type specified. |
RayLength | Returns the ray length. |
SelectWindshield | Returns the windshield collector which the v points will be projected onto. |
ShowPoints | Returns or sets the show points to determine whether to create points or not. |
ShowRays | Returns or sets the show rays to determine whether to create ray lines or not. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
TopAngle | Returns the top inclined angle. |
UseStandardLoading | Returns or sets the option that determines whether to use the loading specified by standard or not. |
VisionType | Returns or sets the vision type; standard or customer defined. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
WindshieldDatumBuilderCustomVisionAngle Enumeration | Represents the vision angle type to define the Windshield Datum. |
WindshieldDatumBuilderEnumEyeType Enumeration | Represents the eye definition type to define the Windshield Datum. |
Property Detail¶
AssoToggle¶
-
WindshieldDatumBuilder.
AssoToggle
¶ Returns or sets the associative option that determines whether to create feature or not.
-------------------------------------
Getter Method
Signature
AssoToggle
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AssoToggle
Parameters: assoToggle (bool) – New in version NX6.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
BottomAngle¶
-
WindshieldDatumBuilder.
BottomAngle
¶ Returns the bottom inclined angle.
-------------------------------------
Getter Method
Signature
BottomAngle
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
EyeFeature¶
-
WindshieldDatumBuilder.
EyeFeature
¶ Returns the eye feature; select eec feature when eye type specified.
-------------------------------------
Getter Method
Signature
EyeFeature
Returns: Return type: NXOpen.Features.SelectFeature
New in version NX6.0.0.
License requirements: None.
EyeType¶
-
WindshieldDatumBuilder.
EyeType
¶ Returns or sets the eye type to determine which type of v points to be used.
-------------------------------------
Getter Method
Signature
EyeType
Returns: Return type: NXOpen.Features.VehicleDesign.WindshieldDatumBuilderEnumEyeType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EyeType
Parameters: eyeType ( NXOpen.Features.VehicleDesign.WindshieldDatumBuilderEnumEyeType
) –New in version NX6.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
HorizontalAngle¶
-
WindshieldDatumBuilder.
HorizontalAngle
¶ Returns the horizontal inclined angle.
-------------------------------------
Getter Method
Signature
HorizontalAngle
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
LoadingName¶
-
WindshieldDatumBuilder.
LoadingName
¶ Returns or sets the name of the used loading in the Windshield Datum.
-------------------------------------
Getter Method
Signature
LoadingName
Returns: Return type: str New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LoadingName
Parameters: loadingName (str) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
PointV1¶
-
WindshieldDatumBuilder.
PointV1
¶ Returns or sets the point v1; select one point when eye type specified.
-------------------------------------
Getter Method
Signature
PointV1
Returns: Return type: NXOpen.Point
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointV1
Parameters: pointV1 ( NXOpen.Point
) –New in version NX6.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
PointV2¶
-
WindshieldDatumBuilder.
PointV2
¶ Returns or sets the point v2; select one point when eye type specified.
-------------------------------------
Getter Method
Signature
PointV2
Returns: Return type: NXOpen.Point
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointV2
Parameters: pointV2 ( NXOpen.Point
) –New in version NX6.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
RayLength¶
-
WindshieldDatumBuilder.
RayLength
¶ Returns the ray length.
-------------------------------------
Getter Method
Signature
RayLength
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
SelectWindshield¶
-
WindshieldDatumBuilder.
SelectWindshield
¶ Returns the windshield collector which the v points will be projected onto.
-------------------------------------
Getter Method
Signature
SelectWindshield
Returns: Return type: NXOpen.ScCollector
New in version NX6.0.0.
License requirements: None.
ShowPoints¶
-
WindshieldDatumBuilder.
ShowPoints
¶ Returns or sets the show points to determine whether to create points or not.
-------------------------------------
Getter Method
Signature
ShowPoints
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShowPoints
Parameters: showPoints (bool) – New in version NX6.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
ShowRays¶
-
WindshieldDatumBuilder.
ShowRays
¶ Returns or sets the show rays to determine whether to create ray lines or not.
-------------------------------------
Getter Method
Signature
ShowRays
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShowRays
Parameters: showRays (bool) – New in version NX6.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
TopAngle¶
-
WindshieldDatumBuilder.
TopAngle
¶ Returns the top inclined angle.
-------------------------------------
Getter Method
Signature
TopAngle
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
UseStandardLoading¶
-
WindshieldDatumBuilder.
UseStandardLoading
¶ Returns or sets the option that determines whether to use the loading specified by standard or not.
-------------------------------------
Getter Method
Signature
UseStandardLoading
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseStandardLoading
Parameters: useStandardLoading (bool) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
VisionType¶
-
WindshieldDatumBuilder.
VisionType
¶ Returns or sets the vision type; standard or customer defined.
-------------------------------------
Getter Method
Signature
VisionType
Returns: Return type: NXOpen.Features.VehicleDesign.WindshieldDatumBuilderCustomVisionAngle
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisionType
Parameters: visionType ( NXOpen.Features.VehicleDesign.WindshieldDatumBuilderCustomVisionAngle
) –New in version NX6.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Method Detail¶
Validate¶
-
WindshieldDatumBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.