HoodVisibilityBuilder Class¶
-
class
NXOpen.Features.VehicleDesign.
HoodVisibilityBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.VehicleDesign.HoodVisibility
builderTo create a new instance of this class, use
NXOpen.Features.VehicleDesignCollection.CreateHoodVisibilityBuilder()
Default values.
Property Value AssoToggle 0 PitchAngle 0 New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
AssoToggle | Returns or sets the associative toggle; toggle on to create feature |
EyePoint | Returns or sets the eye point |
FacetBodies | Returns the hood facet body |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
PitchAngle | Returns or sets the pitch angle which determines the quantity of section planes |
SelectFace | Returns the hood face |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AssoToggle¶
-
HoodVisibilityBuilder.
AssoToggle
¶ Returns or sets the associative toggle; toggle on to create feature
-------------------------------------
Getter Method
Signature
AssoToggle
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AssoToggle
Parameters: assoToggle (bool) – New in version NX6.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
EyePoint¶
-
HoodVisibilityBuilder.
EyePoint
¶ Returns or sets the eye point
-------------------------------------
Getter Method
Signature
EyePoint
Returns: Return type: NXOpen.Point
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EyePoint
Parameters: eyePoint ( NXOpen.Point
) –New in version NX6.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
FacetBodies¶
-
HoodVisibilityBuilder.
FacetBodies
¶ Returns the hood facet body
-------------------------------------
Getter Method
Signature
FacetBodies
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX11.0.0.
License requirements: None.
PitchAngle¶
-
HoodVisibilityBuilder.
PitchAngle
¶ Returns or sets the pitch angle which determines the quantity of section planes
-------------------------------------
Getter Method
Signature
PitchAngle
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PitchAngle
Parameters: pitchAngle (float) – New in version NX6.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
SelectFace¶
-
HoodVisibilityBuilder.
SelectFace
¶ Returns the hood face
-------------------------------------
Getter Method
Signature
SelectFace
Returns: Return type: NXOpen.ScCollector
New in version NX6.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
HoodVisibilityBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.