DynamicCurbBuilder Class¶
-
class
NXOpen.Features.VehicleDesign.
DynamicCurbBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.VehicleDesign.DynamicCurb
builderTo create a new instance of this class, use
NXOpen.Features.VehicleDesignCollection.CreateDynamicCurbBuilder()
Default values.
Property Value InnerLineType Horizontal Position Front RequirementsControl StandardDriven ShowClearance 0 Visualization Surface WheelSize StaticRadius New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
FrontInnerLength | Returns the expression defining the length of the inner line in front for dynamic curb. |
FrontInnerOffset | Returns the expression defining the value of inner offset in front for dynamic curb. |
FrontOuterOffset | Returns the expression defining the value of outer offset in front for dynamic curb. |
FrontSelector | Returns the faces representing the front car body geometry for the measurement. |
InnerLineType | Returns or sets the inner line type for dynamic curb. |
Loading | Returns or sets the loading used in the dynamic curb. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
Position | Returns or sets the dynamic curb position. |
RearInnerLength | Returns the expression defining the length of the inner line in rear for dynamic curb. |
RearInnerOffset | Returns the expression defining the value of inner offset in rear for dynamic curb. |
RearOuterOffset | Returns the expression defining the value of outer offset in rear for dynamic curb. |
RearSelector | Returns the faces representing the rear car body geometry for the measurement. |
RequirementsControl | Returns or sets the requirements control for standard driven or user defined. |
ShowClearance | Returns or sets the indication if the distance measurement will be shown. |
Standard | Returns or sets the standard used to define the dynamic curb. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Visualization | Returns or sets the visualization type of the dynamic curb output. |
WheelSize | Returns or sets the wheel size option which determines the size of the wheels in the dynamic curb. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
DynamicCurbBuilderMethodType Enumeration | Represents the type of inner line to create dynamic curb. |
DynamicCurbBuilderPositionType Enumeration | Represents the dynamic curb positions. |
DynamicCurbBuilderRequirementsControlType Enumeration | Represents the requirements control types to define the dynamic curb. |
DynamicCurbBuilderVisualizationType Enumeration | Represents the visualization types of the output. |
DynamicCurbBuilderWheelType Enumeration | Represents the type of the wheel size option for dynamic curb. |
Property Detail¶
FrontInnerLength¶
-
DynamicCurbBuilder.
FrontInnerLength
¶ Returns the expression defining the length of the inner line in front for dynamic curb.
-------------------------------------
Getter Method
Signature
FrontInnerLength
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
FrontInnerOffset¶
-
DynamicCurbBuilder.
FrontInnerOffset
¶ Returns the expression defining the value of inner offset in front for dynamic curb.
-------------------------------------
Getter Method
Signature
FrontInnerOffset
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
FrontOuterOffset¶
-
DynamicCurbBuilder.
FrontOuterOffset
¶ Returns the expression defining the value of outer offset in front for dynamic curb.
-------------------------------------
Getter Method
Signature
FrontOuterOffset
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
FrontSelector¶
-
DynamicCurbBuilder.
FrontSelector
¶ Returns the faces representing the front car body geometry for the measurement.
-------------------------------------
Getter Method
Signature
FrontSelector
Returns: Return type: NXOpen.ScCollector
New in version NX8.5.0.
License requirements: None.
InnerLineType¶
-
DynamicCurbBuilder.
InnerLineType
¶ Returns or sets the inner line type for dynamic curb.
-------------------------------------
Getter Method
Signature
InnerLineType
Returns: Return type: NXOpen.Features.VehicleDesign.DynamicCurbBuilderMethodType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InnerLineType
Parameters: innerLineType ( NXOpen.Features.VehicleDesign.DynamicCurbBuilderMethodType
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Loading¶
-
DynamicCurbBuilder.
Loading
¶ Returns or sets the loading used in the dynamic curb.
-------------------------------------
Getter Method
Signature
Loading
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Loading
Parameters: loading (str) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Position¶
-
DynamicCurbBuilder.
Position
¶ Returns or sets the dynamic curb position.
-------------------------------------
Getter Method
Signature
Position
Returns: Return type: NXOpen.Features.VehicleDesign.DynamicCurbBuilderPositionType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Position
Parameters: position ( NXOpen.Features.VehicleDesign.DynamicCurbBuilderPositionType
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
RearInnerLength¶
-
DynamicCurbBuilder.
RearInnerLength
¶ Returns the expression defining the length of the inner line in rear for dynamic curb.
-------------------------------------
Getter Method
Signature
RearInnerLength
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
RearInnerOffset¶
-
DynamicCurbBuilder.
RearInnerOffset
¶ Returns the expression defining the value of inner offset in rear for dynamic curb.
-------------------------------------
Getter Method
Signature
RearInnerOffset
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
RearOuterOffset¶
-
DynamicCurbBuilder.
RearOuterOffset
¶ Returns the expression defining the value of outer offset in rear for dynamic curb.
-------------------------------------
Getter Method
Signature
RearOuterOffset
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
RearSelector¶
-
DynamicCurbBuilder.
RearSelector
¶ Returns the faces representing the rear car body geometry for the measurement.
-------------------------------------
Getter Method
Signature
RearSelector
Returns: Return type: NXOpen.ScCollector
New in version NX8.5.0.
License requirements: None.
RequirementsControl¶
-
DynamicCurbBuilder.
RequirementsControl
¶ Returns or sets the requirements control for standard driven or user defined.
-------------------------------------
Getter Method
Signature
RequirementsControl
Returns: Return type: NXOpen.Features.VehicleDesign.DynamicCurbBuilderRequirementsControlType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RequirementsControl
Parameters: requirementsControl ( NXOpen.Features.VehicleDesign.DynamicCurbBuilderRequirementsControlType
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
ShowClearance¶
-
DynamicCurbBuilder.
ShowClearance
¶ Returns or sets the indication if the distance measurement will be shown.
-------------------------------------
Getter Method
Signature
ShowClearance
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShowClearance
Parameters: showClearance (bool) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Standard¶
-
DynamicCurbBuilder.
Standard
¶ Returns or sets the standard used to define the dynamic curb.
-------------------------------------
Getter Method
Signature
Standard
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Standard
Parameters: standard (str) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Visualization¶
-
DynamicCurbBuilder.
Visualization
¶ Returns or sets the visualization type of the dynamic curb output.
-------------------------------------
Getter Method
Signature
Visualization
Returns: Return type: NXOpen.Features.VehicleDesign.DynamicCurbBuilderVisualizationType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Visualization
Parameters: visualization ( NXOpen.Features.VehicleDesign.DynamicCurbBuilderVisualizationType
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
WheelSize¶
-
DynamicCurbBuilder.
WheelSize
¶ Returns or sets the wheel size option which determines the size of the wheels in the dynamic curb.
-------------------------------------
Getter Method
Signature
WheelSize
Returns: Return type: NXOpen.Features.VehicleDesign.DynamicCurbBuilderWheelType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
WheelSize
Parameters: wheelSize ( NXOpen.Features.VehicleDesign.DynamicCurbBuilderWheelType
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Method Detail¶
Validate¶
-
DynamicCurbBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.