UserDefinedFeatureCreateEvent Class¶
-
class
NXOpen.Features.
UserDefinedFeatureCreateEvent
¶ Bases:
NXOpen.TaggedObject
JA interface for the UserDefinedFeatureCreateEvent object
This calls cannot be created
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
ApplicationData | Returns the application data |
ClassName | Returns the class name |
CopiedFeature | Returns the feature in the destination part |
Definition | Returns the user defined feature definition |
OriginalFeature | Returns the original feature being copied |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
GetComponentFeatures | The component features that have been created so far |
GetExpressionData | The expressions of the instantiation feature |
GetReferenceData | The references of the instantiation feature |
Property Detail¶
ApplicationData¶
-
UserDefinedFeatureCreateEvent.
ApplicationData
¶ Returns the application data
-------------------------------------
Getter Method
Signature
ApplicationData
Returns: the application data Return type: NXOpen.Features.UserDefinedFeatureApplicationData
New in version NX8.0.0.
License requirements: None.
ClassName¶
-
UserDefinedFeatureCreateEvent.
ClassName
¶ Returns the class name
-------------------------------------
Getter Method
Signature
ClassName
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
CopiedFeature¶
-
UserDefinedFeatureCreateEvent.
CopiedFeature
¶ Returns the feature in the destination part
-------------------------------------
Getter Method
Signature
CopiedFeature
Returns: The feature being copied Return type: NXOpen.Features.Feature
New in version NX8.0.0.
License requirements: None.
Definition¶
-
UserDefinedFeatureCreateEvent.
Definition
¶ Returns the user defined feature definition
-------------------------------------
Getter Method
Signature
Definition
Returns: The UDF definition that is being created Return type: NXOpen.Features.Feature
New in version NX8.0.0.
License requirements: None.
OriginalFeature¶
-
UserDefinedFeatureCreateEvent.
OriginalFeature
¶ Returns the original feature being copied
-------------------------------------
Getter Method
Signature
OriginalFeature
Returns: The feature being copied Return type: NXOpen.Features.Feature
New in version NX8.0.0.
License requirements: None.
Method Detail¶
GetComponentFeatures¶
-
UserDefinedFeatureCreateEvent.
GetComponentFeatures
¶ The component features that have been created so far
Signature
GetComponentFeatures()
Returns: Return type: list of NXOpen.Features.Feature
New in version NX8.0.0.
License requirements: None.
GetExpressionData¶
-
UserDefinedFeatureCreateEvent.
GetExpressionData
¶ The expressions of the instantiation feature
Signature
GetExpressionData()
Returns: Return type: list of NXOpen.Features.UserDefinedFeatureExpressionData
New in version NX8.0.0.
License requirements: None.
GetReferenceData¶
-
UserDefinedFeatureCreateEvent.
GetReferenceData
¶ The references of the instantiation feature
Signature
GetReferenceData()
Returns: Return type: list of NXOpen.Features.UserDefinedFeatureReferenceData
New in version NX8.0.0.
License requirements: None.