UserDefinedFeatureExpressionData Class¶
-
class
NXOpen.Features.
UserDefinedFeatureExpressionData
¶ Bases:
NXOpen.TaggedObject
JA interface for UserDefinedFeatureExpressionData object.
Object of this class contain an expression of a user defined feature and the corresponding prompt. This calls cannot be created
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
Expression | Returns the expression of the user defined feature |
Prompt | Returns the prompt for the expression of the user defined feature |
Tag | Returns the Tag for this object. |
Methods¶
Property Detail¶
Expression¶
-
UserDefinedFeatureExpressionData.
Expression
¶ Returns the expression of the user defined feature
-------------------------------------
Getter Method
Signature
Expression
Returns: the expression of the user defined feature Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
Prompt¶
-
UserDefinedFeatureExpressionData.
Prompt
¶ Returns the prompt for the expression of the user defined feature
-------------------------------------
Getter Method
Signature
Prompt
Returns: the prompt for the expression of the user defined feature Return type: str New in version NX8.0.0.
License requirements: None.