TrimBodyBuilder Class¶
-
class
NXOpen.Features.
TrimBodyBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents the trim body feature builder.
This class is to be used only for editing pre-NX7.5.0 trim body features. Use
NXOpen.Features.TrimBody2Builder
to create and edit trim body features. To create a new instance of this class, useNXOpen.Features.FeatureCollection.CreateTrimBodyBuilder()
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Tool | Returns or sets the tool of the trim body feature |
TrimDirection | Returns or sets the trim direction of the trim body feature |
Methods¶
Method | Description |
---|---|
AddTarget | Adds a target body during create. |
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
GetTargets | Returns the target bodies of the trim body operation. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
RemoveTarget | Removes a target body is removed from trim body in create. |
Reverse | Reverse the trim direction of trim body feature |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
SetTargets | Sets the targets for a trim body opearation. |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
TrimBodyBuilderDirectionType Enumeration | Represents the trim direction |
Property Detail¶
Tool¶
-
TrimBodyBuilder.
Tool
¶ Returns or sets the tool of the trim body feature
-------------------------------------
Getter Method
Signature
Tool
Returns: Return type: NXOpen.NXObject
New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Tool
Parameters: tool ( NXOpen.NXObject
) – Set trim body toolNew in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
TrimDirection¶
-
TrimBodyBuilder.
TrimDirection
¶ Returns or sets the trim direction of the trim body feature
-------------------------------------
Getter Method
Signature
TrimDirection
Returns: Return type: NXOpen.Features.TrimBodyBuilderDirectionType
New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TrimDirection
Parameters: direction ( NXOpen.Features.TrimBodyBuilderDirectionType
) – Set trim directionNew in version NX4.0.0.
License requirements: None.
Method Detail¶
AddTarget¶
-
TrimBodyBuilder.
AddTarget
¶ Adds a target body during create.
A new target will be added to the * trim body operation. During edit, an exception will be thrown as * the target can not be modified during edit.
Signature
AddTarget(target)
Parameters: target ( NXOpen.Body
) – Body to addNew in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
GetTargets¶
-
TrimBodyBuilder.
GetTargets
¶ Returns the target bodies of the trim body operation.
Signature
GetTargets()
Returns: Target bodies Return type: list of NXOpen.Body
New in version NX4.0.0.
License requirements: None.
RemoveTarget¶
-
TrimBodyBuilder.
RemoveTarget
¶ Removes a target body is removed from trim body in create.
- During edit, an exception will be thrown as
- target body can not be changed during edit.
Signature
RemoveTarget(target)
Parameters: target ( NXOpen.Body
) – Body to removeNew in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Reverse¶
-
TrimBodyBuilder.
Reverse
¶ Reverse the trim direction of trim body feature
Signature
Reverse()
New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SetTargets¶
-
TrimBodyBuilder.
SetTargets
¶ Sets the targets for a trim body opearation.
Any existing targets will * be erased. For create multiple target bodies can be set. * This method will throw an exception during edit operation as the bodies * can not be changed at that point.
Signature
SetTargets(target)
Parameters: target (list of NXOpen.Body
) – target bodiesNew in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Validate¶
-
TrimBodyBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.