StartSymmetricModelingBuilder Class¶
-
class
NXOpen.Features.Subdivision.
StartSymmetricModelingBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Features.Subdivision.StartSymmetricModelingBuilder
builderTo create a new instance of this class, use
NXOpen.Features.Subdivision.SubdivisionBodyCollection.CreateStartSymmetricModelingBuilder()
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
EdgesToProject | Returns the edges to project |
MirrorProcedureOptions | Returns or sets the mirror procedure options |
Plane | Returns or sets the plane |
SwitchSide | Returns or sets the flag indicating if the mirror side should be switched |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
StartSymmetricModelingBuilderMirrorProcedureOption Enumeration | The options used to establish symmetric model |
Property Detail¶
EdgesToProject¶
-
StartSymmetricModelingBuilder.
EdgesToProject
¶ Returns the edges to project
-------------------------------------
Getter Method
Signature
EdgesToProject
Returns: Return type: NXOpen.Features.Subdivision.SelectCageObjectData
New in version NX9.0.0.
License requirements: None.
MirrorProcedureOptions¶
-
StartSymmetricModelingBuilder.
MirrorProcedureOptions
¶ Returns or sets the mirror procedure options
-------------------------------------
Getter Method
Signature
MirrorProcedureOptions
Returns: Return type: NXOpen.Features.Subdivision.StartSymmetricModelingBuilderMirrorProcedureOption
New in version NX9.0.0.
Deprecated since version NX10.0.0: This property is redundent and hence not necessary.
License requirements: None.
-------------------------------------
Setter Method
Signature
MirrorProcedureOptions
Parameters: mirrorProcedureOptions ( NXOpen.Features.Subdivision.StartSymmetricModelingBuilderMirrorProcedureOption
) –New in version NX9.0.0.
Deprecated since version NX10.0.0: This property is redundent and hence not necessary.
License requirements: nx_subdivision (” NX SUBDIVISION”)
Plane¶
-
StartSymmetricModelingBuilder.
Plane
¶ Returns or sets the plane
-------------------------------------
Getter Method
Signature
Plane
Returns: Return type: NXOpen.Plane
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Plane
Parameters: plane ( NXOpen.Plane
) –New in version NX9.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
SwitchSide¶
-
StartSymmetricModelingBuilder.
SwitchSide
¶ Returns or sets the flag indicating if the mirror side should be switched
-------------------------------------
Getter Method
Signature
SwitchSide
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SwitchSide
Parameters: switchSide (bool) – New in version NX9.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
Method Detail¶
Validate¶
-
StartSymmetricModelingBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.