SelectCageObjectData Class¶
-
class
NXOpen.Features.Subdivision.
SelectCageObjectData
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents subdivision cage topology object selection.
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
CanDeselectObjectsAutomatically | Returns or sets the flag indicating if previously selected objects can be de-selected during selection of new objects. |
SelectionList | Returns the object list. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
ClearAndAdd | Clears the currently present objects and adds new objects. |
SetCursorLocation | Sets the cursor location in absolute coordinates. |
SetViewDirection | Sets the view direction. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CanDeselectObjectsAutomatically¶
-
SelectCageObjectData.
CanDeselectObjectsAutomatically
¶ Returns or sets the flag indicating if previously selected objects can be de-selected during selection of new objects.
-------------------------------------
Getter Method
Signature
CanDeselectObjectsAutomatically
Returns: Return type: bool New in version NX9.0.0.
Deprecated since version NX11.0.0: There is no replacement for this unused property.
License requirements: None.
-------------------------------------
Setter Method
Signature
CanDeselectObjectsAutomatically
Parameters: canDeselect (bool) – New in version NX9.0.0.
Deprecated since version NX11.0.0: There is no replacement for this unused property.
License requirements: nx_subdivision (” NX SUBDIVISION”)
SelectionList¶
-
SelectCageObjectData.
SelectionList
¶ Returns the object list.
-------------------------------------
Getter Method
Signature
SelectionList
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX9.0.0.
License requirements: None.
Method Detail¶
ClearAndAdd¶
-
SelectCageObjectData.
ClearAndAdd
¶ Clears the currently present objects and adds new objects.
Signature
ClearAndAdd(objects, view, point)
Parameters: - objects (list of
NXOpen.NXObject
) – Objects to process. - view (
NXOpen.View
) – Selected object view when selecting a single object. - point (
NXOpen.Point3d
) – Selected object point when selecting a single object.
New in version NX9.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
- objects (list of
SetCursorLocation¶
-
SelectCageObjectData.
SetCursorLocation
¶ Sets the cursor location in absolute coordinates.
Signature
SetCursorLocation(point)
Parameters: point ( NXOpen.Point3d
) –New in version NX9.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
SetViewDirection¶
-
SelectCageObjectData.
SetViewDirection
¶ Sets the view direction.
Signature
SetViewDirection(direction)
Parameters: direction ( NXOpen.Vector3d
) –New in version NX9.0.1.
License requirements: nx_subdivision (” NX SUBDIVISION”)
Validate¶
-
SelectCageObjectData.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.