StartSymmetricModelingBuilderMirrorProcedureOption Enumeration¶
NXOpen.Features.Subdivision.StartSymmetricModelingBuilder.MirrorProcedureOption is an alias for NXOpen.Features.Subdivision.StartSymmetricModelingBuilderMirrorProcedureOption
-
class
NXOpen.Features.Subdivision.
StartSymmetricModelingBuilderMirrorProcedureOption
¶ Bases:
object
The options used to establish symmetric model
Deprecated since version NX10.0.0: This enumeration is redundent and hence not necessary.
Enum Members
Enum Member Enum Member Description CutBody Cuts the mesh ProjectEdge Projects the edges -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-