SplitBodyBuilder Class¶
-
class
NXOpen.Features.
SplitBodyBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.SplitBody
builder.Inputs to this class can be convergent objects.
To create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateSplitBodyBuilderUsingCollector()
Default values.
Property Value BooleanTool.ToolOption FaceOrPlane New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
BooleanTool | Returns the tool bodies to split the target body(s). |
KeepImprintedEdges | Returns or sets the keep imprinted edges option |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
TargetBody | Returns the target body to split. |
TargetBodyCollector | Returns or sets the collector of target bodies to split. |
Tolerance | Returns or sets the tolerance |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
BooleanTool¶
-
SplitBodyBuilder.
BooleanTool
¶ Returns the tool bodies to split the target body(s).
The tool bodies are * gotten through the BooleanTool Builder
-------------------------------------
Getter Method
Signature
BooleanTool
Returns: Return type: NXOpen.GeometricUtilities.BooleanToolBuilder
New in version NX6.0.0.
License requirements: None.
KeepImprintedEdges¶
-
SplitBodyBuilder.
KeepImprintedEdges
¶ Returns or sets the keep imprinted edges option
-------------------------------------
Getter Method
Signature
KeepImprintedEdges
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
KeepImprintedEdges
Parameters: keepImprintedEdges (bool) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
TargetBody¶
-
SplitBodyBuilder.
TargetBody
¶ Returns the target body to split.
It can be a single * solid/sheet body, or multiple solid/sheet bodies
-------------------------------------
Getter Method
Signature
TargetBody
Returns: Return type: NXOpen.SelectBodyList
New in version NX6.0.0.
License requirements: None.
TargetBodyCollector¶
-
SplitBodyBuilder.
TargetBodyCollector
¶ Returns or sets the collector of target bodies to split.
It can be a single * solid/sheet body, or multiple solid/sheet bodies
-------------------------------------
Getter Method
Signature
TargetBodyCollector
Returns: Return type: NXOpen.ScCollector
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TargetBodyCollector
Parameters: toolBodyCollector ( NXOpen.ScCollector
) –New in version NX7.5.0.
License requirements: None.
Tolerance¶
-
SplitBodyBuilder.
Tolerance
¶ Returns or sets the tolerance
-------------------------------------
Getter Method
Signature
Tolerance
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Tolerance
Parameters: tolerance (float) – New in version NX7.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
Validate¶
-
SplitBodyBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.