SphereBuilder Class¶
-
class
NXOpen.Features.
SphereBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.Sphere
builder.To create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateSphereBuilder()
Default values.
Property Value Diameter.Value 100 (millimeters part), 4 (inches part) New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Arc | Returns the selected arc associated with the Sphere. |
BooleanOption | Returns the boolean operation associated with the Sphere. |
CenterPoint | Returns or sets the center point of the Sphere. |
Diameter | Returns the diameter of the Sphere. |
ParentAssociativity | Returns or sets the option to keep associativity of the sphere center point |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Type | Returns or sets the sphere type represented by NXOpen.Features.SphereBuilderTypes |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SphereBuilderTypes Enumeration | Represents the sphere types. |
Property Detail¶
Arc¶
-
SphereBuilder.
Arc
¶ Returns the selected arc associated with the Sphere.
-------------------------------------
Getter Method
Signature
Arc
Returns: Return type: NXOpen.SelectICurve
New in version NX6.0.0.
License requirements: None.
BooleanOption¶
-
SphereBuilder.
BooleanOption
¶ Returns the boolean operation associated with the Sphere.
-------------------------------------
Getter Method
Signature
BooleanOption
Returns: Return type: NXOpen.GeometricUtilities.BooleanOperation
New in version NX6.0.0.
License requirements: None.
CenterPoint¶
-
SphereBuilder.
CenterPoint
¶ Returns or sets the center point of the Sphere.
-------------------------------------
Getter Method
Signature
CenterPoint
Returns: Return type: NXOpen.Point
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CenterPoint
Parameters: centerPoint ( NXOpen.Point
) –New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Diameter¶
-
SphereBuilder.
Diameter
¶ Returns the diameter of the Sphere.
-------------------------------------
Getter Method
Signature
Diameter
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
ParentAssociativity¶
-
SphereBuilder.
ParentAssociativity
¶ Returns or sets the option to keep associativity of the sphere center point
-------------------------------------
Getter Method
Signature
ParentAssociativity
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ParentAssociativity
Parameters: parentAssociativity (bool) – New in version NX8.0.0.
License requirements: features_modeling (“FEATURES MODELING”), solid_modeling (“SOLIDS MODELING”)
Type¶
-
SphereBuilder.
Type
¶ Returns or sets the sphere type represented by
NXOpen.Features.SphereBuilderTypes
-------------------------------------
Getter Method
Signature
Type
Returns: Return type: NXOpen.Features.SphereBuilderTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type
Parameters: type ( NXOpen.Features.SphereBuilderTypes
) –New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
Validate¶
-
SphereBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.