SphereBuilderTypes Enumeration¶
NXOpen.Features.SphereBuilder.Types is an alias for NXOpen.Features.SphereBuilderTypes
-
class
NXOpen.Features.
SphereBuilderTypes
¶ Bases:
object
Represents the sphere types.
Enum Members
Enum Member Enum Member Description CenterPointAndDiameter Represents the type of sphere created by providing center point and diameter. Arc Represents the type of sphere created by providing arc. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-