SteelInsulationBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
SteelInsulationBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a builder that is used to create or edit a
NXOpen.Features.ShipDesign.SteelInsulation
feature.The steel insulation feature creates a single solid body representing the insultion on the steel surfaces.
To create a new instance of this class, use
NXOpen.Features.ShipCollection.CreateSteelInsulationBuilder()
Default values.
Property Value Thickness.Value 25 (millimeters part), 1.0 (inches part) New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
BoundaryList | Returns the list of NXOpen.Features.ShipDesign.SteelInsulationBoundaryBuilder defining the insulation boundaries that need to be adjusted. |
DistanceTolerance | Returns or sets the modeling distance tolerance. |
EnableBoundaryAdjustment | Returns or sets the indication if the boundary adjustement is enabled. |
InsulateProfile | Returns or sets the indication if the profile attached to the plate should be insulated. |
InsulationHeight | Returns the expression containing the insulation height value for the profiles. |
MaterialType | Returns or sets the insulation material type. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SteelFaces | Returns the collection of faces to be insulated. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
ThickenDirection | Returns or sets the indication if the thicken direction of the insulation should be the same as the sewn face normal. |
Thickness | Returns the expression containing the insulation material thickness value. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
CreateSteelInsulationBoundary | Creates a NXOpen.Features.ShipDesign.SteelInsulationBoundaryBuilder builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
BoundaryList¶
-
SteelInsulationBuilder.
BoundaryList
¶ Returns the list of
NXOpen.Features.ShipDesign.SteelInsulationBoundaryBuilder
defining the insulation boundaries that need to be adjusted.-------------------------------------
Getter Method
Signature
BoundaryList
Returns: Return type: NXOpen.Features.ShipDesign.SteelInsulationBoundaryBuilderList
New in version NX8.0.0.
License requirements: None.
DistanceTolerance¶
-
SteelInsulationBuilder.
DistanceTolerance
¶ Returns or sets the modeling distance tolerance.
-------------------------------------
Getter Method
Signature
DistanceTolerance
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DistanceTolerance
Parameters: distanceTolerance (float) – New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
EnableBoundaryAdjustment¶
-
SteelInsulationBuilder.
EnableBoundaryAdjustment
¶ Returns or sets the indication if the boundary adjustement is enabled.
-------------------------------------
Getter Method
Signature
EnableBoundaryAdjustment
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EnableBoundaryAdjustment
Parameters: enableBoundaryAdjustment (bool) – New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
InsulateProfile¶
-
SteelInsulationBuilder.
InsulateProfile
¶ Returns or sets the indication if the profile attached to the plate should be insulated.
-------------------------------------
Getter Method
Signature
InsulateProfile
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InsulateProfile
Parameters: insulateProfile (bool) – New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
InsulationHeight¶
-
SteelInsulationBuilder.
InsulationHeight
¶ Returns the expression containing the insulation height value for the profiles.
-------------------------------------
Getter Method
Signature
InsulationHeight
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
MaterialType¶
-
SteelInsulationBuilder.
MaterialType
¶ Returns or sets the insulation material type.
The material information is defined in nxship_manufacturing_config.dat file.
-------------------------------------
Getter Method
Signature
MaterialType
Returns: Return type: int New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MaterialType
Parameters: materialType (int) – New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
SteelFaces¶
-
SteelInsulationBuilder.
SteelFaces
¶ Returns the collection of faces to be insulated.
During creation, each set of faces that can be sewn into a single sheet will form a new steel insulation feature. During edit, all the faces must be sewable to a single sheet body.
-------------------------------------
Getter Method
Signature
SteelFaces
Returns: Return type: NXOpen.ScCollector
New in version NX8.0.0.
License requirements: None.
ThickenDirection¶
-
SteelInsulationBuilder.
ThickenDirection
¶ Returns or sets the indication if the thicken direction of the insulation should be the same as the sewn face normal.
True indicates that the insulation will be thickened in the same direction as the sewn face normal.
-------------------------------------
Getter Method
Signature
ThickenDirection
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ThickenDirection
Parameters: thickenDirection (bool) – New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
Thickness¶
-
SteelInsulationBuilder.
Thickness
¶ Returns the expression containing the insulation material thickness value.
-------------------------------------
Getter Method
Signature
Thickness
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
Method Detail¶
CreateSteelInsulationBoundary¶
-
SteelInsulationBuilder.
CreateSteelInsulationBoundary
¶ Creates a
NXOpen.Features.ShipDesign.SteelInsulationBoundaryBuilder
builder.Signature
CreateSteelInsulationBoundary()
Returns: Return type: NXOpen.Features.ShipDesign.SteelInsulationBoundaryBuilder
New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
Validate¶
-
SteelInsulationBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.