ExcessMaterialBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
ExcessMaterialBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.ShipDesign.ExcessMaterial
builder.The Excess Material feature adds excess manufacturing material to the end of plate.
To create a new instance of this class, use
NXOpen.Features.ShipCollection.CreateExcessMaterialBuilder()
Default values.
Property Value EndOffset.Value 10 (millimeters part), 10 (inches part) ExtendEndFace 0 ExtendStartFace 0 OffsetDistance.Value (deprecated) 10 (millimeters part), 10 (inches part) OffsetType Constant StartOffset.Value 10 (millimeters part), 10 (inches part) New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
EndOffset | Returns the end offset (only applicable for excess material with variable offsets, fitup and constant offset excess material will ignore this value) |
ExtendEndFace | Returns or sets the extend end side face option (not applicable for fitup) |
ExtendStartFace | Returns or sets the extend start side face option (not applicable for fitup) |
OffsetDistance | Returns the offset distance |
OffsetType | Returns or sets the offset type (only applicable for excess material, fitup will ignore the offset type) |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SelectFace | Returns the selection face. |
SelectFaces | Returns the faces that need to have excess material. |
StartOffset | Returns the start offset (replaces the legacy offset distance property, and is used for both excess material and fitup) |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Type | Returns or sets the feature type (ie excess material or fitup) |
Version | Returns the version of the feature (used to determine which properties and methods are applicable) during edit. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ExcessMaterialBuilderOffset Enumeration | The offset type (only applicable for excess material, fitup will ignore the offset type) |
ExcessMaterialBuilderTypes Enumeration | The feature type |
ExcessMaterialBuilderVersionID Enumeration | version identifiers for the different revisions of the excess material feature. |
Property Detail¶
EndOffset¶
-
ExcessMaterialBuilder.
EndOffset
¶ Returns the end offset (only applicable for excess material with variable offsets, fitup and constant offset excess material will ignore this value)
-------------------------------------
Getter Method
Signature
EndOffset
Returns: Return type: NXOpen.Expression
New in version NX9.0.2.
License requirements: None.
ExtendEndFace¶
-
ExcessMaterialBuilder.
ExtendEndFace
¶ Returns or sets the extend end side face option (not applicable for fitup)
-------------------------------------
Getter Method
Signature
ExtendEndFace
Returns: Return type: bool New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
ExtendEndFace
Parameters: extendEndFace (bool) – New in version NX9.0.2.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_mfg_prep (“Ship Manufacturing”)
ExtendStartFace¶
-
ExcessMaterialBuilder.
ExtendStartFace
¶ Returns or sets the extend start side face option (not applicable for fitup)
-------------------------------------
Getter Method
Signature
ExtendStartFace
Returns: Return type: bool New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
ExtendStartFace
Parameters: extendStartFace (bool) – New in version NX9.0.2.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_mfg_prep (“Ship Manufacturing”)
OffsetDistance¶
-
ExcessMaterialBuilder.
OffsetDistance
¶ Returns the offset distance
-------------------------------------
Getter Method
Signature
OffsetDistance
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
Deprecated since version NX9.0.2: Use
NXOpen.Features.ShipDesign.ExcessMaterialBuilder.StartOffset()
instead.License requirements: None.
OffsetType¶
-
ExcessMaterialBuilder.
OffsetType
¶ Returns or sets the offset type (only applicable for excess material, fitup will ignore the offset type)
-------------------------------------
Getter Method
Signature
OffsetType
Returns: Return type: NXOpen.Features.ShipDesign.ExcessMaterialBuilderOffset
New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
OffsetType
Parameters: offsetType ( NXOpen.Features.ShipDesign.ExcessMaterialBuilderOffset
) –New in version NX9.0.2.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_mfg_prep (“Ship Manufacturing”)
SelectFace¶
-
ExcessMaterialBuilder.
SelectFace
¶ Returns the selection face.
The selected face will be offset by the specified distance.
-------------------------------------
Getter Method
Signature
SelectFace
Returns: Return type: NXOpen.SelectFace
New in version NX7.5.0.
Deprecated since version NX8.0.0: Use
NXOpen.Features.ShipDesign.ExcessMaterialBuilder.SelectFaces()
instead.License requirements: None.
SelectFaces¶
-
ExcessMaterialBuilder.
SelectFaces
¶ Returns the faces that need to have excess material.
-------------------------------------
Getter Method
Signature
SelectFaces
Returns: Return type: NXOpen.ScCollector
New in version NX8.0.0.
License requirements: None.
StartOffset¶
-
ExcessMaterialBuilder.
StartOffset
¶ Returns the start offset (replaces the legacy offset distance property, and is used for both excess material and fitup)
-------------------------------------
Getter Method
Signature
StartOffset
Returns: Return type: NXOpen.Expression
New in version NX9.0.2.
License requirements: None.
Type¶
-
ExcessMaterialBuilder.
Type
¶ Returns or sets the feature type (ie excess material or fitup)
-------------------------------------
Getter Method
Signature
Type
Returns: Return type: NXOpen.Features.ShipDesign.ExcessMaterialBuilderTypes
New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type
Parameters: type ( NXOpen.Features.ShipDesign.ExcessMaterialBuilderTypes
) –New in version NX9.0.2.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_mfg_prep (“Ship Manufacturing”)
Version¶
-
ExcessMaterialBuilder.
Version
¶ Returns the version of the feature (used to determine which properties and methods are applicable) during edit.
The version of new features during create will be NX902
-------------------------------------
Getter Method
Signature
Version
Returns: Return type: NXOpen.Features.ShipDesign.ExcessMaterialBuilderVersionID
New in version NX9.0.2.
License requirements: None.
Method Detail¶
Validate¶
-
ExcessMaterialBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.