DvToMvMappingBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
DvToMvMappingBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.ShipDesign.DvToMvMapping
builder.This builder is used to create ship version-up design view to manufacturing view mapping feature. The mapping feature is created during a special version-up process, and will be used to drive NX to propagate changes from design body to manufacturing body automatically.
To create a new instance of this class, use
NXOpen.Features.ShipCollection.CreateDvToMvMappingBuilder()
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
AdoptedDesignBody | Returns or sets the adopted design body. |
AdoptedMfgBody | Returns or sets the adopted manufacturing body. |
DesignFeatureGroup | Returns or sets the design feature group. |
MfgFeatureGroup | Returns or sets the mfg feature group. |
OriginalDesignBody | Returns or sets the original design body. |
OriginalMfgBody | Returns or sets the original manufacturing body. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AdoptedDesignBody¶
-
DvToMvMappingBuilder.
AdoptedDesignBody
¶ Returns or sets the adopted design body.
-------------------------------------
Getter Method
Signature
AdoptedDesignBody
Returns: Return type: NXOpen.Body
New in version NX8.5.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
-------------------------------------
Setter Method
Signature
AdoptedDesignBody
Parameters: adoptedDesignBody ( NXOpen.Body
) –New in version NX8.5.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
AdoptedMfgBody¶
-
DvToMvMappingBuilder.
AdoptedMfgBody
¶ Returns or sets the adopted manufacturing body.
-------------------------------------
Getter Method
Signature
AdoptedMfgBody
Returns: Return type: NXOpen.Body
New in version NX8.5.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
-------------------------------------
Setter Method
Signature
AdoptedMfgBody
Parameters: adoptedMfgBody ( NXOpen.Body
) –New in version NX8.5.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
DesignFeatureGroup¶
-
DvToMvMappingBuilder.
DesignFeatureGroup
¶ Returns or sets the design feature group.
-------------------------------------
Getter Method
Signature
DesignFeatureGroup
Returns: Return type: NXOpen.Features.Feature
New in version NX8.5.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
-------------------------------------
Setter Method
Signature
DesignFeatureGroup
Parameters: designFeatureGroup ( NXOpen.Features.Feature
) –New in version NX8.5.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
MfgFeatureGroup¶
-
DvToMvMappingBuilder.
MfgFeatureGroup
¶ Returns or sets the mfg feature group.
-------------------------------------
Getter Method
Signature
MfgFeatureGroup
Returns: Return type: NXOpen.Features.Feature
New in version NX8.5.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
-------------------------------------
Setter Method
Signature
MfgFeatureGroup
Parameters: mfgFeatureGroup ( NXOpen.Features.Feature
) –New in version NX8.5.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
OriginalDesignBody¶
-
DvToMvMappingBuilder.
OriginalDesignBody
¶ Returns or sets the original design body.
-------------------------------------
Getter Method
Signature
OriginalDesignBody
Returns: Return type: NXOpen.Body
New in version NX8.5.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
-------------------------------------
Setter Method
Signature
OriginalDesignBody
Parameters: originalDesignBody ( NXOpen.Body
) –New in version NX8.5.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
OriginalMfgBody¶
-
DvToMvMappingBuilder.
OriginalMfgBody
¶ Returns or sets the original manufacturing body.
-------------------------------------
Getter Method
Signature
OriginalMfgBody
Returns: Return type: NXOpen.Body
New in version NX8.5.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
-------------------------------------
Setter Method
Signature
OriginalMfgBody
Parameters: originalMfgBody ( NXOpen.Body
) –New in version NX8.5.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
Method Detail¶
Validate¶
-
DvToMvMappingBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.