CopyPasteNewBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
CopyPasteNewBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
,NXOpen.IAttributeSourceObjectBuilder
Represents a
NXOpen.Features.ShipDesign.CopyPasteNewBuilder
It is used in Ship Building Application.The operation copies one or more components and pastes them as new parts while re-parenting and maintaining WAVE links
To create a new instance of this class, use
NXOpen.Features.ShipCollection.CreateCopyPasteNewBuilder()
Default values.
Property Value AngularTolerance 5 CopySection false New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
AlgorithmVersion | Returns or sets the value of algorithm version is used to define the version information. |
AngularTolerance | Returns or sets the value of angular tolerance is used to define the angular difference from qualified candidate face / plane normal to source face / plane normal. |
ComponentsToCopy | Returns the components to copy |
CopyApproachOption | Returns or sets an option to determine the approach to copy the ship standard parts between planes. |
CopySection | Returns or sets the flag is used to define if linear tolerance on UI would be used when matching geometry. |
LinearTolerance | Returns or sets the value of linear tolerance is used to define the tolerance between candidate object and transformed source object. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SelectionFrom | Returns the From geometry |
SelectionTo | Returns the To geometry |
ShipNames | Returns the Ship Names builder, used to assign names to the copied objects created. |
ShowXmlReport | Returns or sets the flag to indicate whether or not to show the xml report on copy paste results |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
AutoAssignAttributes | Auto assigns the attributes for a given array of objects and returns an array of objects that failed to auto assign. |
AutoAssignAttributesWithNamingPattern | Auto assigns the attributes for a given object and returns an array of objects that failed to auto assign. |
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
CreateAttributeTitleToNamingPatternMap | Creates a map object of attribute titles to their corresponding naming pattern |
CreateLogicalObjects | Creates the pre-creation logical objects |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
GetOperationFailures | Gets the operation failure error list object |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
CopyPasteNewBuilderCopyApproach Enumeration | Represents the approach of copying ship standard parts. |
CopyPasteNewBuilderVersionID Enumeration | add version identifiers for the different revisions of the copy paste new feature. |
Property Detail¶
AlgorithmVersion¶
-
CopyPasteNewBuilder.
AlgorithmVersion
¶ Returns or sets the value of algorithm version is used to define the version information.
-------------------------------------
Getter Method
Signature
AlgorithmVersion
Returns: Return type: NXOpen.Features.ShipDesign.CopyPasteNewBuilderVersionID
New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AlgorithmVersion
Parameters: algorithmVersion ( NXOpen.Features.ShipDesign.CopyPasteNewBuilderVersionID
) –New in version NX12.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
AngularTolerance¶
-
CopyPasteNewBuilder.
AngularTolerance
¶ Returns or sets the value of angular tolerance is used to define the angular difference from qualified candidate face / plane normal to source face / plane normal.
-------------------------------------
Getter Method
Signature
AngularTolerance
Returns: Return type: float New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AngularTolerance
Parameters: tolerance (float) – New in version NX11.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
ComponentsToCopy¶
-
CopyPasteNewBuilder.
ComponentsToCopy
¶ Returns the components to copy
-------------------------------------
Getter Method
Signature
ComponentsToCopy
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
CopyApproachOption¶
-
CopyPasteNewBuilder.
CopyApproachOption
¶ Returns or sets an option to determine the approach to copy the ship standard parts between planes.
-------------------------------------
Getter Method
Signature
CopyApproachOption
Returns: Return type: NXOpen.Features.ShipDesign.CopyPasteNewBuilderCopyApproach
New in version NX11.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
CopyApproachOption
Parameters: copyApproachOption ( NXOpen.Features.ShipDesign.CopyPasteNewBuilderCopyApproach
) –New in version NX11.0.2.
License requirements: nx_ship_detail (“Ship Detail Design”)
CopySection¶
-
CopyPasteNewBuilder.
CopySection
¶ Returns or sets the flag is used to define if linear tolerance on UI would be used when matching geometry.
If false, the linear tolerance will be set with max double value as default.
-------------------------------------
Getter Method
Signature
CopySection
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CopySection
Parameters: copySection (bool) – New in version NX11.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
LinearTolerance¶
-
CopyPasteNewBuilder.
LinearTolerance
¶ Returns or sets the value of linear tolerance is used to define the tolerance between candidate object and transformed source object.
For example, the distance from the qualified candidate curve to the transformed sample points of source curve shoud be within linear tolerance. And for body, it checks the distance from the qualified body’s faces and the transformed sample points of source body’s corresponding faces.
-------------------------------------
Getter Method
Signature
LinearTolerance
Returns: Return type: float New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LinearTolerance
Parameters: tolerance (float) – New in version NX11.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
SelectionFrom¶
-
CopyPasteNewBuilder.
SelectionFrom
¶ Returns the From geometry
-------------------------------------
Getter Method
Signature
SelectionFrom
Returns: Return type: NXOpen.SelectNXObject
New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
SelectionTo¶
-
CopyPasteNewBuilder.
SelectionTo
¶ Returns the To geometry
-------------------------------------
Getter Method
Signature
SelectionTo
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
ShipNames¶
-
CopyPasteNewBuilder.
ShipNames
¶ Returns the Ship Names builder, used to assign names to the copied objects created.
-------------------------------------
Getter Method
Signature
ShipNames
Returns: Ship Names List Builder Return type: NXOpen.Features.ShipDesign.ShipNamesListBuilder
New in version NX10.0.0.
License requirements: None.
ShowXmlReport¶
-
CopyPasteNewBuilder.
ShowXmlReport
¶ Returns or sets the flag to indicate whether or not to show the xml report on copy paste results
-------------------------------------
Getter Method
Signature
ShowXmlReport
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShowXmlReport
Parameters: showXmlReport (bool) – New in version NX11.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
Method Detail¶
AutoAssignAttributes¶
-
CopyPasteNewBuilder.
AutoAssignAttributes
¶ Auto assigns the attributes for a given array of objects and returns an array of objects that failed to auto assign.
Signature
AutoAssignAttributes(objects)
Parameters: objects (list of NXOpen.NXObject
) –Returns: Return type: NXOpen.ErrorList
New in version NX8.5.0.
License requirements: None.
AutoAssignAttributesWithNamingPattern¶
-
CopyPasteNewBuilder.
AutoAssignAttributesWithNamingPattern
¶ Auto assigns the attributes for a given object and returns an array of objects that failed to auto assign.
properties needs to be created using
CreateAttributeTitleToNamingPatternMap()
Signature
AutoAssignAttributesWithNamingPattern(objects, properties)
Parameters: - objects (list of
NXOpen.NXObject
) – - properties (list of
NXOpen.NXObject
) –
Returns: Return type: New in version NX12.0.0.
License requirements: None.
- objects (list of
CreateAttributeTitleToNamingPatternMap¶
-
CopyPasteNewBuilder.
CreateAttributeTitleToNamingPatternMap
¶ Creates a map object of attribute titles to their corresponding naming pattern
Signature
CreateAttributeTitleToNamingPatternMap(attributeTitles, titlePatterns)
Parameters: - attributeTitles (list of str) –
- titlePatterns (list of str) –
Returns: Return type: New in version NX12.0.0.
License requirements: None.
CreateLogicalObjects¶
-
CopyPasteNewBuilder.
CreateLogicalObjects
¶ Creates the pre-creation logical objects
Signature
CreateLogicalObjects()
Returns: Return type: list of NXOpen.PDM.LogicalObject
New in version NX8.5.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
GetOperationFailures¶
-
CopyPasteNewBuilder.
GetOperationFailures
¶ Gets the operation failure error list object
Signature
GetOperationFailures()
Returns: List of errors encountered during the copy parts Return type: NXOpen.ErrorList
New in version NX10.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
Validate¶
-
CopyPasteNewBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.