ResizeBendRadiusBuilder Class¶
-
class
NXOpen.Features.SheetMetal.
ResizeBendRadiusBuilder
¶ Bases:
NXOpen.Features.SheetMetal.SheetmetalBaseBuilder
Represents a ResizeBendRadius feature builder.
To create a new instance of this class, use
NXOpen.Features.SheetMetal.SheetmetalManager.CreateResizeBendRadiusFeatureBuilder()
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
BendFaces | Returns the bend faces |
BendRadius | Returns the bend radius |
BendReliefDepth | Returns the bend relief depth. |
BendReliefType | Returns the relief type for the resize bend radius feature. |
BendReliefWidth | Returns the bend relief width. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
ReferenceEntity | Returns the non-thickness planar face or linear edge to remain fixed while bend is resized |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Type | Returns or sets the feature type |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetApplicationContext | Get the application context. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetApplicationContext | Set the application context. |
SetBendReliefType | |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ResizeBendRadiusBuilderBendReliefTypeOptions Enumeration | This enum represents the bend relief type. |
ResizeBendRadiusBuilderTypes Enumeration | This enum represents the feature types. |
Property Detail¶
BendFaces¶
-
ResizeBendRadiusBuilder.
BendFaces
¶ Returns the bend faces
-------------------------------------
Getter Method
Signature
BendFaces
Returns: The Bend Face Collection Return type: NXOpen.ScCollector
New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
BendRadius¶
-
ResizeBendRadiusBuilder.
BendRadius
¶ Returns the bend radius
-------------------------------------
Getter Method
Signature
BendRadius
Returns: The Bend Radius Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
BendReliefDepth¶
-
ResizeBendRadiusBuilder.
BendReliefDepth
¶ Returns the bend relief depth.
-------------------------------------
Getter Method
Signature
BendReliefDepth
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
BendReliefType¶
-
ResizeBendRadiusBuilder.
BendReliefType
¶ Returns the relief type for the resize bend radius feature.
The options are in
NXOpen.Features.SheetMetal.ResizeBendRadiusBuilder.BendReliefType()
.-------------------------------------
Getter Method
Signature
BendReliefType
Returns: Return type: NXOpen.Features.SheetMetal.ResizeBendRadiusBuilderBendReliefTypeOptions
New in version NX9.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
BendReliefWidth¶
-
ResizeBendRadiusBuilder.
BendReliefWidth
¶ Returns the bend relief width.
-------------------------------------
Getter Method
Signature
BendReliefWidth
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
ReferenceEntity¶
-
ResizeBendRadiusBuilder.
ReferenceEntity
¶ Returns the non-thickness planar face or linear edge to remain fixed while bend is resized
-------------------------------------
Getter Method
Signature
ReferenceEntity
Returns: Return type: NXOpen.SelectDisplayableObject
New in version NX7.0.0.
License requirements: None.
Type¶
-
ResizeBendRadiusBuilder.
Type
¶ Returns or sets the feature type
-------------------------------------
Getter Method
Signature
Type
Returns: Return type: NXOpen.Features.SheetMetal.ResizeBendRadiusBuilderTypes
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type
Parameters: type ( NXOpen.Features.SheetMetal.ResizeBendRadiusBuilderTypes
) –New in version NX7.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
Method Detail¶
SetBendReliefType¶
-
ResizeBendRadiusBuilder.
SetBendReliefType
¶ Signature
SetBendReliefType(bendReliefType)
Parameters: bendReliefType ( NXOpen.Features.SheetMetal.ResizeBendRadiusBuilderBendReliefTypeOptions
) –New in version NX9.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
Validate¶
-
ResizeBendRadiusBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.