MigratedPanelBuilder Class¶
-
class
NXOpen.Features.SheetMetal.
MigratedPanelBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents an I-DEAS Migrated Panel feature builder
This builder cannot be instantiated separately.
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
AlongFaceNormal | Returns or sets the along face normal flag. |
BendFace | Returns or sets the parent bend face. |
BendOptions | Returns the bend options for the panel feature. |
BendRadius | Returns or sets the bend radius expression. |
CutoffAngle | Returns or sets the cutoff angle expression. |
EndConditions | Returns the end conditions |
GapTolerance | Returns or sets the gap tolerance expression. |
MovingFace | Returns or sets the parent moving face. |
NeutralOffset | Returns or sets the neutral offset (i. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
ParentSmBody | Returns or sets the parent sheet metal body. |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
StationaryFace | Returns or sets the parent stationary face. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AlongFaceNormal¶
-
MigratedPanelBuilder.
AlongFaceNormal
¶ Returns or sets the along face normal flag.
This value only has meaning for the ground panel.
The edge that defines an end condition must be linear and must be on the stationary face for the Ground Panel and the moving face for other panels. The index indicates the position of the End Condition that will be modified. The first End Condition has an index of zero.
-------------------------------------
Getter Method
Signature
AlongFaceNormal
Returns: Along Face Normal flag Return type: bool New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
-------------------------------------
Setter Method
Signature
AlongFaceNormal
Parameters: alongFaceNormal (bool) – Along Face Normal flag New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
BendFace¶
-
MigratedPanelBuilder.
BendFace
¶ Returns or sets the parent bend face.
This face will usually be NULL. It will be non-NULL if this Migrated Panel was defined using the BFCS (Bend From Cylindrical Surface) method.
The set method is only available inside the I-DEAS to NX Content Migration Manager.
-------------------------------------
Getter Method
Signature
BendFace
Returns: The bend face Return type: NXOpen.Face
New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
-------------------------------------
Setter Method
Signature
BendFace
Parameters: bendFace ( NXOpen.Face
) – The bend faceNew in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
BendOptions¶
-
MigratedPanelBuilder.
BendOptions
¶ Returns the bend options for the panel feature.
-------------------------------------
Getter Method
Signature
BendOptions
Returns: Bend Options Return type: NXOpen.Features.SheetMetal.BendOptions
New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
BendRadius¶
-
MigratedPanelBuilder.
BendRadius
¶ Returns or sets the bend radius expression.
-------------------------------------
Getter Method
Signature
BendRadius
Returns: Gap tolerance Return type: str New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
-------------------------------------
Setter Method
Signature
BendRadius
Parameters: bendRadius (str) – Gap tolerance New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
CutoffAngle¶
-
MigratedPanelBuilder.
CutoffAngle
¶ Returns or sets the cutoff angle expression.
-------------------------------------
Getter Method
Signature
CutoffAngle
Returns: Cutoff angle Return type: str New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
-------------------------------------
Setter Method
Signature
CutoffAngle
Parameters: cutoffAngle (str) – Cutoff angle New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
EndConditions¶
-
MigratedPanelBuilder.
EndConditions
¶ Returns the end conditions
-------------------------------------
Getter Method
Signature
EndConditions
Returns: Return type: NXOpen.ExpressionCollectorSet
New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
GapTolerance¶
-
MigratedPanelBuilder.
GapTolerance
¶ Returns or sets the gap tolerance expression.
This is the size of the gap introduced between this panel and neighboring features.
-------------------------------------
Getter Method
Signature
GapTolerance
Returns: Gap tolerance Return type: str New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
-------------------------------------
Setter Method
Signature
GapTolerance
Parameters: gapTolerance (str) – Gap tolerance New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
MovingFace¶
-
MigratedPanelBuilder.
MovingFace
¶ Returns or sets the parent moving face.
This face will be NULL for the ground panel. If non-NULL, the face must be planar.
The set method is only available inside the I-DEAS to NX Content Migration Manager.
-------------------------------------
Getter Method
Signature
MovingFace
Returns: The moving face Return type: NXOpen.Face
New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
-------------------------------------
Setter Method
Signature
MovingFace
Parameters: moveFace ( NXOpen.Face
) – The moving faceNew in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
NeutralOffset¶
-
MigratedPanelBuilder.
NeutralOffset
¶ Returns or sets the neutral offset (i.
e., K Factor) expression.
-------------------------------------
Getter Method
Signature
NeutralOffset
Returns: Gap tolerance Return type: str New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
-------------------------------------
Setter Method
Signature
NeutralOffset
Parameters: gapTolerance (str) – Gap tolerance New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
ParentSmBody¶
-
MigratedPanelBuilder.
ParentSmBody
¶ Returns or sets the parent sheet metal body.
The Migrated Panel is applied to this body. The body must be made up of other Migrated Panel features. This body will be NULL for the ground panel.
The set method is only available inside the I-DEAS to NX Content Migration Manager.
-------------------------------------
Getter Method
Signature
ParentSmBody
Returns: Parent Sheet Metal Body Return type: NXOpen.Body
New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
-------------------------------------
Setter Method
Signature
ParentSmBody
Parameters: sheetMetalBody ( NXOpen.Body
) – Parent Sheet Metal BodyNew in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
StationaryFace¶
-
MigratedPanelBuilder.
StationaryFace
¶ Returns or sets the parent stationary face.
This face cannot be NULL.
The set method is only available inside the I-DEAS to NX Content Migration Manager.
-------------------------------------
Getter Method
Signature
StationaryFace
Returns: The stationary face Return type: NXOpen.Face
New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
-------------------------------------
Setter Method
Signature
StationaryFace
Parameters: stationaryFace ( NXOpen.Face
) – The stationary faceNew in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
Method Detail¶
Validate¶
-
MigratedPanelBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.