HemFlangeBuilder Class¶
-
class
NXOpen.Features.SheetMetal.
HemFlangeBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.HemFlange
builderTo create a new instance of this class, use
NXOpen.Features.SheetMetal.SheetmetalManager.CreateHemFlangeFeatureBuilder()
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
BendReliefDepth | Returns the bend relief depth |
BendReliefType | Returns or sets the bend relief type |
BendReliefWidth | Returns the bend relief width |
EdgeChain | Returns the edge chain |
FirstBendRadius | Returns the first bend radius |
FirstFlangeLength | Returns the first flange length |
InsetType | Returns or sets the inset type options |
MiterAngle | Returns the miter angle |
NeutralFactor | Returns the neutral factor |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SecondBendRadius | Returns the second bend radius |
SecondFlangeLength | Returns the second flange length |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
SweepAngle | Returns the sweep |
Tag | Returns the Tag for this object. |
Type | Returns or sets the hem type |
UseMiter | Returns or sets the use miter hem |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
HemFlangeBuilderBendReliefOptions Enumeration | This enum represents the Bend relief type of the hem flange. |
HemFlangeBuilderInsetTypeOptions Enumeration | This enum represents the inset type for the material of the hem flange. |
HemFlangeBuilderTypeOptions Enumeration | Represents the Hem Flange type. |
Property Detail¶
BendReliefDepth¶
-
HemFlangeBuilder.
BendReliefDepth
¶ Returns the bend relief depth
-------------------------------------
Getter Method
Signature
BendReliefDepth
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
BendReliefType¶
-
HemFlangeBuilder.
BendReliefType
¶ Returns or sets the bend relief type
-------------------------------------
Getter Method
Signature
BendReliefType
Returns: Return type: NXOpen.Features.SheetMetal.HemFlangeBuilderBendReliefOptions
New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
-------------------------------------
Setter Method
Signature
BendReliefType
Parameters: bendReliefType ( NXOpen.Features.SheetMetal.HemFlangeBuilderBendReliefOptions
) –New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
BendReliefWidth¶
-
HemFlangeBuilder.
BendReliefWidth
¶ Returns the bend relief width
-------------------------------------
Getter Method
Signature
BendReliefWidth
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
EdgeChain¶
-
HemFlangeBuilder.
EdgeChain
¶ Returns the edge chain
-------------------------------------
Getter Method
Signature
EdgeChain
Returns: Return type: NXOpen.ScCollector
New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
FirstBendRadius¶
-
HemFlangeBuilder.
FirstBendRadius
¶ Returns the first bend radius
-------------------------------------
Getter Method
Signature
FirstBendRadius
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
FirstFlangeLength¶
-
HemFlangeBuilder.
FirstFlangeLength
¶ Returns the first flange length
-------------------------------------
Getter Method
Signature
FirstFlangeLength
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
InsetType¶
-
HemFlangeBuilder.
InsetType
¶ Returns or sets the inset type options
-------------------------------------
Getter Method
Signature
InsetType
Returns: Return type: NXOpen.Features.SheetMetal.HemFlangeBuilderInsetTypeOptions
New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
-------------------------------------
Setter Method
Signature
InsetType
Parameters: insetType ( NXOpen.Features.SheetMetal.HemFlangeBuilderInsetTypeOptions
) –New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
MiterAngle¶
-
HemFlangeBuilder.
MiterAngle
¶ Returns the miter angle
-------------------------------------
Getter Method
Signature
MiterAngle
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
NeutralFactor¶
-
HemFlangeBuilder.
NeutralFactor
¶ Returns the neutral factor
-------------------------------------
Getter Method
Signature
NeutralFactor
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
SecondBendRadius¶
-
HemFlangeBuilder.
SecondBendRadius
¶ Returns the second bend radius
-------------------------------------
Getter Method
Signature
SecondBendRadius
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
SecondFlangeLength¶
-
HemFlangeBuilder.
SecondFlangeLength
¶ Returns the second flange length
-------------------------------------
Getter Method
Signature
SecondFlangeLength
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
SweepAngle¶
-
HemFlangeBuilder.
SweepAngle
¶ Returns the sweep
-------------------------------------
Getter Method
Signature
SweepAngle
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
Type¶
-
HemFlangeBuilder.
Type
¶ Returns or sets the hem type
-------------------------------------
Getter Method
Signature
Type
Returns: Return type: NXOpen.Features.SheetMetal.HemFlangeBuilderTypeOptions
New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
-------------------------------------
Setter Method
Signature
Type
Parameters: type ( NXOpen.Features.SheetMetal.HemFlangeBuilderTypeOptions
) –New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
UseMiter¶
-
HemFlangeBuilder.
UseMiter
¶ Returns or sets the use miter hem
-------------------------------------
Getter Method
Signature
UseMiter
Returns: Return type: bool New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
-------------------------------------
Setter Method
Signature
UseMiter
Parameters: useMiterHem (bool) – New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
Method Detail¶
Validate¶
-
HemFlangeBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.