ExportFlatPatternBuilder Class¶
-
class
NXOpen.Features.SheetMetal.
ExportFlatPatternBuilder
¶ Bases:
NXOpen.Builder
Represents a Export flat pattern builder.
To create a new instance of this class, use
NXOpen.Features.SheetMetal.SheetmetalManager.CreateExportFlatPatternBuilder()
Default values.
Property Value AddedBottom false AddedTop false BendDown true BendTangent false BendUp true InteriorCutout true InteriorFeature false New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
AddedBottom | Returns or sets the option to export the added bottom geometry |
AddedTop | Returns or sets the option to export the added top geometry |
BendDown | Returns or sets the option to export the bend down center line |
BendTangent | Returns or sets the option to export the bend tangent line |
BendUp | Returns or sets the option to export the bend up center line |
DeviationalTolerance | Returns or sets the deviational tolerance |
DxfRevision | Returns or sets the dxf revision. |
FlatPattern | Returns the flat pattern feature |
InnerMold | Returns or sets the option to export the inner mold |
InteriorCutout | Returns or sets the option to export the interior cutout |
InteriorFeature | Returns or sets the option to export the interior feature |
OuterMold | Returns or sets the option to export the outer mold |
OutputFile | Returns or sets the output file used to export flat pattern curves |
Tag | Returns the Tag for this object. |
Type | Returns or sets the type for the flat pattern export. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ExportFlatPatternBuilderDxfRevisionType Enumeration | Specifies the DXF Revisions for flat pattern export |
ExportFlatPatternBuilderFileType Enumeration | Specifies the flat pattern export type |
Property Detail¶
AddedBottom¶
-
ExportFlatPatternBuilder.
AddedBottom
¶ Returns or sets the option to export the added bottom geometry
-------------------------------------
Getter Method
Signature
AddedBottom
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AddedBottom
Parameters: addedBottom (bool) – New in version NX8.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
AddedTop¶
-
ExportFlatPatternBuilder.
AddedTop
¶ Returns or sets the option to export the added top geometry
-------------------------------------
Getter Method
Signature
AddedTop
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AddedTop
Parameters: addedTop (bool) – New in version NX8.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
BendDown¶
-
ExportFlatPatternBuilder.
BendDown
¶ Returns or sets the option to export the bend down center line
-------------------------------------
Getter Method
Signature
BendDown
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BendDown
Parameters: bendDown (bool) – New in version NX8.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
BendTangent¶
-
ExportFlatPatternBuilder.
BendTangent
¶ Returns or sets the option to export the bend tangent line
-------------------------------------
Getter Method
Signature
BendTangent
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BendTangent
Parameters: bendTangent (bool) – New in version NX8.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
BendUp¶
-
ExportFlatPatternBuilder.
BendUp
¶ Returns or sets the option to export the bend up center line
-------------------------------------
Getter Method
Signature
BendUp
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BendUp
Parameters: bendUp (bool) – New in version NX8.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
DeviationalTolerance¶
-
ExportFlatPatternBuilder.
DeviationalTolerance
¶ Returns or sets the deviational tolerance
-------------------------------------
Getter Method
Signature
DeviationalTolerance
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DeviationalTolerance
Parameters: deviationalTolerance (float) – New in version NX8.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
DxfRevision¶
-
ExportFlatPatternBuilder.
DxfRevision
¶ Returns or sets the dxf revision.
The options are in
NXOpen.Features.SheetMetal.ExportFlatPatternBuilderDxfRevisionType
.-------------------------------------
Getter Method
Signature
DxfRevision
Returns: Return type: NXOpen.Features.SheetMetal.ExportFlatPatternBuilderDxfRevisionType
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DxfRevision
Parameters: dxfRevision ( NXOpen.Features.SheetMetal.ExportFlatPatternBuilderDxfRevisionType
) –New in version NX8.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
FlatPattern¶
-
ExportFlatPatternBuilder.
FlatPattern
¶ Returns the flat pattern feature
-------------------------------------
Getter Method
Signature
FlatPattern
Returns: Return type: NXOpen.Features.SelectFlatPattern
New in version NX8.0.0.
License requirements: None.
InnerMold¶
-
ExportFlatPatternBuilder.
InnerMold
¶ Returns or sets the option to export the inner mold
Use this option only for the DXF type.
-------------------------------------
Getter Method
Signature
InnerMold
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InnerMold
Parameters: innerMold (bool) – New in version NX11.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
InteriorCutout¶
-
ExportFlatPatternBuilder.
InteriorCutout
¶ Returns or sets the option to export the interior cutout
-------------------------------------
Getter Method
Signature
InteriorCutout
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InteriorCutout
Parameters: interiorCutout (bool) – New in version NX8.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
InteriorFeature¶
-
ExportFlatPatternBuilder.
InteriorFeature
¶ Returns or sets the option to export the interior feature
-------------------------------------
Getter Method
Signature
InteriorFeature
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InteriorFeature
Parameters: interiorFeature (bool) – New in version NX8.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
OuterMold¶
-
ExportFlatPatternBuilder.
OuterMold
¶ Returns or sets the option to export the outer mold
Use this option only for the DXF type.
-------------------------------------
Getter Method
Signature
OuterMold
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OuterMold
Parameters: outerMold (bool) – New in version NX11.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
OutputFile¶
-
ExportFlatPatternBuilder.
OutputFile
¶ Returns or sets the output file used to export flat pattern curves
-------------------------------------
Getter Method
Signature
OutputFile
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OutputFile
Parameters: filename (str) – New in version NX8.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
Type¶
-
ExportFlatPatternBuilder.
Type
¶ Returns or sets the type for the flat pattern export.
The options are in
NXOpen.Features.SheetMetal.ExportFlatPatternBuilder.Type()
.-------------------------------------
Getter Method
Signature
Type
Returns: Return type: NXOpen.Features.SheetMetal.ExportFlatPatternBuilderFileType
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type
Parameters: type ( NXOpen.Features.SheetMetal.ExportFlatPatternBuilderFileType
) –New in version NX8.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
Method Detail¶
Validate¶
-
ExportFlatPatternBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.