ExportFlatPatternBuilderDxfRevisionType Enumeration¶
NXOpen.Features.SheetMetal.ExportFlatPatternBuilder.DxfRevisionType is an alias for NXOpen.Features.SheetMetal.ExportFlatPatternBuilderDxfRevisionType
-
class
NXOpen.Features.SheetMetal.
ExportFlatPatternBuilderDxfRevisionType
¶ Bases:
object
Specifies the DXF Revisions for flat pattern export
Enum Members
Enum Member Enum Member Description R2005 R2004 R2000 R14 R2007 R20102012 R20132016 R12 R13 -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-