ExportFlatPatternBuilderFileType Enumeration¶
NXOpen.Features.SheetMetal.ExportFlatPatternBuilder.FileType is an alias for NXOpen.Features.SheetMetal.ExportFlatPatternBuilderFileType
-
class
NXOpen.Features.SheetMetal.
ExportFlatPatternBuilderFileType
¶ Bases:
object
Specifies the flat pattern export type
Enum Members
Enum Member Enum Member Description Dxf DXF Export TrumpfGeo Trumpf Geo Export -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-