CleanUpUtilityBuilder Class¶
-
class
NXOpen.Features.SheetMetal.
CleanUpUtilityBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a Clean-Up Utility builder builder
To create a new instance of this class, use
NXOpen.Features.SheetMetal.SheetmetalManager.CreateCleanUpUtilityBuilder()
Default values.
Property Value SliverTol 0.009 ThicknessValue.Value 0 (millimeters part), 0 (inches part) UseGlobal 1 New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
HideOriginal | Returns or sets the hide original |
InferThickness | Returns or sets the infer thickness |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SelectBaseFace | Returns the select base face for clean-up utility |
SliverTol | Returns or sets the sliver tolerance |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
ThicknessValue | Returns the thickness value |
UseGlobal | Returns or sets the use global, if it equals to true - use global thickness value |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
HideOriginal¶
-
CleanUpUtilityBuilder.
HideOriginal
¶ Returns or sets the hide original
-------------------------------------
Getter Method
Signature
HideOriginal
Returns: The option to hide original value Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HideOriginal
Parameters: hideOriginal (bool) – The option to hide original value New in version NX7.5.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
InferThickness¶
-
CleanUpUtilityBuilder.
InferThickness
¶ Returns or sets the infer thickness
-------------------------------------
Getter Method
Signature
InferThickness
Returns: The option to infer thickness value Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InferThickness
Parameters: inferThickness (bool) – The option to infer thickness value New in version NX8.5.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
SelectBaseFace¶
-
CleanUpUtilityBuilder.
SelectBaseFace
¶ Returns the select base face for clean-up utility
-------------------------------------
Getter Method
Signature
SelectBaseFace
Returns: This face will specify top layer in processing the body. Return type: NXOpen.ScCollector
New in version NX7.5.0.
License requirements: None.
SliverTol¶
-
CleanUpUtilityBuilder.
SliverTol
¶ Returns or sets the sliver tolerance
-------------------------------------
Getter Method
Signature
SliverTol
Returns: The sliver tolerance value Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SliverTol
Parameters: sliverTol (float) – The sliver tolerance value New in version NX7.5.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
ThicknessValue¶
-
CleanUpUtilityBuilder.
ThicknessValue
¶ Returns the thickness value
-------------------------------------
Getter Method
Signature
ThicknessValue
Returns: The thickness value Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
UseGlobal¶
-
CleanUpUtilityBuilder.
UseGlobal
¶ Returns or sets the use global, if it equals to true - use global thickness value
-------------------------------------
Getter Method
Signature
UseGlobal
Returns: The option for global value Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseGlobal
Parameters: useGlobal (bool) – The option for global value New in version NX7.5.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
Method Detail¶
Validate¶
-
CleanUpUtilityBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.