BreakCornerBuilder Class¶
-
class
NXOpen.Features.SheetMetal.
BreakCornerBuilder
¶ Bases:
NXOpen.Features.SheetMetal.SheetmetalBaseBuilder
Represents a break corner feature builder.
To create a new instance of this class, use
NXOpen.Features.SheetMetal.SheetmetalManager.CreateBreakCornerFeatureBuilder()
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Type | Returns or sets the type of the break corner. |
Value | Returns the fillet radius or the setback value, depending on the type of the break corner. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetApplicationContext | Get the application context. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetEdges | The array of input edges for the break corner. |
GetFaces | The array of input faces that implicitly include all connected sharp thickness edges as input for the break corner. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetApplicationContext | Set the application context. |
SetEdges | The array of input edges for the break corner. |
SetFaces | The array of input faces that implicitly include all connected sharp thickness edges as input for the break corner. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
SetValue | |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
ValidateBuilderData | Verify that the builder data is valid for creating a break corner. |
Enumerations¶
BreakCornerBuilderTypeOptions Enumeration | This enum represents the break corner type. |
Property Detail¶
Type¶
-
BreakCornerBuilder.
Type
¶ Returns or sets the type of the break corner.
Specify
Features.SheetMetal.BreakCornerBuilderTypeOptions.Fillet
to fillet the edge. SpecifyFeatures.SheetMetal.BreakCornerBuilderTypeOptions.ChamferEqualSetback
to chamfer the edge.-------------------------------------
Getter Method
Signature
Type
Returns: Break corner type Return type: NXOpen.Features.SheetMetal.BreakCornerBuilderTypeOptions
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
-------------------------------------
Setter Method
Signature
Type
Parameters: type ( NXOpen.Features.SheetMetal.BreakCornerBuilderTypeOptions
) – Break corner typeNew in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
Value¶
-
BreakCornerBuilder.
Value
¶ Returns the fillet radius or the setback value, depending on the type of the break corner.
-------------------------------------
Getter Method
Signature
Value
Returns: Either fillet radius or setback value (depending on the type of break corner) Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
Method Detail¶
GetEdges¶
-
BreakCornerBuilder.
GetEdges
¶ The array of input edges for the break corner.
Signature
GetEdges()
Returns: Edge list Return type: list of NXOpen.Edge
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
GetFaces¶
-
BreakCornerBuilder.
GetFaces
¶ The array of input faces that implicitly include all connected sharp thickness edges as input for the break corner.
Signature
GetFaces()
Returns: Face list Return type: list of NXOpen.Face
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
SetEdges¶
-
BreakCornerBuilder.
SetEdges
¶ The array of input edges for the break corner.
Signature
SetEdges(edges)
Parameters: edges (list of NXOpen.Edge
) – Edge listNew in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
SetFaces¶
-
BreakCornerBuilder.
SetFaces
¶ The array of input faces that implicitly include all connected sharp thickness edges as input for the break corner.
Signature
SetFaces(faces)
Parameters: faces (list of NXOpen.Face
) – Face listNew in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
SetValue¶
-
BreakCornerBuilder.
SetValue
¶ Signature
SetValue(filletRadiusOrSetback)
Parameters: filletRadiusOrSetback (str) – Either fillet radius or setback value (depending on the type of break corner) New in version NX4.0.0.
Deprecated since version NX10.0.0: Use
Expression.RightHandSide()
on theExpression
object returned fromFeatures.SheetMetal.BreakCornerBuilder.Value()
instead.License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
Validate¶
-
BreakCornerBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.
ValidateBuilderData¶
-
BreakCornerBuilder.
ValidateBuilderData
¶ Verify that the builder data is valid for creating a break corner.
If the Builder data is valid, return value is 0
Signature
ValidateBuilderData()
Returns: Data validity flag (zero for valid and non-zero for invalid) Return type: int New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)