ScaleCurveBuilder Class¶
-
class
NXOpen.Features.
ScaleCurveBuilder
¶ Bases:
NXOpen.Features.ServiceOrientedFeatureCurveBuilder
Represents a
Features.ScaleCurveBuilder
builderTo create a new instance of this class, use
NXOpen.Features.CurveFeatureCollection.CreateScaleCurveBuilder()
Default values.
Property Value CurveSettings.CurveFitData.CurveJoinMethod No CurveSettings.CurveFitData.Degree 7 CurveSettings.CurveFitData.FitMethod DegreeAndSegments CurveSettings.CurveFitData.IsAdvancedFit 0 CurveSettings.CurveFitData.IsAlignShape 0 CurveSettings.CurveFitData.MaximumDegree 7 CurveSettings.CurveFitData.MaximumSegments 1 CurveSettings.CurveFitData.MinimumDegree 5 CurveSettings.CurveFitData.Segments 1 ScaleAlongXDirection.Value 1 ScaleAlongYDirection.Value 1 ScaleAlongZDirection.Value 1 ScaleType Uniform UniformScaleFactor.Value 1 New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
CurveSettings | Returns or sets the curve setting data |
ObjectsToScale | Returns the input cuvres,point to scale |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
ReferenceCSYS | Returns or sets the reference csys |
ReferencePoint | Returns or sets the reference point |
ScaleAlongXDirection | Returns the scale along xdirection |
ScaleAlongYDirection | Returns the scale along ydirection |
ScaleAlongZDirection | Returns the scale along zdirection |
ScaleType | Returns or sets the scale type |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
UniformScaleFactor | Returns the uniform scale factor |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ScaleCurveBuilderScaleCurveType Enumeration | Scale type |
Property Detail¶
CurveSettings¶
-
ScaleCurveBuilder.
CurveSettings
¶ Returns or sets the curve setting data
-------------------------------------
Getter Method
Signature
CurveSettings
Returns: Return type: NXOpen.GeometricUtilities.CurveSettings
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CurveSettings
Parameters: curveSettingData ( NXOpen.GeometricUtilities.CurveSettings
) –New in version NX11.0.0.
License requirements: None.
ObjectsToScale¶
-
ScaleCurveBuilder.
ObjectsToScale
¶ Returns the input cuvres,point to scale
-------------------------------------
Getter Method
Signature
ObjectsToScale
Returns: Return type: NXOpen.Section
New in version NX11.0.0.
License requirements: None.
ReferenceCSYS¶
-
ScaleCurveBuilder.
ReferenceCSYS
¶ Returns or sets the reference csys
-------------------------------------
Getter Method
Signature
ReferenceCSYS
Returns: Return type: NXOpen.CoordinateSystem
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReferenceCSYS
Parameters: referenceCSYS ( NXOpen.CoordinateSystem
) –New in version NX11.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
ReferencePoint¶
-
ScaleCurveBuilder.
ReferencePoint
¶ Returns or sets the reference point
-------------------------------------
Getter Method
Signature
ReferencePoint
Returns: Return type: NXOpen.Point
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReferencePoint
Parameters: referencePoint ( NXOpen.Point
) –New in version NX11.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
ScaleAlongXDirection¶
-
ScaleCurveBuilder.
ScaleAlongXDirection
¶ Returns the scale along xdirection
-------------------------------------
Getter Method
Signature
ScaleAlongXDirection
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: None.
ScaleAlongYDirection¶
-
ScaleCurveBuilder.
ScaleAlongYDirection
¶ Returns the scale along ydirection
-------------------------------------
Getter Method
Signature
ScaleAlongYDirection
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: None.
ScaleAlongZDirection¶
-
ScaleCurveBuilder.
ScaleAlongZDirection
¶ Returns the scale along zdirection
-------------------------------------
Getter Method
Signature
ScaleAlongZDirection
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: None.
ScaleType¶
-
ScaleCurveBuilder.
ScaleType
¶ Returns or sets the scale type
-------------------------------------
Getter Method
Signature
ScaleType
Returns: Return type: NXOpen.Features.ScaleCurveBuilderScaleCurveType
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ScaleType
Parameters: scaleType ( NXOpen.Features.ScaleCurveBuilderScaleCurveType
) –New in version NX11.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
UniformScaleFactor¶
-
ScaleCurveBuilder.
UniformScaleFactor
¶ Returns the uniform scale factor
-------------------------------------
Getter Method
Signature
UniformScaleFactor
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
ScaleCurveBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.