RapidSurfaceBuilder Class¶
-
class
NXOpen.Features.
RapidSurfaceBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.RapidSurface
builderTo create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateRapidSurfaceBuilder()
Default values.
Property Value AttachmentType FacetBody Degree 3 LoopType FourSided NodeTolerance 1.0 Segments 10 Smoothness 100 UPatches 2 VPatches 2 New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
AttachmentType | Returns or sets the attachment type |
Body | Returns the facet body. |
BoundaryPointSetManager | Returns the boundary point set manager |
ConnectCurves | Returns the connect curves |
ConstraintSetManager | Returns the constraint set manager |
Degree | Returns or sets the degree |
DeleteCurves | Returns the delete curves |
DragCurve | Returns the drag curve |
DragCurvePointManager | Returns the curve used for drag curve point |
FacetBody | Returns the facet body |
ImportCurves | Returns the import curves |
LoopType | Returns or sets the subdivision loop type |
NodeTolerance | Returns or sets the node tolerance |
OperationType | Returns or sets the operation type |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
ProjectDirection | Returns or sets the projection direction |
Segments | Returns or sets the segments |
Smoothness | Returns or sets the smoothness |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
ULoopCurve | Returns the loop curve(U) |
UPatches | Returns or sets the patches(U) |
VLoopCurve | Returns the loop curve(V) |
VPatches | Returns or sets the patches(V) |
Methods¶
Method | Description |
---|---|
AcceptNewFacetBody | Accepts new facet body |
AcceptSubdivision | Accepts subdivision |
AskEdge | Asks an edge in the current curve network |
AskEdgeCount | Asks edge count in the current curve network |
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
ConnectCurve | Accepts connect curve |
CreateAnimationPolyline | Creates animation polyline |
CreateBoundaryCurve | Creates boundary curve |
CreateNodePoints | Creates points to record every mesh node |
DeleteCurve | Deletes curve |
DeleteNode | Deletes node |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
DragCurvePoint | Drags curve point |
DrawBoundaryCurve | Draws boundary curve |
DrawCurve | Draws curve |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetNode | Gets a node in the current curve network |
GetNodeCount | Gets node count in the current curve network |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
ImportCurve | Imports curve |
MoveNode | Moves node |
ReprojectEdgesAfterMoveNode | Reprojects edges after move node |
ResetAnimationPolyline | Resets animation polyline |
SetADefinePoint | Set a define point (pre-NX6) |
SetDefiningPoint | Sets a defining point |
SetNumberOfDefinePoints | Set number of define points (pre-NX6) |
SetNumberOfDefiningPoints | Sets number of defining points |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
RapidSurfaceBuilderAttachmentTypes Enumeration | the attachment types |
RapidSurfaceBuilderLoopTypes Enumeration | the subdivision loop types |
RapidSurfaceBuilderOperationTypes Enumeration | the operation types |
Property Detail¶
AttachmentType¶
-
RapidSurfaceBuilder.
AttachmentType
¶ Returns or sets the attachment type
-------------------------------------
Getter Method
Signature
AttachmentType
Returns: Return type: NXOpen.Features.RapidSurfaceBuilderAttachmentTypes
New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
-------------------------------------
Setter Method
Signature
AttachmentType
Parameters: option ( NXOpen.Features.RapidSurfaceBuilderAttachmentTypes
) –New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
Body¶
-
RapidSurfaceBuilder.
Body
¶ Returns the facet body.
Inputs to this command can be convergent objects.
-------------------------------------
Getter Method
Signature
Body
Returns: Return type: NXOpen.SelectDisplayableObject
New in version NX11.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
BoundaryPointSetManager¶
-
RapidSurfaceBuilder.
BoundaryPointSetManager
¶ Returns the boundary point set manager
-------------------------------------
Getter Method
Signature
BoundaryPointSetManager
Returns: Return type: NXOpen.Features.GeometricConstraintDataSetManager
New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
ConnectCurves¶
-
RapidSurfaceBuilder.
ConnectCurves
¶ Returns the connect curves
-------------------------------------
Getter Method
Signature
ConnectCurves
Returns: Return type: NXOpen.SelectCurveList
New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
ConstraintSetManager¶
-
RapidSurfaceBuilder.
ConstraintSetManager
¶ Returns the constraint set manager
-------------------------------------
Getter Method
Signature
ConstraintSetManager
Returns: Return type: NXOpen.Features.GeometricConstraintDataSetManager
New in version NX5.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
Degree¶
-
RapidSurfaceBuilder.
Degree
¶ Returns or sets the degree
-------------------------------------
Getter Method
Signature
Degree
Returns: Return type: int New in version NX5.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
-------------------------------------
Setter Method
Signature
Degree
Parameters: degree (int) – New in version NX5.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
DeleteCurves¶
-
RapidSurfaceBuilder.
DeleteCurves
¶ Returns the delete curves
-------------------------------------
Getter Method
Signature
DeleteCurves
Returns: Return type: NXOpen.SelectCurveList
New in version NX5.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
DragCurve¶
-
RapidSurfaceBuilder.
DragCurve
¶ Returns the drag curve
-------------------------------------
Getter Method
Signature
DragCurve
Returns: Return type: NXOpen.SelectCurve
New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
DragCurvePointManager¶
-
RapidSurfaceBuilder.
DragCurvePointManager
¶ Returns the curve used for drag curve point
-------------------------------------
Getter Method
Signature
DragCurvePointManager
Returns: Return type: NXOpen.Features.GeometricConstraintDataSetManager
New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
FacetBody¶
-
RapidSurfaceBuilder.
FacetBody
¶ Returns the facet body
-------------------------------------
Getter Method
Signature
FacetBody
Returns: Return type: NXOpen.Facet.SelectFacetedBody
New in version NX5.0.0.
Deprecated since version NX11.0.0: Use
NXOpen.Features.RapidSurfaceBuilder.Body()
instead.License requirements: studio_free_form (“STUDIO FREE FORM”)
ImportCurves¶
-
RapidSurfaceBuilder.
ImportCurves
¶ Returns the import curves
-------------------------------------
Getter Method
Signature
ImportCurves
Returns: Return type: NXOpen.SelectCurveList
New in version NX5.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
LoopType¶
-
RapidSurfaceBuilder.
LoopType
¶ Returns or sets the subdivision loop type
-------------------------------------
Getter Method
Signature
LoopType
Returns: Return type: NXOpen.Features.RapidSurfaceBuilderLoopTypes
New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
-------------------------------------
Setter Method
Signature
LoopType
Parameters: option ( NXOpen.Features.RapidSurfaceBuilderLoopTypes
) –New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
NodeTolerance¶
-
RapidSurfaceBuilder.
NodeTolerance
¶ Returns or sets the node tolerance
-------------------------------------
Getter Method
Signature
NodeTolerance
Returns: Return type: float New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
-------------------------------------
Setter Method
Signature
NodeTolerance
Parameters: nodeTolerance (float) – New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
OperationType¶
-
RapidSurfaceBuilder.
OperationType
¶ Returns or sets the operation type
-------------------------------------
Getter Method
Signature
OperationType
Returns: Return type: NXOpen.Features.RapidSurfaceBuilderOperationTypes
New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
-------------------------------------
Setter Method
Signature
OperationType
Parameters: option ( NXOpen.Features.RapidSurfaceBuilderOperationTypes
) –New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
ProjectDirection¶
-
RapidSurfaceBuilder.
ProjectDirection
¶ Returns or sets the projection direction
-------------------------------------
Getter Method
Signature
ProjectDirection
Returns: Return type: NXOpen.Direction
New in version NX5.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
-------------------------------------
Setter Method
Signature
ProjectDirection
Parameters: projectDirection ( NXOpen.Direction
) –New in version NX5.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
Segments¶
-
RapidSurfaceBuilder.
Segments
¶ Returns or sets the segments
-------------------------------------
Getter Method
Signature
Segments
Returns: Return type: int New in version NX5.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
-------------------------------------
Setter Method
Signature
Segments
Parameters: segments (int) – New in version NX5.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
Smoothness¶
-
RapidSurfaceBuilder.
Smoothness
¶ Returns or sets the smoothness
-------------------------------------
Getter Method
Signature
Smoothness
Returns: Return type: int New in version NX5.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
-------------------------------------
Setter Method
Signature
Smoothness
Parameters: smoothness (int) – New in version NX5.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
ULoopCurve¶
-
RapidSurfaceBuilder.
ULoopCurve
¶ Returns the loop curve(U)
-------------------------------------
Getter Method
Signature
ULoopCurve
Returns: Return type: NXOpen.SelectCurve
New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
UPatches¶
-
RapidSurfaceBuilder.
UPatches
¶ Returns or sets the patches(U)
-------------------------------------
Getter Method
Signature
UPatches
Returns: Return type: int New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
-------------------------------------
Setter Method
Signature
UPatches
Parameters: patchesU (int) – New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
VLoopCurve¶
-
RapidSurfaceBuilder.
VLoopCurve
¶ Returns the loop curve(V)
-------------------------------------
Getter Method
Signature
VLoopCurve
Returns: Return type: NXOpen.SelectCurve
New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
VPatches¶
-
RapidSurfaceBuilder.
VPatches
¶ Returns or sets the patches(V)
-------------------------------------
Getter Method
Signature
VPatches
Returns: Return type: int New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
-------------------------------------
Setter Method
Signature
VPatches
Parameters: patchesV (int) – New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
Method Detail¶
AcceptNewFacetBody¶
-
RapidSurfaceBuilder.
AcceptNewFacetBody
¶ Accepts new facet body
Signature
AcceptNewFacetBody()
New in version NX5.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
AcceptSubdivision¶
-
RapidSurfaceBuilder.
AcceptSubdivision
¶ Accepts subdivision
Signature
AcceptSubdivision()
New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
AskEdge¶
-
RapidSurfaceBuilder.
AskEdge
¶ Asks an edge in the current curve network
Signature
AskEdge(edgeIndex)
Parameters: edgeIndex (int) – Edge Index Returns: Return type: NXOpen.Spline
New in version NX5.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
AskEdgeCount¶
-
RapidSurfaceBuilder.
AskEdgeCount
¶ Asks edge count in the current curve network
Signature
AskEdgeCount()
Returns: Return type: int New in version NX5.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
ConnectCurve¶
-
RapidSurfaceBuilder.
ConnectCurve
¶ Accepts connect curve
Signature
ConnectCurve()
New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
CreateAnimationPolyline¶
-
RapidSurfaceBuilder.
CreateAnimationPolyline
¶ Creates animation polyline
Signature
CreateAnimationPolyline()
New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
CreateBoundaryCurve¶
-
RapidSurfaceBuilder.
CreateBoundaryCurve
¶ Creates boundary curve
Signature
CreateBoundaryCurve()
New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
CreateNodePoints¶
-
RapidSurfaceBuilder.
CreateNodePoints
¶ Creates points to record every mesh node
Signature
CreateNodePoints()
Returns: Return type: list of NXOpen.Point
New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
DeleteCurve¶
-
RapidSurfaceBuilder.
DeleteCurve
¶ Deletes curve
Signature
DeleteCurve()
New in version NX5.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
DeleteNode¶
-
RapidSurfaceBuilder.
DeleteNode
¶ Deletes node
Signature
DeleteNode(point)
Parameters: point ( NXOpen.Point
) – PointNew in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
DragCurvePoint¶
-
RapidSurfaceBuilder.
DragCurvePoint
¶ Drags curve point
Signature
DragCurvePoint()
New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
DrawBoundaryCurve¶
-
RapidSurfaceBuilder.
DrawBoundaryCurve
¶ Draws boundary curve
Signature
DrawBoundaryCurve()
New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
DrawCurve¶
-
RapidSurfaceBuilder.
DrawCurve
¶ Draws curve
Signature
DrawCurve()
New in version NX5.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
GetNode¶
-
RapidSurfaceBuilder.
GetNode
¶ Gets a node in the current curve network
Signature
GetNode(nodeIndex)
Parameters: nodeIndex (int) – Node Index Returns: Return type: NXOpen.Point
New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
GetNodeCount¶
-
RapidSurfaceBuilder.
GetNodeCount
¶ Gets node count in the current curve network
Signature
GetNodeCount()
Returns: Return type: int New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
ImportCurve¶
-
RapidSurfaceBuilder.
ImportCurve
¶ Imports curve
Signature
ImportCurve()
New in version NX5.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
MoveNode¶
-
RapidSurfaceBuilder.
MoveNode
¶ Moves node
Signature
MoveNode(point, newPosition)
Parameters: - point (
NXOpen.Point
) – Point - newPosition (
NXOpen.Point3d
) – the new position the point move to
New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
- point (
ReprojectEdgesAfterMoveNode¶
-
RapidSurfaceBuilder.
ReprojectEdgesAfterMoveNode
¶ Reprojects edges after move node
Signature
ReprojectEdgesAfterMoveNode()
New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
ResetAnimationPolyline¶
-
RapidSurfaceBuilder.
ResetAnimationPolyline
¶ Resets animation polyline
Signature
ResetAnimationPolyline()
New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
SetADefinePoint¶
-
RapidSurfaceBuilder.
SetADefinePoint
¶ Set a define point (pre-NX6)
Signature
SetADefinePoint(index, xx, yy, zz, facetID)
Parameters: - index (int) – Index of Defined Point
- xx (float) – XC of Defined Point
- yy (float) – YC of Defined Point
- zz (float) – ZC of Defined Point
- facetID (int) – Facet ID of Defined Point
New in version NX5.0.0.
Deprecated since version NX6.0.0: Use
NXOpen.Features.RapidSurfaceBuilder.SetDefiningPoint()
instead.License requirements: studio_free_form (“STUDIO FREE FORM”)
SetDefiningPoint¶
-
RapidSurfaceBuilder.
SetDefiningPoint
¶ Sets a defining point
Signature
SetDefiningPoint(index, coordination, facetID)
Parameters: - index (int) – Index of Defined Point
- coordination (
NXOpen.Point3d
) – x,y,z coordination of Defined Point - facetID (int) – Facet ID of Defined Point
New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
SetNumberOfDefinePoints¶
-
RapidSurfaceBuilder.
SetNumberOfDefinePoints
¶ Set number of define points (pre-NX6)
Signature
SetNumberOfDefinePoints(number)
Parameters: number (int) – Number of Defined Points New in version NX5.0.0.
Deprecated since version NX6.0.0: Use
NXOpen.Features.RapidSurfaceBuilder.SetNumberOfDefiningPoints()
instead.License requirements: studio_free_form (“STUDIO FREE FORM”)
SetNumberOfDefiningPoints¶
-
RapidSurfaceBuilder.
SetNumberOfDefiningPoints
¶ Sets number of defining points
Signature
SetNumberOfDefiningPoints(number)
Parameters: number (int) – Number of Defined Points New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
Validate¶
-
RapidSurfaceBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.