RapidSurfaceBuilderLoopTypes Enumeration¶
NXOpen.Features.RapidSurfaceBuilder.LoopTypes is an alias for NXOpen.Features.RapidSurfaceBuilderLoopTypes
-
class
NXOpen.Features.
RapidSurfaceBuilderLoopTypes
¶ Bases:
object
the subdivision loop types
Enum Members
Enum Member Enum Member Description FourSided subdivide four sided loops ThreeSided subdivide three sided loops -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-