MeshSurfaceBuilder Class¶
-
class
NXOpen.Features.
MeshSurfaceBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Mesh Surface Builder class.
To create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateMeshSurfaceBuilder()
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
FaceConstraintDirection | Returns or sets |
FeatureType | Returns or sets |
NormalToEndSections | Returns or sets the normal to end sections for Through Curves surface. |
ParametersData | Returns or sets |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
RebuildData | Returns or sets |
SimpleConstruction | Returns or sets |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
BuildProfileFromSections | Creates mesh surface profile string. |
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetAngleAlignmentPoints | Get angle alignment points |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetDistanceAlignmentVector | Get distance alignment vector |
GetFaceConstraintCollectors | Get faces constraints collectors for through curves and curves mesh types surfaces. |
GetFaceConstraintTypes | Get end constraints types. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
GetProfile | Get mesh profile string with provided index. |
GetProfilePointAlignment | Get profile string point alignment info. |
GetToleranceString | Get tolerances strings. |
GetTolerances | Get tolerances. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
InsertProfileString | Insert a string (string_index, with order) into a profile (profile_index). |
NewParametersData | Create a mesh parameters transient object data. |
NewProfile | Construct a new mesh profile string transient object. |
NewRebuildData | Allocate memory for Mesh type surface rebuild data. |
RemovePointsAlignment | Remove points alignment information. |
RemoveProfileString | Remove a string (string_index) from a profile (profile_index) |
RemoveSpineAlignment | Remove spine alignment. |
ReorderProfileStringCurves | Reorder profile string curves. |
RestorePointsAlignment | Restore the last removed points alignment information if there is one. |
SetAngleAlignmentPoints | Set angle alignment points. |
SetDistanceAlignmentVector | Set distance alignment vector |
SetFaceConstraintCollectors | Set faces constraints collectors for through curves and curves mesh types surfaces. |
SetFaceConstraintTypes | Set end constraints types. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
SetProfilePointAlignment | Set profile string alignment info. |
SetToleranceString | Set tolerances strings for mesh type surface. |
SetTolerances | Set tolerances for mesh type surfaces. |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
ValidateFeatureParameters | Validate the new parameters for mesh surface editing. |
Enumerations¶
MeshSurfaceBuilderConstraintDirection Enumeration | End face constraints direction. |
MeshSurfaceBuilderConstraintType Enumeration | End face constraints types. |
Property Detail¶
FaceConstraintDirection¶
-
MeshSurfaceBuilder.
FaceConstraintDirection
¶ Returns or sets
-------------------------------------
Getter Method
Signature
FaceConstraintDirection
Returns: Return type: NXOpen.Features.MeshSurfaceBuilderConstraintDirection
New in version NX4.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
-------------------------------------
Setter Method
Signature
FaceConstraintDirection
Parameters: constraintDirection ( NXOpen.Features.MeshSurfaceBuilderConstraintDirection
) –New in version NX4.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
FeatureType¶
-
MeshSurfaceBuilder.
FeatureType
¶ Returns or sets
-------------------------------------
Getter Method
Signature
FeatureType
Returns: Return type: NXOpen.MeshParameterDataFeatureType
New in version NX4.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
-------------------------------------
Setter Method
Signature
FeatureType
Parameters: featureType ( NXOpen.MeshParameterDataFeatureType
) –New in version NX4.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
NormalToEndSections¶
-
MeshSurfaceBuilder.
NormalToEndSections
¶ Returns or sets the normal to end sections for Through Curves surface.
-------------------------------------
Getter Method
Signature
NormalToEndSections
Returns: Return type: bool New in version NX5.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
-------------------------------------
Setter Method
Signature
NormalToEndSections
Parameters: normalToEndSections (bool) – New in version NX5.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
ParametersData¶
-
MeshSurfaceBuilder.
ParametersData
¶ Returns or sets
-------------------------------------
Getter Method
Signature
ParametersData
Returns: Return type: NXOpen.MeshParameterData
New in version NX4.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
-------------------------------------
Setter Method
Signature
ParametersData
Parameters: parameters ( NXOpen.MeshParameterData
) –New in version NX4.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
RebuildData¶
-
MeshSurfaceBuilder.
RebuildData
¶ Returns or sets
-------------------------------------
Getter Method
Signature
RebuildData
Returns: Requested rebuild data. Return type: NXOpen.SurfaceRebuildData
New in version NX4.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
-------------------------------------
Setter Method
Signature
RebuildData
Parameters: rbData ( NXOpen.SurfaceRebuildData
) – Rebuild dataNew in version NX4.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
SimpleConstruction¶
-
MeshSurfaceBuilder.
SimpleConstruction
¶ Returns or sets
-------------------------------------
Getter Method
Signature
SimpleConstruction
Returns: Return type: bool New in version NX4.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
-------------------------------------
Setter Method
Signature
SimpleConstruction
Parameters: simple (bool) – New in version NX4.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
Method Detail¶
BuildProfileFromSections¶
-
MeshSurfaceBuilder.
BuildProfileFromSections
¶ Creates mesh surface profile string.
Signature
BuildProfileFromSections(conehead, profileStringType, skinType, stringPointType, sections, editInsertProfile, profile)
Parameters: - conehead (bool) – Display conehead?
- profileStringType (
NXOpen.MeshProfileStringType
) – Mesh profile string type - skinType (
NXOpen.MeshParameterDataFeatureType
) – Mesh surface type - stringPointType (
NXOpen.MeshProfileStringSelectedPoint
) – Profile string point type - sections (list of
NXOpen.Section
) – Sections - editInsertProfile (bool) – Flag to indicate if this is temporary profile to inserting new string purpose only.
- profile (
NXOpen.MeshProfileString
) – Mesh profile string
New in version NX4.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
GetAngleAlignmentPoints¶
-
MeshSurfaceBuilder.
GetAngleAlignmentPoints
¶ Get angle alignment points
Signature
GetAngleAlignmentPoints()
Returns: a tuple Return type: A tuple consisting of (point1, point2). point1 is a NXOpen.Point3d
. Point 1 point2 is aNXOpen.Point3d
. Point 2New in version NX4.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
GetDistanceAlignmentVector¶
-
MeshSurfaceBuilder.
GetDistanceAlignmentVector
¶ Get distance alignment vector
Signature
GetDistanceAlignmentVector()
Returns: Vector Return type: NXOpen.Vector3d
New in version NX4.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
GetFaceConstraintCollectors¶
-
MeshSurfaceBuilder.
GetFaceConstraintCollectors
¶ Get faces constraints collectors for through curves and curves mesh types surfaces.
Signature
GetFaceConstraintCollectors(nSides, numCollectors, numConsTypes)
Parameters: - nSides (int) –
- numCollectors (int) –
- numConsTypes (int) –
Returns: a tuple
Return type: A tuple consisting of (facesCons, collectors, consTypes). facesCons is a list of int. Number of faces on each side collectors is a list of
NXOpen.ScCollector
. Constraints collectors. consTypes is a list ofNXOpen.Features.MeshSurfaceBuilderConstraintType
. type on each side.New in version NX4.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
GetFaceConstraintTypes¶
-
MeshSurfaceBuilder.
GetFaceConstraintTypes
¶ Get end constraints types.
Signature
GetFaceConstraintTypes(constraintSize)
Parameters: constraintSize (int) – Returns: Constraint types Return type: list of NXOpen.Features.MeshSurfaceBuilderConstraintType
New in version NX4.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
GetProfile¶
-
MeshSurfaceBuilder.
GetProfile
¶ Get mesh profile string with provided index.
Signature
GetProfile(index)
Parameters: index (int) – Profile index. Returns: Requested profile data. Return type: NXOpen.MeshProfileString
New in version NX4.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
GetProfilePointAlignment¶
-
MeshSurfaceBuilder.
GetProfilePointAlignment
¶ Get profile string point alignment info.
Given a profile string, get alignment point parameters on segments indexed by align_index along the profile string.
Signature
GetProfilePointAlignment(stringIndex, arrayLength)
Parameters: - stringIndex (int) – string index in profile strings
- arrayLength (int) –
Returns: a tuple
Return type: A tuple consisting of (alignIndex, alignParams) alignIndex is a list of int. Alignment indices alignParams is a list of float. Alignment parameters
New in version NX4.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
GetToleranceString¶
-
MeshSurfaceBuilder.
GetToleranceString
¶ Get tolerances strings.
Signature
GetToleranceString(tolStrLength)
Parameters: tolStrLength (int) – Returns: Return type: list of str New in version NX4.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
GetTolerances¶
-
MeshSurfaceBuilder.
GetTolerances
¶ Get tolerances.
Signature
GetTolerances(tolLength)
Parameters: tolLength (int) – Returns: Return type: list of float New in version NX4.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
InsertProfileString¶
-
MeshSurfaceBuilder.
InsertProfileString
¶ Insert a string (string_index, with order) into a profile (profile_index).
Signature
InsertProfileString(profileIndex, order, stringIndex)
Parameters: - profileIndex (int) – mesh profile string index
- order (
NXOpen.MeshProfileStringInsertOrder
) – before or after - stringIndex (int) – String index in mesh profile string
New in version NX4.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
NewParametersData¶
-
MeshSurfaceBuilder.
NewParametersData
¶ Create a mesh parameters transient object data.
Signature
NewParametersData()
Returns: Allocated rebuild data. Return type: NXOpen.MeshParameterData
New in version NX4.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
NewProfile¶
-
MeshSurfaceBuilder.
NewProfile
¶ Construct a new mesh profile string transient object.
Signature
NewProfile()
Returns: New mesh profile string. Return type: NXOpen.MeshProfileString
New in version NX4.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
NewRebuildData¶
-
MeshSurfaceBuilder.
NewRebuildData
¶ Allocate memory for Mesh type surface rebuild data.
Signature
NewRebuildData()
Returns: Allocated rebuild data. Return type: NXOpen.SurfaceRebuildData
New in version NX4.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
RemovePointsAlignment¶
-
MeshSurfaceBuilder.
RemovePointsAlignment
¶ Remove points alignment information.
Remove alignment can be restore by calling
Features.MeshSurfaceBuilder.RestorePointsAlignment()
Signature
RemovePointsAlignment()
New in version NX4.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
RemoveProfileString¶
-
MeshSurfaceBuilder.
RemoveProfileString
¶ Remove a string (string_index) from a profile (profile_index)
Signature
RemoveProfileString(profileIndex, stringIndex)
Parameters: - profileIndex (int) – mesh profile string index
- stringIndex (int) – String index in mesh profile string
New in version NX4.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
RemoveSpineAlignment¶
-
MeshSurfaceBuilder.
RemoveSpineAlignment
¶ Remove spine alignment.
Signature
RemoveSpineAlignment()
New in version NX4.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
ReorderProfileStringCurves¶
-
MeshSurfaceBuilder.
ReorderProfileStringCurves
¶ Reorder profile string curves.
Signature
ReorderProfileStringCurves(stringIndex, stringStartCurve)
Parameters: - stringIndex (int) – Profile string index.
- stringStartCurve (
NXOpen.Curve
) – New start curve.
New in version NX4.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
RestorePointsAlignment¶
-
MeshSurfaceBuilder.
RestorePointsAlignment
¶ Restore the last removed points alignment information if there is one.
Once restored, the saved alignment information will no logner be available.
Signature
RestorePointsAlignment()
New in version NX4.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
SetAngleAlignmentPoints¶
-
MeshSurfaceBuilder.
SetAngleAlignmentPoints
¶ Set angle alignment points.
Points will be used to evaluate the alignment angle.
Signature
SetAngleAlignmentPoints(point1, point2)
Parameters: - point1 (
NXOpen.Point3d
) – Point 1 - point2 (
NXOpen.Point3d
) – Point 2
New in version NX4.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
- point1 (
SetDistanceAlignmentVector¶
-
MeshSurfaceBuilder.
SetDistanceAlignmentVector
¶ Set distance alignment vector
Signature
SetDistanceAlignmentVector(vector)
Parameters: vector ( NXOpen.Vector3d
) – VectorNew in version NX4.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
SetFaceConstraintCollectors¶
-
MeshSurfaceBuilder.
SetFaceConstraintCollectors
¶ Set faces constraints collectors for through curves and curves mesh types surfaces.
Signature
SetFaceConstraintCollectors(facesCons, collectors, consTypes)
Parameters: - facesCons (list of int) – Number of faces on all sides
- collectors (list of
NXOpen.ScCollector
) – Constraints collectors. - consTypes (list of
NXOpen.Features.MeshSurfaceBuilderConstraintType
) – type on each side.
New in version NX4.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
SetFaceConstraintTypes¶
-
MeshSurfaceBuilder.
SetFaceConstraintTypes
¶ Set end constraints types.
Signature
SetFaceConstraintTypes(constraintTypes)
Parameters: constraintTypes (list of NXOpen.Features.MeshSurfaceBuilderConstraintType
) – Constraint typesNew in version NX4.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
SetProfilePointAlignment¶
-
MeshSurfaceBuilder.
SetProfilePointAlignment
¶ Set profile string alignment info.
For each profile string, user needs to spectify the point alignment parameters on segments indexed by align_index along the profile string.
Signature
SetProfilePointAlignment(stringIndex, alignIndex, alignParams)
Parameters: - stringIndex (int) – string index in profile strings
- alignIndex (list of int) – Alignment indices
- alignParams (list of float) – Alignment parameters (normalized)
New in version NX4.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
SetToleranceString¶
-
MeshSurfaceBuilder.
SetToleranceString
¶ Set tolerances strings for mesh type surface.
The strings much match the values.
Signature
SetToleranceString(tolString)
Parameters: tolString (list of str) – Tolerances New in version NX4.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
SetTolerances¶
-
MeshSurfaceBuilder.
SetTolerances
¶ Set tolerances for mesh type surfaces.
Signature
SetTolerances(tol)
Parameters: tol (list of float) – Tolerances New in version NX4.0.0.
License requirements: features_modeling (“FEATURES MODELING”), nx_freeform_1 (“basic freeform modeling”)
Validate¶
-
MeshSurfaceBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.