MathIntegrationBuilder Class¶
-
class
NXOpen.Features.
MathIntegrationBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.MathIntegration
builderTo create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateMathIntegrationBuilder()
Default values.
Property Value Associative 0 AssociativityType None EmbedWorksheet 0 ShowInformationWindow 0 New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
Associative | Returns or sets the associativity of the expression in the feature to the Symbolica or Maple worksheet |
AssociativityType | Returns or sets the option to control associativity to the equation |
EmbedWorksheet | Returns or sets the option to embed worksheet in the feature |
EmbeddedWorksheet | Returns or sets the currently selected embedded worksheet index. |
FileBrowser | Returns or sets the file name returned by the Browser |
Inputs | Returns or sets the number of input expressions |
Location | Returns or sets the source location of the Symbolica or Maple worksheet. |
NativeFileBrowser | Returns or sets the native OS file name returned by the Browser. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
ShowInformationWindow | Returns or sets the option to show the information window |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetExpressions | The array of expressions |
GetFeature | Returns the feature currently being edited by this builder. |
GetMathNames | The array of math names |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetExpressions | Set the expressions in the Math Interface Builder |
SetMathNames | Set the math names corresponding to expressions in the Math Interface Builder |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
MathIntegrationBuilderAssociativityTypes Enumeration | the associativity |
MathIntegrationBuilderLocationTypes Enumeration | The option to specify where the Symbolica or Maple worksheet exists. |
Property Detail¶
Associative¶
-
MathIntegrationBuilder.
Associative
¶ Returns or sets the associativity of the expression in the feature to the Symbolica or Maple worksheet
-------------------------------------
Getter Method
Signature
Associative
Returns: Return type: bool New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Associative
Parameters: associative (bool) – New in version NX12.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
AssociativityType¶
-
MathIntegrationBuilder.
AssociativityType
¶ Returns or sets the option to control associativity to the equation
-------------------------------------
Getter Method
Signature
AssociativityType
Returns: Return type: NXOpen.Features.MathIntegrationBuilderAssociativityTypes
New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AssociativityType
Parameters: associativityType ( NXOpen.Features.MathIntegrationBuilderAssociativityTypes
) –New in version NX12.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
EmbedWorksheet¶
-
MathIntegrationBuilder.
EmbedWorksheet
¶ Returns or sets the option to embed worksheet in the feature
-------------------------------------
Getter Method
Signature
EmbedWorksheet
Returns: Return type: bool New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EmbedWorksheet
Parameters: embedWorksheet (bool) – New in version NX12.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
EmbeddedWorksheet¶
-
MathIntegrationBuilder.
EmbeddedWorksheet
¶ Returns or sets the currently selected embedded worksheet index.
-------------------------------------
Getter Method
Signature
EmbeddedWorksheet
Returns: Return type: int New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EmbeddedWorksheet
Parameters: embeddedWorksheet (int) – New in version NX12.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
FileBrowser¶
-
MathIntegrationBuilder.
FileBrowser
¶ Returns or sets the file name returned by the Browser
-------------------------------------
Getter Method
Signature
FileBrowser
Returns: Return type: str New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FileBrowser
Parameters: filename (str) – New in version NX12.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Inputs¶
-
MathIntegrationBuilder.
Inputs
¶ Returns or sets the number of input expressions
-------------------------------------
Getter Method
Signature
Inputs
Returns: Return type: int New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Inputs
Parameters: numInputExpressions (int) – New in version NX12.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Location¶
-
MathIntegrationBuilder.
Location
¶ Returns or sets the source location of the Symbolica or Maple worksheet.
-------------------------------------
Getter Method
Signature
Location
Returns: Return type: NXOpen.Features.MathIntegrationBuilderLocationTypes
New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Location
Parameters: location ( NXOpen.Features.MathIntegrationBuilderLocationTypes
) –New in version NX12.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
NativeFileBrowser¶
-
MathIntegrationBuilder.
NativeFileBrowser
¶ Returns or sets the native OS file name returned by the Browser.
Used when the session is Teamcenter, but the location is
NXOpen.Features.MathIntegrationBuilderLocationTypes.OperatingSystem
.-------------------------------------
Getter Method
Signature
NativeFileBrowser
Returns: Return type: str New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NativeFileBrowser
Parameters: filename (str) – New in version NX12.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
ShowInformationWindow¶
-
MathIntegrationBuilder.
ShowInformationWindow
¶ Returns or sets the option to show the information window
-------------------------------------
Getter Method
Signature
ShowInformationWindow
Returns: Return type: bool New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShowInformationWindow
Parameters: showInformationWindow (bool) – New in version NX12.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
GetExpressions¶
-
MathIntegrationBuilder.
GetExpressions
¶ The array of expressions
Signature
GetExpressions()
Returns: array of expressions Return type: list of NXOpen.Expression
New in version NX12.0.0.
License requirements: None.
GetMathNames¶
-
MathIntegrationBuilder.
GetMathNames
¶ The array of math names
Signature
GetMathNames()
Returns: array of names Return type: list of str New in version NX12.0.0.
License requirements: None.
SetExpressions¶
-
MathIntegrationBuilder.
SetExpressions
¶ Set the expressions in the Math Interface Builder
Signature
SetExpressions(expressions)
Parameters: expressions (list of NXOpen.Expression
) – array of expressionsNew in version NX12.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SetMathNames¶
-
MathIntegrationBuilder.
SetMathNames
¶ Set the math names corresponding to expressions in the Math Interface Builder
Signature
SetMathNames(names)
Parameters: names (list of str) – array of names New in version NX12.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Validate¶
-
MathIntegrationBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.