MathIntegrationBuilderAssociativityTypes Enumeration¶
NXOpen.Features.MathIntegrationBuilder.AssociativityTypes is an alias for NXOpen.Features.MathIntegrationBuilderAssociativityTypes
-
class
NXOpen.Features.
MathIntegrationBuilderAssociativityTypes
¶ Bases:
object
the associativity
Enum Members
Enum Member Enum Member Description NotSet No associativity to the worksheet New Make associative to the worksheet Existing Maintain associativity to the worksheet -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-