LawExtensionBuilder Class¶
-
class
NXOpen.Features.
LawExtensionBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.LawExtension
builderTo create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateLawExtensionBuilder()
Default values.
Property Value AngleLaw.Function ft AngleLaw.LawType MultiTransition AngleLaw.Parameter t LengthLaw.LawType MultiTransition MergeFacesIfPossible True OppositeSideLengthLaw.LawType MultiTransition Rebuild.Degree 3 Rebuild.RebuildType None New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
AngleLaw | Returns the angle law |
AngleTolerance | Returns or sets the angle tolerance |
BaseProfile | Returns the base profile |
DistanceTolerance | Returns or sets the distance tolerance |
Faces | Returns the faces. |
IsReferenceFaceNormalReversed | Returns or sets a value indicating whether to reverse the reference face normal. |
LengthLaw | Returns the length law |
MergeFacesIfPossible | Returns or sets a value indicating whether to merge the faces if possible |
OppositeSideExtensionOption | Returns or sets the opposite side extension option |
OppositeSideLengthLaw | Returns the opposite side length law. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
Rebuild | Returns the rebuild data. |
Spine | Returns the spine. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Type | Returns or sets the type |
Vector | Returns or sets the vector. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
LawExtensionBuilderOppositeSideExtensionOptions Enumeration | Opposite side extension options |
LawExtensionBuilderTypes Enumeration | Law extension creation types |
Property Detail¶
AngleLaw¶
-
LawExtensionBuilder.
AngleLaw
¶ Returns the angle law
-------------------------------------
Getter Method
Signature
AngleLaw
Returns: Return type: NXOpen.GeometricUtilities.LawBuilder
New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR free_form_modeling (“FREE-FORM MODELING”)
AngleTolerance¶
-
LawExtensionBuilder.
AngleTolerance
¶ Returns or sets the angle tolerance
-------------------------------------
Getter Method
Signature
AngleTolerance
Returns: Return type: float New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR free_form_modeling (“FREE-FORM MODELING”)
-------------------------------------
Setter Method
Signature
AngleTolerance
Parameters: angleTolerance (float) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR free_form_modeling (“FREE-FORM MODELING”)
BaseProfile¶
-
LawExtensionBuilder.
BaseProfile
¶ Returns the base profile
-------------------------------------
Getter Method
Signature
BaseProfile
Returns: Return type: NXOpen.Section
New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR free_form_modeling (“FREE-FORM MODELING”)
DistanceTolerance¶
-
LawExtensionBuilder.
DistanceTolerance
¶ Returns or sets the distance tolerance
-------------------------------------
Getter Method
Signature
DistanceTolerance
Returns: Return type: float New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR free_form_modeling (“FREE-FORM MODELING”)
-------------------------------------
Setter Method
Signature
DistanceTolerance
Parameters: distanceTolerance (float) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR free_form_modeling (“FREE-FORM MODELING”)
Faces¶
-
LawExtensionBuilder.
Faces
¶ Returns the faces.
Faces are used only when
NXOpen.Features.LawExtensionBuilderTypes
isNXOpen.Features.LawExtensionBuilderTypes.Faces
. The faces must be sew able to form a single sheet body. The normal of the sewed sheet body and base profile direction provide local reference co-ordinate system for the orientation of the surface rule lines.-------------------------------------
Getter Method
Signature
Faces
Returns: Return type: NXOpen.ScCollector
New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR free_form_modeling (“FREE-FORM MODELING”)
IsReferenceFaceNormalReversed¶
-
LawExtensionBuilder.
IsReferenceFaceNormalReversed
¶ Returns or sets a value indicating whether to reverse the reference face normal.
When
NXOpen.Features.LawExtensionBuilderTypes
isNXOpen.Features.LawExtensionBuilderTypes.Faces
, the input faces are sewed to form a single sheet body. The normal of the sheet body is decided based on the face which is nearest to the parametric mid point of the base profile and acts as the reference face normal.-------------------------------------
Getter Method
Signature
IsReferenceFaceNormalReversed
Returns: Return type: bool New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR free_form_modeling (“FREE-FORM MODELING”)
-------------------------------------
Setter Method
Signature
IsReferenceFaceNormalReversed
Parameters: reverseNormal (bool) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR free_form_modeling (“FREE-FORM MODELING”)
LengthLaw¶
-
LawExtensionBuilder.
LengthLaw
¶ Returns the length law
-------------------------------------
Getter Method
Signature
LengthLaw
Returns: Return type: NXOpen.GeometricUtilities.LawBuilder
New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR free_form_modeling (“FREE-FORM MODELING”)
MergeFacesIfPossible¶
-
LawExtensionBuilder.
MergeFacesIfPossible
¶ Returns or sets a value indicating whether to merge the faces if possible
-------------------------------------
Getter Method
Signature
MergeFacesIfPossible
Returns: Return type: bool New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR free_form_modeling (“FREE-FORM MODELING”)
-------------------------------------
Setter Method
Signature
MergeFacesIfPossible
Parameters: mergeFacesIfPossible (bool) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR free_form_modeling (“FREE-FORM MODELING”)
OppositeSideExtensionOption¶
-
LawExtensionBuilder.
OppositeSideExtensionOption
¶ Returns or sets the opposite side extension option
-------------------------------------
Getter Method
Signature
OppositeSideExtensionOption
Returns: Return type: NXOpen.Features.LawExtensionBuilderOppositeSideExtensionOptions
New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR free_form_modeling (“FREE-FORM MODELING”)
-------------------------------------
Setter Method
Signature
OppositeSideExtensionOption
Parameters: oppositeSideExtension ( NXOpen.Features.LawExtensionBuilderOppositeSideExtensionOptions
) –New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR free_form_modeling (“FREE-FORM MODELING”)
OppositeSideLengthLaw¶
-
LawExtensionBuilder.
OppositeSideLengthLaw
¶ Returns the opposite side length law.
Opposite side extension law is required only when
NXOpen.Features.LawExtensionBuilderOppositeSideExtensionOptions
isNXOpen.Features.LawExtensionBuilderOppositeSideExtensionOptions.Asymmetric
-------------------------------------
Getter Method
Signature
OppositeSideLengthLaw
Returns: Return type: NXOpen.GeometricUtilities.LawBuilder
New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR free_form_modeling (“FREE-FORM MODELING”)
Rebuild¶
-
LawExtensionBuilder.
Rebuild
¶ Returns the rebuild data.
This data is used to rebuild the surface in the base profile direction.
-------------------------------------
Getter Method
Signature
Rebuild
Returns: Return type: NXOpen.GeometricUtilities.Rebuild
New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR free_form_modeling (“FREE-FORM MODELING”)
Spine¶
-
LawExtensionBuilder.
Spine
¶ Returns the spine.
Spine is optional
-------------------------------------
Getter Method
Signature
Spine
Returns: Return type: NXOpen.Section
New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR free_form_modeling (“FREE-FORM MODELING”)
Type¶
-
LawExtensionBuilder.
Type
¶ Returns or sets the type
-------------------------------------
Getter Method
Signature
Type
Returns: Return type: NXOpen.Features.LawExtensionBuilderTypes
New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR free_form_modeling (“FREE-FORM MODELING”)
-------------------------------------
Setter Method
Signature
Type
Parameters: type ( NXOpen.Features.LawExtensionBuilderTypes
) –New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR free_form_modeling (“FREE-FORM MODELING”)
Vector¶
-
LawExtensionBuilder.
Vector
¶ Returns or sets the vector.
Vector is used only when
NXOpen.Features.LawExtensionBuilderTypes
isNXOpen.Features.LawExtensionBuilderTypes.Vector
-------------------------------------
Getter Method
Signature
Vector
Returns: Return type: NXOpen.Direction
New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR free_form_modeling (“FREE-FORM MODELING”)
-------------------------------------
Setter Method
Signature
Vector
Parameters: vector ( NXOpen.Direction
) –New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR free_form_modeling (“FREE-FORM MODELING”)
Method Detail¶
Validate¶
-
LawExtensionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.