JoinCurvesBuilder Class¶
-
class
NXOpen.Features.
JoinCurvesBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.JoinCurves
builder.To create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateJoinCurvesBuilder()
Default values.
Property Value OutputCurveType General New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
AngleTolerance | Returns or sets the angle tolerance. |
CurveOptions | Returns the Curve Options. |
DistanceTolerance | Returns or sets the distance tolerance. |
MaximumDegree | Returns or sets the maximum degree of the advanced spline output. |
MaximumSegments | Returns or sets the maximum number of segments of the advanced spline output. |
OutputCurveType | Returns or sets the output curve type. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
Section | Returns the section that collects the input curves that are to be joined. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
JoinCurvesBuilderOutputCurve Enumeration | Represents the output curve type. |
Property Detail¶
AngleTolerance¶
-
JoinCurvesBuilder.
AngleTolerance
¶ Returns or sets the angle tolerance.
This tolerance is used while creating the joined curve. The same tolerance is also applied to the section.
-------------------------------------
Getter Method
Signature
AngleTolerance
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AngleTolerance
Parameters: angleTolerance (float) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
CurveOptions¶
-
JoinCurvesBuilder.
CurveOptions
¶ Returns the Curve Options.
This object contains the data about the associativity and corresponding action on the input curves. A feature is created only if the associativity is switched ON and the input curves can not be deleted or replaced.
-------------------------------------
Getter Method
Signature
CurveOptions
Returns: Curve Options Return type: NXOpen.GeometricUtilities.CurveOptions
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
DistanceTolerance¶
-
JoinCurvesBuilder.
DistanceTolerance
¶ Returns or sets the distance tolerance.
This tolerance is used while creating the joined curve. The same tolerance is also applied to the section.
-------------------------------------
Getter Method
Signature
DistanceTolerance
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DistanceTolerance
Parameters: distanceTolerance (float) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
MaximumDegree¶
-
JoinCurvesBuilder.
MaximumDegree
¶ Returns or sets the maximum degree of the advanced spline output.
This integer is only used in cases where the output curve option is set to advanced type.
-------------------------------------
Getter Method
Signature
MaximumDegree
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MaximumDegree
Parameters: maximumDegree (int) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
MaximumSegments¶
-
JoinCurvesBuilder.
MaximumSegments
¶ Returns or sets the maximum number of segments of the advanced spline output.
This integer is only used in cases where the output curve option is set to advanced type.
-------------------------------------
Getter Method
Signature
MaximumSegments
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MaximumSegments
Parameters: maximumSegments (int) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
OutputCurveType¶
-
JoinCurvesBuilder.
OutputCurveType
¶ Returns or sets the output curve type.
If the output curve type is advaned, the maximum degree for output spline and maximum number of segments should also be provided.
-------------------------------------
Getter Method
Signature
OutputCurveType
Returns: Return type: NXOpen.Features.JoinCurvesBuilderOutputCurve
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OutputCurveType
Parameters: outputCurveType ( NXOpen.Features.JoinCurvesBuilderOutputCurve
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
Section¶
-
JoinCurvesBuilder.
Section
¶ Returns the section that collects the input curves that are to be joined.
Multiple loops or self intersecting curves should not be added to the section.
-------------------------------------
Getter Method
Signature
Section
Returns: Return type: NXOpen.Section
New in version NX5.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
JoinCurvesBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.