JoinCurvesBuilderOutputCurve Enumeration

NXOpen.Features.JoinCurvesBuilder.OutputCurve is an alias for NXOpen.Features.JoinCurvesBuilderOutputCurve

class NXOpen.Features.JoinCurvesBuilderOutputCurve

Bases: object

Represents the output curve type.

Enum Members

Enum Member Enum Member Description
General General output curve
Cubic Cubic output curve
Quintic Quintic output curve
Advanced Advanced output curve
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.