GeneralConicBuilder Class¶
-
class
NXOpen.Features.
GeneralConicBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.GeneralConic
builderTo create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateGeneralConicBuilder()
Default values.
Property Value DrawingPlaneOption View Extender.EndExtensionOption None Extender.EndValue.Value 0 (millimeters part), 0 (inches part) Extender.StartExtensionOption None Extender.StartValue.Value 0 (millimeters part), 0 (inches part) PlaneConstrainedToggle 0 RhoValue 0.5 ValueA 1.0 ValueB 0.0 ValueC 1.0 ValueD 0.0 ValueE 0.0 ValueF -1.0 New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
AnchorPoint | Returns or sets the anchor point. |
AssociativeToggle | Returns or sets the associative toggle |
CoefficientCSYS | Returns or sets the coefficient type coordinate system. |
ConstrainedPlaneCSYS | Returns or sets the constrained plane. |
DrawingPlaneOption | Returns or sets the drawing plane. |
EndPoint | Returns or sets the end point. |
Extender | Returns the extension option |
GeneralDrawingPlane | Returns or sets the specify plane. |
InteriorPoint1 | Returns or sets the first interior point. |
InteriorPoint2 | Returns or sets the second interior point. |
InteriorPoint3 | Returns or sets the third interior point. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
PlaneConstrainedToggle | Returns or sets the plane constrained toggle. |
RhoValue | Returns or sets the rho value. |
SlopeAtEndPoint | Returns or sets the slope at end point. |
SlopeAtStartPoint | Returns or sets the slope at start point. |
StartPoint | Returns or sets the start point. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Type | Returns or sets the conic creation type. |
ValueA | Returns or sets the coefficient value for a. |
ValueB | Returns or sets the coefficient value for b. |
ValueC | Returns or sets the coefficient value for c. |
ValueD | Returns or sets the coefficient value for d. |
ValueE | Returns or sets the coefficient value for e. |
ValueF | Returns or sets the coefficient value for f. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
Evaluate | Evaluates the curve. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
GeneralConicBuilderDrawingPlaneOptions Enumeration | Drawing Plane options. |
GeneralConicBuilderTypes Enumeration | General Conic Types. |
Property Detail¶
AnchorPoint¶
-
GeneralConicBuilder.
AnchorPoint
¶ Returns or sets the anchor point.
Used by
Types.ThreePointsAnchor
Types.TwoPointsAnchorRho
-------------------------------------
Getter Method
Signature
AnchorPoint
Returns: Return type: NXOpen.Point
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AnchorPoint
Parameters: anchorPoint ( NXOpen.Point
) –New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)
AssociativeToggle¶
-
GeneralConicBuilder.
AssociativeToggle
¶ Returns or sets the associative toggle
-------------------------------------
Getter Method
Signature
AssociativeToggle
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AssociativeToggle
Parameters: associativeToggle (bool) – New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)
CoefficientCSYS¶
-
GeneralConicBuilder.
CoefficientCSYS
¶ Returns or sets the coefficient type coordinate system.
Only used by
Types.Coefficients
-------------------------------------
Getter Method
Signature
CoefficientCSYS
Returns: Return type: NXOpen.CoordinateSystem
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CoefficientCSYS
Parameters: coefficientCSYS ( NXOpen.CoordinateSystem
) –New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)
ConstrainedPlaneCSYS¶
-
GeneralConicBuilder.
ConstrainedPlaneCSYS
¶ Returns or sets the constrained plane.
Used by point types. Enabled by
PlaneConstrainedToggle`()
.-------------------------------------
Getter Method
Signature
ConstrainedPlaneCSYS
Returns: Return type: NXOpen.CoordinateSystem
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ConstrainedPlaneCSYS
Parameters: constrainedPlaneCSYS ( NXOpen.CoordinateSystem
) –New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)
DrawingPlaneOption¶
-
GeneralConicBuilder.
DrawingPlaneOption
¶ Returns or sets the drawing plane.
Used by point types. Disabled by
PlaneConstrainedToggle`()
.-------------------------------------
Getter Method
Signature
DrawingPlaneOption
Returns: Return type: NXOpen.Features.GeneralConicBuilderDrawingPlaneOptions
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DrawingPlaneOption
Parameters: drawingPlaneOption ( NXOpen.Features.GeneralConicBuilderDrawingPlaneOptions
) –New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)
EndPoint¶
-
GeneralConicBuilder.
EndPoint
¶ Returns or sets the end point.
Used by all point types
-------------------------------------
Getter Method
Signature
EndPoint
Returns: Return type: NXOpen.Point
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndPoint
Parameters: endPoint ( NXOpen.Point
) –New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)
Extender¶
-
GeneralConicBuilder.
Extender
¶ Returns the extension option
-------------------------------------
Getter Method
Signature
Extender
Returns: Return type: NXOpen.GeometricUtilities.CurveExtensionBuilder
New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)
GeneralDrawingPlane¶
-
GeneralConicBuilder.
GeneralDrawingPlane
¶ Returns or sets the specify plane.
Used by point types. Disabled by
PlaneConstrainedToggle`()
.-------------------------------------
Getter Method
Signature
GeneralDrawingPlane
Returns: Return type: NXOpen.Plane
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
GeneralDrawingPlane
Parameters: generalDrawingPlane ( NXOpen.Plane
) –New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)
InteriorPoint1¶
-
GeneralConicBuilder.
InteriorPoint1
¶ Returns or sets the first interior point.
Used by
Types.FivePoints
Types.FourPointsOneSlope
Types. ThreePointsTwoSlopes
Types.ThreePointsAnchor
-------------------------------------
Getter Method
Signature
InteriorPoint1
Returns: Return type: NXOpen.Point
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InteriorPoint1
Parameters: interiorPoint1 ( NXOpen.Point
) –New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)
InteriorPoint2¶
-
GeneralConicBuilder.
InteriorPoint2
¶ Returns or sets the second interior point.
Used by
Types.FivePoints
Types.FourPointsOneSlope
-------------------------------------
Getter Method
Signature
InteriorPoint2
Returns: Return type: NXOpen.Point
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InteriorPoint2
Parameters: interiorPoint2 ( NXOpen.Point
) –New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)
InteriorPoint3¶
-
GeneralConicBuilder.
InteriorPoint3
¶ Returns or sets the third interior point.
Used by
Types.FivePoints
-------------------------------------
Getter Method
Signature
InteriorPoint3
Returns: Return type: NXOpen.Point
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InteriorPoint3
Parameters: interiorPoint3 ( NXOpen.Point
) –New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)
PlaneConstrainedToggle¶
-
GeneralConicBuilder.
PlaneConstrainedToggle
¶ Returns or sets the plane constrained toggle.
Used by point types. Enables
ConstrainedPlaneCSYS`()
. DisablesNXOpen.Features.PolylineBuilderDrawingPlaneOptions
andGeneralDrawingPlane`()
.-------------------------------------
Getter Method
Signature
PlaneConstrainedToggle
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PlaneConstrainedToggle
Parameters: planeConstrainedToggle (bool) – New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)
RhoValue¶
-
GeneralConicBuilder.
RhoValue
¶ Returns or sets the rho value.
Used by
Types.TwoPointsAnchorRho
Types.TwoPointsTwoSlopesRho
-------------------------------------
Getter Method
Signature
RhoValue
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RhoValue
Parameters: rhoValue (float) – New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)
SlopeAtEndPoint¶
-
GeneralConicBuilder.
SlopeAtEndPoint
¶ Returns or sets the slope at end point.
Used by
Types.ThreePointsTwoSlopes
Types.TwoPointsTwoSlopesRho
-------------------------------------
Getter Method
Signature
SlopeAtEndPoint
Returns: Return type: NXOpen.Direction
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SlopeAtEndPoint
Parameters: slopeAtEndPoint ( NXOpen.Direction
) –New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)
SlopeAtStartPoint¶
-
GeneralConicBuilder.
SlopeAtStartPoint
¶ Returns or sets the slope at start point.
Used by
Types.FourPointsOneSlope
Types.ThreePointsTwoSlopes
Types.TwoPointsTwoSlopesRho
-------------------------------------
Getter Method
Signature
SlopeAtStartPoint
Returns: Return type: NXOpen.Direction
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SlopeAtStartPoint
Parameters: slopeAtStartPoint ( NXOpen.Direction
) –New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)
StartPoint¶
-
GeneralConicBuilder.
StartPoint
¶ Returns or sets the start point.
Used by all point types
-------------------------------------
Getter Method
Signature
StartPoint
Returns: Return type: NXOpen.Point
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StartPoint
Parameters: startPoint ( NXOpen.Point
) –New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)
Type¶
-
GeneralConicBuilder.
Type
¶ Returns or sets the conic creation type.
See
NXOpen.Features.SewBuilderTypes
-------------------------------------
Getter Method
Signature
Type
Returns: Return type: NXOpen.Features.GeneralConicBuilderTypes
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type
Parameters: type ( NXOpen.Features.GeneralConicBuilderTypes
) –New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)
ValueA¶
-
GeneralConicBuilder.
ValueA
¶ Returns or sets the coefficient value for a.
Only used by
Types.Coefficients
-------------------------------------
Getter Method
Signature
ValueA
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ValueA
Parameters: valueA (float) – New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)
ValueB¶
-
GeneralConicBuilder.
ValueB
¶ Returns or sets the coefficient value for b.
Only used by
Types.Coefficients
-------------------------------------
Getter Method
Signature
ValueB
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ValueB
Parameters: valueB (float) – New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)
ValueC¶
-
GeneralConicBuilder.
ValueC
¶ Returns or sets the coefficient value for c.
Only used by
Types.Coefficients
-------------------------------------
Getter Method
Signature
ValueC
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ValueC
Parameters: valueC (float) – New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)
ValueD¶
-
GeneralConicBuilder.
ValueD
¶ Returns or sets the coefficient value for d.
Only used by
Types.Coefficients
-------------------------------------
Getter Method
Signature
ValueD
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ValueD
Parameters: valueD (float) – New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)
ValueE¶
-
GeneralConicBuilder.
ValueE
¶ Returns or sets the coefficient value for e.
Only used by
Types.Coefficients
-------------------------------------
Getter Method
Signature
ValueE
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ValueE
Parameters: valueE (float) – New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)
ValueF¶
-
GeneralConicBuilder.
ValueF
¶ Returns or sets the coefficient value for f.
Only used by
Types.Coefficients
-------------------------------------
Getter Method
Signature
ValueF
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ValueF
Parameters: valueF (float) – New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)
Method Detail¶
Evaluate¶
-
GeneralConicBuilder.
Evaluate
¶ Evaluates the curve.
Does not call update. Used to preview results.
Signature
Evaluate()
New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)
Validate¶
-
GeneralConicBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.