GeneralConicBuilderTypes Enumeration¶
NXOpen.Features.GeneralConicBuilder.Types is an alias for NXOpen.Features.GeneralConicBuilderTypes
-
class
NXOpen.Features.
GeneralConicBuilderTypes
¶ Bases:
object
General Conic Types. There are several creation methods available. All except the
Types.Coefficients
type require setting points/slopes.Enum Members
Enum Member Enum Member Description FivePoints Five points, no slopes, no anchor, no rho value FourPointsOneSlope Four points, one slope, no anchor, no rho value ThreePointsTwoSlopes Three points, two slopes, no anchor, no rho value ThreePointsAnchor Three points, no slopes, anchor, no rho value TwoPointsAnchorRho Two points, no slopes, anchor, rho value TwoPointsTwoSlopesRho Two points, two slopes, no anchor, rho value Coefficients Coefficient values and CoefficientCSYS`()
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-