FlowBlendBuilder Class¶
-
class
NXOpen.Features.
FlowBlendBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.FlowBlend
builderTo create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateFlowBlendBuilder()
Default values.
Property Value Patch 1 Trim (deprecated) 0 New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
ControlPoint | Returns the control point object |
EdgeToBlend | Returns the edge to blend |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
Patch | Returns or sets the toggle to specify patch to body or not |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SmoothRange | Returns the smooth range object |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Tolerance | Returns or sets the tolerance |
Trim | Returns or sets the toggle to specify trim input faces or not |
TrimInputFacesToExtendedRail | Returns or sets the patch trim option |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
NewControlPoint | The control point object’s create function |
NewSmoothRange | The smooth range object’s create function |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ControlPoint¶
-
FlowBlendBuilder.
ControlPoint
¶ Returns the control point object
-------------------------------------
Getter Method
Signature
ControlPoint
Returns: Return type: NXOpen.Features.VariableRadiusPointsBuilderList
New in version NX10.0.0.
License requirements: None.
EdgeToBlend¶
-
FlowBlendBuilder.
EdgeToBlend
¶ Returns the edge to blend
-------------------------------------
Getter Method
Signature
EdgeToBlend
Returns: Return type: NXOpen.ScCollector
New in version NX10.0.0.
License requirements: None.
Patch¶
-
FlowBlendBuilder.
Patch
¶ Returns or sets the toggle to specify patch to body or not
-------------------------------------
Getter Method
Signature
Patch
Returns: Return type: bool New in version NX10.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
Patch
Parameters: patch (bool) – New in version NX10.0.1.
License requirements: solid_modeling (“SOLIDS MODELING”)
SmoothRange¶
-
FlowBlendBuilder.
SmoothRange
¶ Returns the smooth range object
-------------------------------------
Getter Method
Signature
SmoothRange
Returns: Return type: NXOpen.Features.SmoothRangeBuilderList
New in version NX10.0.0.
License requirements: None.
Tolerance¶
-
FlowBlendBuilder.
Tolerance
¶ Returns or sets the tolerance
-------------------------------------
Getter Method
Signature
Tolerance
Returns: Return type: float New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Tolerance
Parameters: tolerance (float) – New in version NX10.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Trim¶
-
FlowBlendBuilder.
Trim
¶ Returns or sets the toggle to specify trim input faces or not
-------------------------------------
Getter Method
Signature
Trim
Returns: Return type: bool New in version NX10.0.0.
Deprecated since version NX10.0.1: This functionality is no longer supported.
License requirements: None.
-------------------------------------
Setter Method
Signature
Trim
Parameters: trim (bool) – New in version NX10.0.0.
Deprecated since version NX10.0.1: This functionality is no longer supported.
License requirements: solid_modeling (“SOLIDS MODELING”)
TrimInputFacesToExtendedRail¶
-
FlowBlendBuilder.
TrimInputFacesToExtendedRail
¶ Returns or sets the patch trim option
-------------------------------------
Getter Method
Signature
TrimInputFacesToExtendedRail
Returns: Return type: bool New in version NX11.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
TrimInputFacesToExtendedRail
Parameters: trimInputFacesToExtendedRail (bool) – New in version NX11.0.1.
License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
NewControlPoint¶
-
FlowBlendBuilder.
NewControlPoint
¶ The control point object’s create function
Signature
NewControlPoint()
Returns: Return type: NXOpen.Features.VariableRadiusPointsBuilder
New in version NX10.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
NewSmoothRange¶
-
FlowBlendBuilder.
NewSmoothRange
¶ The smooth range object’s create function
Signature
NewSmoothRange()
Returns: Return type: NXOpen.Features.SmoothRangeBuilder
New in version NX10.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Validate¶
-
FlowBlendBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.