FeatureGroup Class¶
-
class
NXOpen.Features.
FeatureGroup
¶ Bases:
NXOpen.Features.Feature
Represents a
NXOpen.Features.FeatureGroup
Not support KF.
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
AlgorithmVersion | Returns the algorithm version of the feature |
AllowDeleteMembers | Returns or sets the allow delete members flag of features group. |
ContainerFeature | Returns the container feature for this feature. |
FeatureType | Returns the feature type |
IsContainedFeature | Returns true if the feature is a contained feature. |
IsInternal | Returns true if the feature is internal. |
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Location | Returns the location of the feature |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
Suppressed | Returns the suppression status of the feature |
Tag | Returns the Tag for this object. |
Timestamp | Returns the timestamp of the feature |
Methods¶
Method | Description |
---|---|
AddMembersWithRelocation | Adds given features into feature group. |
BreakWaveLink | Break Wave Link Feature |
ChangeBooleanType | Change Boolean Type |
CreateAttributeIterator | Create an attribute iterator |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteClueAlerts | Delete all clue alerts from the features |
DeleteHintAlerts | Delete all clue alerts from the features |
DeleteInformationalAlerts | Delete all informational alerts from the features |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
DeleteWarningAlerts | Delete all warning alerts from the features |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAllChildren | Returns all immediate child features. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetChildren | Returns the immediate child features. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetEntities | Returns the entities created by the feature. |
GetExpressions | Returns the expressions created by the feature. |
GetFeatureClueHintMessages | Returns both clue and hint messages of the feature. |
GetFeatureClueMessages | Returns the feature clue messages. |
GetFeatureColor | The feature color |
GetFeatureErrorMessages | Returns the feature error messages. |
GetFeatureGroupType | Gets the feaure group type. |
GetFeatureHintMessages | Returns the feature hint messages. |
GetFeatureInformationalMessages | Returns the feature informational messages. |
GetFeatureName | Returns the displayed name of the feature. |
GetFeatureWarningMessages | Returns the feature warning messages. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetMembers | Gets the members of feature group. |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetParents | Returns the immediate parent features. |
GetPdmReferenceAttributeValue | Gets the value of PDM Reference attribute for given object. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetSections | Queries a feature for list of its sections. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator |
HideBody | Hide the body created by the feature |
HideParents | Hide the body created by the parent feature |
Highlight | Highlight the body created by the feature |
LogDiagnostic | Log a diagnostic alert for this feature |
MakeCurrentFeature | Make current feature |
MakeSketchExternal | Make the parent sketch external for reuse by other features. |
MakeSketchInternal | Make the parent sketch internal if referenced only by this feature. |
MakeTimestampsConsecutive | Try to make timestamps of members of feature group consecutive. |
MakeTimestampsSequential | Try to make timestamps of members of feature group sequential. |
NewAddMembers | Adds given features into feature group. |
NewRemoveMembers | Removes given features from the feature group. |
Prints a representation of this object to the system log file. | |
RemoveAllMembers | Removes all features from the feature group. |
RemoveForEdit | Remove all the feature faces before a NoHistory mode edit. |
RemoveParameters | Remove Local feature parameters in history free mode. |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetFeatureGroupType | Sets the feaure group type. |
SetGroupActive | Set a feature group as active group. |
SetName | Sets the custom name of the object. |
SetPdmReferenceAttribute | Sets the value of PDM Reference attribute on the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
ShowBody | Show the body created by the feature. |
ShowDimensions | Show all feature dimensions of a feature. |
ShowParents | Show the body created by the parent feature. |
Suppress | Suppress the feature |
Unhighlight | Unhighlight the body created by the feature |
Unsuppress | Unsuppress the feature |
Enumerations¶
FeatureGroupType Enumeration | Feature group type. |
Property Detail¶
AllowDeleteMembers¶
-
FeatureGroup.
AllowDeleteMembers
¶ Returns or sets the allow delete members flag of features group.
-------------------------------------
Getter Method
Signature
AllowDeleteMembers
Returns: Allow delete members flag Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AllowDeleteMembers
Parameters: allowDeleteMembers (bool) – Allow delete members flag New in version NX7.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
IsOccurrence¶
-
FeatureGroup.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
FeatureGroup.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
FeatureGroup.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
FeatureGroup.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
FeatureGroup.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
FeatureGroup.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Method Detail¶
AddMembersWithRelocation¶
-
FeatureGroup.
AddMembersWithRelocation
¶ Adds given features into feature group.
Signature
AddMembersWithRelocation(members, reorderTimestamp, updateRelocatedFeatures)
Parameters: - members (list of
NXOpen.Features.Feature
) – Features array - reorderTimestamp (bool) – Allow reorder member features in order to make members sequential
- updateRelocatedFeatures (bool) – Allow update features when members are made sequential
New in version NX8.5.1.
License requirements: solid_modeling (“SOLIDS MODELING”)
- members (list of
FindObject¶
-
FeatureGroup.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetFeatureGroupType¶
-
FeatureGroup.
GetFeatureGroupType
¶ Gets the feaure group type.
Signature
GetFeatureGroupType()
Returns: Feature group type Return type: NXOpen.Features.FeatureGroupType
New in version NX7.5.0.
License requirements: None.
GetMembers¶
-
FeatureGroup.
GetMembers
¶ Gets the members of feature group.
Signature
GetMembers()
Returns: Features array Return type: list of NXOpen.Features.Feature
New in version NX7.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
MakeTimestampsConsecutive¶
-
FeatureGroup.
MakeTimestampsConsecutive
¶ Try to make timestamps of members of feature group consecutive.
Signature
MakeTimestampsConsecutive()
New in version NX7.5.3.
Deprecated since version NX8.5.1: Use
NXOpen.Features.FeatureGroup.MakeTimestampsSequential()
instead.License requirements: solid_modeling (“SOLIDS MODELING”)
MakeTimestampsSequential¶
-
FeatureGroup.
MakeTimestampsSequential
¶ Try to make timestamps of members of feature group sequential.
Signature
MakeTimestampsSequential(updateRelocatedFeatures)
Parameters: updateRelocatedFeatures (bool) – Update features when feature group is made sequential New in version NX8.5.1.
License requirements: solid_modeling (“SOLIDS MODELING”)
NewAddMembers¶
-
FeatureGroup.
NewAddMembers
¶ Adds given features into feature group.
Signature
NewAddMembers(members, reorderTimestamp)
Parameters: - members (list of
NXOpen.Features.Feature
) – Features array - reorderTimestamp (bool) – Allow reorder member feature in order to make members sequential
New in version NX7.5.3.
Deprecated since version NX8.5.1: Use
NXOpen.Features.FeatureGroup.AddMembersWithRelocation()
instead.License requirements: solid_modeling (“SOLIDS MODELING”)
- members (list of
NewRemoveMembers¶
-
FeatureGroup.
NewRemoveMembers
¶ Removes given features from the feature group.
If reorderTimestamp flag is ture, timestamp of remain member features will be made sequential.
Signature
NewRemoveMembers(members, reorderTimestamp)
Parameters: - members (list of
NXOpen.Features.Feature
) – Features array - reorderTimestamp (bool) – Allow reorder member feature in order to make residual members sequential
New in version NX7.5.3.
License requirements: solid_modeling (“SOLIDS MODELING”)
- members (list of
Print¶
-
FeatureGroup.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
RemoveAllMembers¶
-
FeatureGroup.
RemoveAllMembers
¶ Removes all features from the feature group.
Signature
RemoveAllMembers()
New in version NX7.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SetFeatureGroupType¶
-
FeatureGroup.
SetFeatureGroupType
¶ Sets the feaure group type.
Signature
SetFeatureGroupType(type)
Parameters: type ( NXOpen.Features.FeatureGroupType
) – Feature group typeNew in version NX7.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SetName¶
-
FeatureGroup.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.