CurveOnSurfaceBuilder Class¶
-
class
NXOpen.Features.
CurveOnSurfaceBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Curve On Surface builder class.
To create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateCurveOnSurfaceBuilder()
Default values.
Property Value CurveFitData.CurveJoinMethod No CurveFitData.Degree 7 CurveFitData.FitMethod DegreeAndSegments CurveFitData.IsAdvancedFit 0 CurveFitData.IsAlignShape 0 CurveFitData.MaximumDegree 7 CurveFitData.MaximumSegments 1 CurveFitData.MinimumDegree 5 CurveFitData.Segments 1 CurveFitProperties.FitOption Cubic CurveFitProperties.MaximumDegree 7 CurveFitProperties.MaximumSegments 1 New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
AngleTolerance | Returns or sets the angle tolerance |
ConstraintManager | Returns the constraint manager |
CurveFitData | Returns the curve fitting parameters |
CurveFitProperties | Returns the curve fit properties |
DistanceTolerance | Returns or sets the distance tolerance |
Faces | Returns the face collector |
IsPeriodic | Returns or sets the periodicity state of curve on surface |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AngleTolerance¶
-
CurveOnSurfaceBuilder.
AngleTolerance
¶ Returns or sets the angle tolerance
-------------------------------------
Getter Method
Signature
AngleTolerance
Returns: Return type: float New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
-------------------------------------
Setter Method
Signature
AngleTolerance
Parameters: angleTolerance (float) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
ConstraintManager¶
-
CurveOnSurfaceBuilder.
ConstraintManager
¶ Returns the constraint manager
-------------------------------------
Getter Method
Signature
ConstraintManager
Returns: Return type: NXOpen.Features.GeometricConstraintDataManager
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
CurveFitData¶
-
CurveOnSurfaceBuilder.
CurveFitData
¶ Returns the curve fitting parameters
-------------------------------------
Getter Method
Signature
CurveFitData
Returns: Return type: NXOpen.GeometricUtilities.CurveFitData
New in version NX8.5.0.
License requirements: None.
CurveFitProperties¶
-
CurveOnSurfaceBuilder.
CurveFitProperties
¶ Returns the curve fit properties
-------------------------------------
Getter Method
Signature
CurveFitProperties
Returns: Return type: NXOpen.GeometricUtilities.CurveFitOptions
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
DistanceTolerance¶
-
CurveOnSurfaceBuilder.
DistanceTolerance
¶ Returns or sets the distance tolerance
-------------------------------------
Getter Method
Signature
DistanceTolerance
Returns: Return type: float New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
-------------------------------------
Setter Method
Signature
DistanceTolerance
Parameters: distanceTolerance (float) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Faces¶
-
CurveOnSurfaceBuilder.
Faces
¶ Returns the face collector
-------------------------------------
Getter Method
Signature
Faces
Returns: Return type: NXOpen.ScCollector
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
IsPeriodic¶
-
CurveOnSurfaceBuilder.
IsPeriodic
¶ Returns or sets the periodicity state of curve on surface
-------------------------------------
Getter Method
Signature
IsPeriodic
Returns: Return type: bool New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
-------------------------------------
Setter Method
Signature
IsPeriodic
Parameters: periodicity (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
Validate¶
-
CurveOnSurfaceBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.