BlendCornerBuilder Class¶
-
class
NXOpen.Features.
BlendCornerBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.BlendCorner
builder.To create a new instance of this class, use
NXOpen.Features.FreeformSurfaceCollection.CreateBlendCornerBuilder()
Default values.
Property Value AllowTransitionCurveOnBlends 1 Continuity G1 Fullness.Value 0 (millimeters part), 0 (inches part) SewToBody 1 UseCenterPoint 0 New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
AllowTransitionCurveOnBlends | Returns or sets the transition curve on blend faces |
AngleTolerance | Returns or sets the angle tolerance. |
CenterPoint | Returns or sets the center point. |
Continuity | Returns or sets the continuity type |
DistanceTolerance | Returns or sets the distance tolerance. |
Fullness | Returns the fullness value. |
LimitCurveList | Returns the limit curve list |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SewToBody | Returns or sets the sew to body |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
TransitionCurveList | Returns the transition curve list |
UseCenterPoint | Returns or sets the use center point flag. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
CreateBlendSetbackBuilder | Create a blend setback builder object. |
CreateTransitionCurveBuilder | Create a transition curve data builder object. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
BlendCornerBuilderContinuityTypes Enumeration | Continuity options |
Property Detail¶
AllowTransitionCurveOnBlends¶
-
BlendCornerBuilder.
AllowTransitionCurveOnBlends
¶ Returns or sets the transition curve on blend faces
-------------------------------------
Getter Method
Signature
AllowTransitionCurveOnBlends
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AllowTransitionCurveOnBlends
Parameters: allow (bool) – New in version NX9.0.0.
License requirements: nx_freeform_2 (“advanced freeform modeling”)
AngleTolerance¶
-
BlendCornerBuilder.
AngleTolerance
¶ Returns or sets the angle tolerance.
It will be used to control the tangency of the curves and corner surface
-------------------------------------
Getter Method
Signature
AngleTolerance
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AngleTolerance
Parameters: angleTolerance (float) – New in version NX9.0.0.
License requirements: nx_freeform_2 (“advanced freeform modeling”)
CenterPoint¶
-
BlendCornerBuilder.
CenterPoint
¶ Returns or sets the center point.
The corner patch will pass through the center point.
-------------------------------------
Getter Method
Signature
CenterPoint
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CenterPoint
Parameters: centerPoint ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: nx_freeform_2 (“advanced freeform modeling”)
Continuity¶
-
BlendCornerBuilder.
Continuity
¶ Returns or sets the continuity type
-------------------------------------
Getter Method
Signature
Continuity
Returns: Return type: NXOpen.Features.BlendCornerBuilderContinuityTypes
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Continuity
Parameters: continuity ( NXOpen.Features.BlendCornerBuilderContinuityTypes
) –New in version NX9.0.0.
License requirements: nx_freeform_2 (“advanced freeform modeling”)
DistanceTolerance¶
-
BlendCornerBuilder.
DistanceTolerance
¶ Returns or sets the distance tolerance.
It will be used to control the precision of curves and corner surface
-------------------------------------
Getter Method
Signature
DistanceTolerance
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DistanceTolerance
Parameters: distanceTolerance (float) – New in version NX9.0.0.
License requirements: nx_freeform_2 (“advanced freeform modeling”)
Fullness¶
-
BlendCornerBuilder.
Fullness
¶ Returns the fullness value.
It is an offset distance of the center point from the default position when the center point control is off.
-------------------------------------
Getter Method
Signature
Fullness
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
LimitCurveList¶
-
BlendCornerBuilder.
LimitCurveList
¶ Returns the limit curve list
-------------------------------------
Getter Method
Signature
LimitCurveList
Returns: Return type: NXOpen.GeometricUtilities.BlendSetbackBuilderList
New in version NX9.0.0.
License requirements: None.
SewToBody¶
-
BlendCornerBuilder.
SewToBody
¶ Returns or sets the sew to body
-------------------------------------
Getter Method
Signature
SewToBody
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SewToBody
Parameters: sewToBody (bool) – New in version NX9.0.0.
License requirements: nx_freeform_2 (“advanced freeform modeling”)
TransitionCurveList¶
-
BlendCornerBuilder.
TransitionCurveList
¶ Returns the transition curve list
-------------------------------------
Getter Method
Signature
TransitionCurveList
Returns: Return type: NXOpen.GeometricUtilities.TransitionCurveBuilderList
New in version NX9.0.0.
License requirements: None.
UseCenterPoint¶
-
BlendCornerBuilder.
UseCenterPoint
¶ Returns or sets the use center point flag.
It will enable/disable the shape fullness control. When the control is enabled, the patch surface will pass through the specified center point.
-------------------------------------
Getter Method
Signature
UseCenterPoint
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseCenterPoint
Parameters: useCenterPoint (bool) – New in version NX9.0.0.
License requirements: nx_freeform_2 (“advanced freeform modeling”)
Method Detail¶
CreateBlendSetbackBuilder¶
-
BlendCornerBuilder.
CreateBlendSetbackBuilder
¶ Create a blend setback builder object.
Signature
CreateBlendSetbackBuilder()
Returns: Return type: NXOpen.GeometricUtilities.BlendSetbackBuilder
New in version NX9.0.0.
License requirements: nx_freeform_2 (“advanced freeform modeling”)
CreateTransitionCurveBuilder¶
-
BlendCornerBuilder.
CreateTransitionCurveBuilder
¶ Create a transition curve data builder object.
Signature
CreateTransitionCurveBuilder()
Returns: Return type: NXOpen.GeometricUtilities.TransitionCurveBuilder
New in version NX9.0.0.
License requirements: nx_freeform_2 (“advanced freeform modeling”)
Validate¶
-
BlendCornerBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.