AnalyzePocketBuilder Class¶
-
class
NXOpen.Features.
AnalyzePocketBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.AnalyzePocket
builder for Analyze Pocket feature.To create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateAnalyzePocketBuilder()
Default values.
Property Value AcutelyAngledWallsChecker True Diameter.Value 25.0 (millimeters part), 1.0 (inches part) FluteLength.Value 10.0 (millimeters part), 0.38 (inches part) InaccessibleAreasChecker True LowerRadius.Value 5.0 (millimeters part), 0.25 (inches part) NeckDiameter.Value 25.0 (millimeters part), 1.0 (inches part) ToolType EndMill UndercutsChecker True UpperRadius.Value 5.0 (millimeters part), 0.25 (inches part) New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
AcutelyAngledWallsChecker | Returns or sets the flag specifying whether to check acutely angled walls. |
Diameter | Returns the diameter defines the diameter of End Mill or Shperical Mill. |
FloorFaces | Returns or sets the collector of floor faces. |
FluteLength | Returns the flute length defines the length of the flute of T Cutter. |
InaccessibleAreasChecker | Returns or sets the flag specifying whether to check inaccessible areas. |
LowerRadius | Returns the lower radius defines the radius of blend on the bottom of End Mill or T Cutter. |
NeckDiameter | Returns the neck diameter defines the diameter of the neck of T Cutter. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
ToolType | Returns or sets the tool type defines how the angled walls are cut. |
UndercutsChecker | Returns or sets the flag specifying whether to check undercuts. |
UpperRadius | Returns the upper radius defines the radius of blend on the upper part of T Cutter. |
WallFaces | Returns or sets the collector of wall faces. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
AnalyzePocketBuilderAngledWallSolutions Enumeration | Represents the solution which defines how the End Mill is positioned with the angled walls. |
AnalyzePocketBuilderToolTypes Enumeration | Represents the tool type which defines how the angled walls are cut. |
Property Detail¶
AcutelyAngledWallsChecker¶
-
AnalyzePocketBuilder.
AcutelyAngledWallsChecker
¶ Returns or sets the flag specifying whether to check acutely angled walls.
If True, check the acutely angled walls, else it is not.
-------------------------------------
Getter Method
Signature
AcutelyAngledWallsChecker
Returns: Return type: bool New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
-------------------------------------
Setter Method
Signature
AcutelyAngledWallsChecker
Parameters: acutelyAngledWallsChecker (bool) – New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Diameter¶
-
AnalyzePocketBuilder.
Diameter
¶ Returns the diameter defines the diameter of End Mill or Shperical Mill.
-------------------------------------
Getter Method
Signature
Diameter
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
FloorFaces¶
-
AnalyzePocketBuilder.
FloorFaces
¶ Returns or sets the collector of floor faces.
It can be a single face, or multiple faces
-------------------------------------
Getter Method
Signature
FloorFaces
Returns: Return type: NXOpen.ScCollector
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FloorFaces
Parameters: floorFaces ( NXOpen.ScCollector
) –New in version NX9.0.0.
License requirements: None.
FluteLength¶
-
AnalyzePocketBuilder.
FluteLength
¶ Returns the flute length defines the length of the flute of T Cutter.
-------------------------------------
Getter Method
Signature
FluteLength
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
InaccessibleAreasChecker¶
-
AnalyzePocketBuilder.
InaccessibleAreasChecker
¶ Returns or sets the flag specifying whether to check inaccessible areas.
If True, check the inaccessible areas, else it is not.
-------------------------------------
Getter Method
Signature
InaccessibleAreasChecker
Returns: Return type: bool New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
-------------------------------------
Setter Method
Signature
InaccessibleAreasChecker
Parameters: inaccessibleAreasChecker (bool) – New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
LowerRadius¶
-
AnalyzePocketBuilder.
LowerRadius
¶ Returns the lower radius defines the radius of blend on the bottom of End Mill or T Cutter.
-------------------------------------
Getter Method
Signature
LowerRadius
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
NeckDiameter¶
-
AnalyzePocketBuilder.
NeckDiameter
¶ Returns the neck diameter defines the diameter of the neck of T Cutter.
-------------------------------------
Getter Method
Signature
NeckDiameter
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
ToolType¶
-
AnalyzePocketBuilder.
ToolType
¶ Returns or sets the tool type defines how the angled walls are cut.
-------------------------------------
Getter Method
Signature
ToolType
Returns: Return type: NXOpen.Features.AnalyzePocketBuilderToolTypes
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ToolType
Parameters: toolType ( NXOpen.Features.AnalyzePocketBuilderToolTypes
) –New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
UndercutsChecker¶
-
AnalyzePocketBuilder.
UndercutsChecker
¶ Returns or sets the flag specifying whether to check undercuts.
If True, check the undercuts, else it is not.
-------------------------------------
Getter Method
Signature
UndercutsChecker
Returns: Return type: bool New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
-------------------------------------
Setter Method
Signature
UndercutsChecker
Parameters: undercutsChecker (bool) – New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
UpperRadius¶
-
AnalyzePocketBuilder.
UpperRadius
¶ Returns the upper radius defines the radius of blend on the upper part of T Cutter.
-------------------------------------
Getter Method
Signature
UpperRadius
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
WallFaces¶
-
AnalyzePocketBuilder.
WallFaces
¶ Returns or sets the collector of wall faces.
It can be a single face, or multiple faces
-------------------------------------
Getter Method
Signature
WallFaces
Returns: Return type: NXOpen.ScCollector
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
WallFaces
Parameters: wallFaces ( NXOpen.ScCollector
) –New in version NX9.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
AnalyzePocketBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.