EditViewSettingsBuilder Class¶
-
class
NXOpen.Drawings.
EditViewSettingsBuilder
¶ Bases:
NXOpen.Drafting.BaseEditSettingsBuilder
Represents a
NXOpen.Drawings.EditViewSettingsBuilder
builder.It provides an interface for editing view style settings. This can be used to change one specific view or all views. To create a new instance of this class, use
NXOpen.Drafting.SettingsManager.CreateDrawingEditViewSettingsBuilder()
Default values.
Property Value ViewStyle.ViewStyleGeneral.AngleSetting.Angle.Value 0 ViewStyle.ViewStyleGeneral.AngleSetting.Associative 0 ViewStyle.ViewStyleGeneral.AngleSetting.EvaluationPlane DrawingSheet ViewStyle.ViewStyleGeneral.Scale.Denominator 1.0 ViewStyle.ViewStyleGeneral.Scale.Numerator 1.0 ViewStyle.ViewStyleGeneral.Scale.ScaleType Ratio ViewStyle.ViewStyleOrientation.HingeLine.ReverseDirection false ViewStyle.ViewStyleOrientation.HingeLine.VectorOption Inferred ViewStyle.ViewStyleOrientation.Ovt.AssociativeOrientation 0 New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
Tag | Returns the Tag for this object. |
ViewCommonViewLabel | Returns the view common view label builder |
ViewDetailLabel | Returns the view detail label builder |
ViewLabel | Returns the view label builder |
ViewProjectedLabel | Returns the view projected label builder |
ViewSectionLabel | Returns the view section label builder |
ViewStyle | Returns the view style builder |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
InheritSettingsFromCustomerDefault | Inherit Settings From Customer Default |
InheritSettingsFromPreferences | Inherit Settings From Preference |
InheritSettingsFromSelectedObjects | Inherit Settings From Selected Objects |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ViewCommonViewLabel¶
-
EditViewSettingsBuilder.
ViewCommonViewLabel
¶ Returns the view common view label builder
-------------------------------------
Getter Method
Signature
ViewCommonViewLabel
Returns: Return type: NXOpen.Drawings.ViewCommonViewLabelBuilder
New in version NX9.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Drawings.ViewStyleBuilder.ViewCommonViewLabel()
instead.License requirements: None.
ViewDetailLabel¶
-
EditViewSettingsBuilder.
ViewDetailLabel
¶ Returns the view detail label builder
-------------------------------------
Getter Method
Signature
ViewDetailLabel
Returns: Return type: NXOpen.Drawings.ViewDetailLabelBuilder
New in version NX9.0.0.
License requirements: None.
ViewLabel¶
-
EditViewSettingsBuilder.
ViewLabel
¶ Returns the view label builder
-------------------------------------
Getter Method
Signature
ViewLabel
Returns: Return type: NXOpen.Drawings.ViewLabelBuilder
New in version NX9.0.0.
License requirements: None.
ViewProjectedLabel¶
-
EditViewSettingsBuilder.
ViewProjectedLabel
¶ Returns the view projected label builder
-------------------------------------
Getter Method
Signature
ViewProjectedLabel
Returns: Return type: NXOpen.Drawings.ViewProjectedLabelBuilder
New in version NX9.0.0.
License requirements: None.
ViewSectionLabel¶
-
EditViewSettingsBuilder.
ViewSectionLabel
¶ Returns the view section label builder
-------------------------------------
Getter Method
Signature
ViewSectionLabel
Returns: Return type: NXOpen.Drawings.ViewSectionLabelBuilder
New in version NX9.0.0.
License requirements: None.
ViewStyle¶
-
EditViewSettingsBuilder.
ViewStyle
¶ Returns the view style builder
-------------------------------------
Getter Method
Signature
ViewStyle
Returns: Return type: NXOpen.Drawings.ViewStyleBuilder
New in version NX9.0.0.
License requirements: None.
Method Detail¶
InheritSettingsFromCustomerDefault¶
-
EditViewSettingsBuilder.
InheritSettingsFromCustomerDefault
¶ Inherit Settings From Customer Default
Signature
InheritSettingsFromCustomerDefault()
New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
InheritSettingsFromPreferences¶
-
EditViewSettingsBuilder.
InheritSettingsFromPreferences
¶ Inherit Settings From Preference
Signature
InheritSettingsFromPreferences()
New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
InheritSettingsFromSelectedObjects¶
-
EditViewSettingsBuilder.
InheritSettingsFromSelectedObjects
¶ Inherit Settings From Selected Objects
Signature
InheritSettingsFromSelectedObjects(selectedObject)
Parameters: selectedObject ( NXOpen.Drawings.DraftingView
) – The selected drafting view instance object. None is not allowed.New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
Validate¶
-
EditViewSettingsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.