ViewProjectedLabelBuilder Class¶
-
class
NXOpen.Drawings.
ViewProjectedLabelBuilder
¶ Bases:
NXOpen.Drawings.ViewLabelBuilder
Represents a
NXOpen.Drawings.ViewProjectedLabelBuilder
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
CustomizedViewLabel | Returns or sets the customized view label |
IncludeParentheses | Returns or sets the include parentheses |
IncludeRotationAngle | Returns or sets the include rotation angle |
IncludeRotationSymbol | Returns or sets the include rotation symbol |
LabelCharacterHeightFactor | Returns or sets the label character height factor |
LabelPosition | Returns or sets the label position |
LabelPrefix | Returns or sets the label prefix |
LetterFormat | Returns or sets the letter format |
PrefixCharacterHeightFactor | Returns or sets the prefix character height factor |
ReferenceToShow | Returns or sets the reference to show |
RotationSymbolType | Returns or sets the rotation symbol type |
ScaleCharacterHeightFactor | Returns or sets the scale character height factor |
ScalePosition | Returns or sets the scale position |
ScalePrefix | Returns or sets the scale prefix |
ShowViewLabel | Returns or sets the show view label |
ShowViewScale | Returns or sets the show view scale |
Tag | Returns the Tag for this object. |
ValueFormat | Returns or sets the value format |
ViewLabelOption | Returns or sets the view label option |
Methods¶
Method | Description |
---|---|
GetCustomizedViewLabelText | Returns the customized view label text |
SetCustomizedViewLabelText | Sets the customized view label text |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Method Detail¶
Validate¶
-
ViewProjectedLabelBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.