DrawingSheetCollection Class¶
-
class
NXOpen.Drawings.
DrawingSheetCollection
¶ Bases:
object
Represents a collection of drawing sheets.
To obtain an instance of this class, refer to
NXOpen.Part
New in version NX3.0.0.
Properties¶
Property | Description |
---|---|
CurrentDrawingSheet | Returns the currently opened drawing sheet. |
SheetTemplates | Returns the Sheet Template Manager for part |
Methods¶
Method | Description |
---|---|
DrawingSheetBuilder | Create a drawing Sheet builder |
FindObject | Finds the NXOpen.Drawings.DrawingSheet with the given identifier as recorded in a journal. |
InsertSheet | Inserts a sheet into a part. |
RefreshCurrentSheet | Refresh the current Sheet |
Property Detail¶
CurrentDrawingSheet¶
-
DrawingSheetCollection.
CurrentDrawingSheet
¶ Returns the currently opened drawing sheet.
This will return None if no drawing sheet is opened.
-------------------------------------
Getter Method
Signature
CurrentDrawingSheet
Returns: Return type: NXOpen.Drawings.DrawingSheet
New in version NX3.0.0.
License requirements: drafting (“DRAFTING”)
SheetTemplates¶
-
DrawingSheetCollection.
SheetTemplates
¶ Returns the Sheet Template Manager for part
Signature
SheetTemplates
New in version NX3.0.0.
Returns: Return type: NXOpen.Drawings.SheetTemplateManager
Method Detail¶
DrawingSheetBuilder¶
-
DrawingSheetCollection.
DrawingSheetBuilder
¶ Create a drawing Sheet builder
Signature
DrawingSheetBuilder(sheet)
Parameters: sheet ( NXOpen.Drawings.DrawingSheet
) – the drawing sheetReturns: the drawing sheet Builder with this identifier Return type: NXOpen.Drawings.DrawingSheetBuilder
New in version NX5.0.0.
Deprecated since version NX12.0.0: Use
NXOpen.Drawings.DraftingDrawingSheetCollection.CreateDraftingDrawingSheetBuilder()
instead.License requirements: drafting (“DRAFTING”)
FindObject¶
-
DrawingSheetCollection.
FindObject
¶ Finds the
NXOpen.Drawings.DrawingSheet
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Identifier of the drawing sheet you want Returns: Drawing sheet with this identifier Return type: NXOpen.Drawings.DrawingSheet
New in version NX3.0.0.
Deprecated since version NX12.0.0: Use
NXOpen.Drawings.DraftingDrawingSheetCollection.FindObject()
instead.License requirements: drafting (“DRAFTING”)
InsertSheet¶
-
DrawingSheetCollection.
InsertSheet
¶ Overloaded method InsertSheet
InsertSheet(drawingName, drawingUnits, width, height, numerator, denominator, projectionAngle)
InsertSheet(drawingName, sheetSize, numerator, denominator, projectionAngle)
-------------------------------------
Inserts a sheet into a part.
Signature
InsertSheet(drawingName, drawingUnits, width, height, numerator, denominator, projectionAngle)
Parameters: - drawingName (str) – Drawing name
- drawingUnits (
NXOpen.Drawings.DrawingSheetUnit
) – Unit of sheet size - width (float) – Width of drawing
- height (float) – Height of drawing
- numerator (float) – Numerator of the scale of drawing
- denominator (float) – Denominator of the scale of drawing
- projectionAngle (
NXOpen.Drawings.DrawingSheetProjectionAngleType
) – Projection angle
Returns: Return type: New in version NX3.0.0.
Deprecated since version NX12.0.0: Use
NXOpen.Drawings.DraftingDrawingSheetCollection.InsertSheet()
instead.License requirements: drafting (“DRAFTING”)
-------------------------------------
Inserts a sheet into a part. The drawings units will be inferred from the standard size.
Signature
InsertSheet(drawingName, sheetSize, numerator, denominator, projectionAngle)
Parameters: - drawingName (str) – Drawing name
- sheetSize (
NXOpen.Drawings.DrawingSheetStandardSheetSize
) – Sheet Size - numerator (float) – Numerator of the scale of drawing
- denominator (float) – Denominator of the scale of drawing
- projectionAngle (
NXOpen.Drawings.DrawingSheetProjectionAngleType
) – Projection angle
Returns: Return type: New in version NX3.0.0.
Deprecated since version NX12.0.0: Use
NXOpen.Drawings.DraftingDrawingSheetCollection.InsertSheet()
instead.License requirements: drafting (“DRAFTING”)
-------------------------------------