DrawingSheetUnit Enumeration

NXOpen.Drawings.DrawingSheet.Unit is an alias for NXOpen.Drawings.DrawingSheetUnit

class NXOpen.Drawings.DrawingSheetUnit

Bases: object

Specifies the units of the drawing sheet.

Enum Members

Enum Member Enum Member Description
Inches
Millimeters
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.