DrawingSheetProjectionAngleType Enumeration¶
NXOpen.Drawings.DrawingSheet.ProjectionAngleType is an alias for NXOpen.Drawings.DrawingSheetProjectionAngleType
-
class
NXOpen.Drawings.
DrawingSheetProjectionAngleType
¶ Bases:
object
Specifies the projection angle of a drawing sheet. All projected views and sections will then comply with the projection angle. Imported model views however, are not affected by projection angle.
Enum Members
Enum Member Enum Member Description FirstAngle ThirdAngle -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-