TrimTaskBuilder Class¶
-
class
NXOpen.Die.
TrimTaskBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a Trim Task feature builder.
To create a new instance of this class, use
NXOpen.Die.DieCollection.TrimTask()
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
AngleTolerance | Returns or sets the angle tolerance of the trim task |
CamDirection | Returns or sets the cam direction of the trim task |
CamType | Returns or sets the cam type of the trim task |
CreateScrap | Returns or sets the create scrap setting of the trim task. |
DistanceTolerance | Returns or sets the distance tolerance of the trim task |
EndPlane | Returns or sets the end plane of the trim task |
FinishOperation | Returns or sets the finish operation of the trim task True indicates the trim is to be a finish trim. |
LayoutFlange | Returns or sets the layout flange setting of the trim task. |
MatchCutExtensionAngle | Returns or sets the match cut extension angle dimension of the trim task |
MatchCutFirstRadius | Returns or sets the match cut first radius dimension of the trim task |
MatchCutNotchOffset | Returns or sets the match cut notch offset dimension of the trim task |
MatchCutOffsetFromPlane | Returns or sets the match cut offset from plane dimension of the trim task |
MatchCutOffsetLength | Returns or sets the match cut offset length dimension of the trim task |
MatchCutScrapCutterLength | Returns or sets the match cut scrap cutter length dimension of the trim task |
MatchCutSecondRadius | Returns or sets the match cut second radius dimension of the trim task |
MatchCutThirdRadius | Returns or sets the match cut third radius dimension of the trim task |
MatchCutType | Returns or sets the match cut type of the trim task |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
ReverseTrimSide | Returns or sets the reverse trim side setting of the trim task. |
StartPlane | Returns or sets the start plane of the trim task |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
TippedProduct | Returns or sets the tipped product of the trim task |
TrimNewDieFace | Returns or sets the trim new die face, from NX10. |
Methods¶
Method | Description |
---|---|
CheckAndMovePlanes | Move end planes if the position of Trim Task is changed. |
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetAssociativeObjects | Gets the associative objects of the trim task |
GetCameraLayerAndXmlp | Gets the camera layer settings and xmlp data |
GetCameraNames | Gets the names of the camera |
GetCameraViews | Gets the camera views of the trim task |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetDetails | Gets the detailed description of the trim task |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
GetScrapCutters | Gets the scrap cutters of the trim task |
GetTrimBounds | Gets the trim bounds of the trim task |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetAssociativeObjects | Sets the associative objects of the trim task |
SetCameraLayerAndXmlp | Sets the camera layer settings and xmlp data |
SetCameraNames | Sets the names of the camera |
SetCameraViews | Sets the camera views of the trim task |
SetDetails | Sets the detailed description of the trim task |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
SetScrapCutters | Sets the scrap cutters of the trim task |
SetTrimBounds | Sets the trim bounds of the trim task. |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
TrimTaskBuilderCamTypes Enumeration | Settings for the cam type of the trim task. |
TrimTaskBuilderMatchCutTypes Enumeration | Settings for the match cut type of the trim task. |
Property Detail¶
AngleTolerance¶
-
TrimTaskBuilder.
AngleTolerance
¶ Returns or sets the angle tolerance of the trim task
-------------------------------------
Getter Method
Signature
AngleTolerance
Returns: Return type: float New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
AngleTolerance
Parameters: angleTolerance (float) – New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
CamDirection¶
-
TrimTaskBuilder.
CamDirection
¶ Returns or sets the cam direction of the trim task
-------------------------------------
Getter Method
Signature
CamDirection
Returns: Return type: NXOpen.ILocation
New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
CamDirection
Parameters: camDirection ( NXOpen.ILocation
) –New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
CamType¶
-
TrimTaskBuilder.
CamType
¶ Returns or sets the cam type of the trim task
-------------------------------------
Getter Method
Signature
CamType
Returns: Return type: NXOpen.Die.TrimTaskBuilderCamTypes
New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
CamType
Parameters: camType ( NXOpen.Die.TrimTaskBuilderCamTypes
) –New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
CreateScrap¶
-
TrimTaskBuilder.
CreateScrap
¶ Returns or sets the create scrap setting of the trim task.
True indicates that the scrap is to be created.
-------------------------------------
Getter Method
Signature
CreateScrap
Returns: Return type: bool New in version NX7.5.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
CreateScrap
Parameters: createScrap (bool) – New in version NX7.5.0.
License requirements: die_engineering (“DIE ENGINEERING”)
DistanceTolerance¶
-
TrimTaskBuilder.
DistanceTolerance
¶ Returns or sets the distance tolerance of the trim task
-------------------------------------
Getter Method
Signature
DistanceTolerance
Returns: Return type: float New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
DistanceTolerance
Parameters: distanceTolerance (float) – New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
EndPlane¶
-
TrimTaskBuilder.
EndPlane
¶ Returns or sets the end plane of the trim task
-------------------------------------
Getter Method
Signature
EndPlane
Returns: Return type: NXOpen.ISurface
New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
EndPlane
Parameters: endPlane ( NXOpen.ISurface
) –New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
FinishOperation¶
-
TrimTaskBuilder.
FinishOperation
¶ Returns or sets the finish operation of the trim task True indicates the trim is to be a finish trim.
False indicates rough trim.
-------------------------------------
Getter Method
Signature
FinishOperation
Returns: Return type: bool New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
FinishOperation
Parameters: finishOperation (bool) – New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
LayoutFlange¶
-
TrimTaskBuilder.
LayoutFlange
¶ Returns or sets the layout flange setting of the trim task.
True indicates that the trim curve is to be laid out on the flange.
-------------------------------------
Getter Method
Signature
LayoutFlange
Returns: Return type: bool New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
LayoutFlange
Parameters: layoutFlange (bool) – New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
MatchCutExtensionAngle¶
-
TrimTaskBuilder.
MatchCutExtensionAngle
¶ Returns or sets the match cut extension angle dimension of the trim task
-------------------------------------
Getter Method
Signature
MatchCutExtensionAngle
Returns: angle of extension line from perpendicular Return type: float New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
MatchCutExtensionAngle
Parameters: extensionAngle (float) – angle of extension line from perpendicular New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
MatchCutFirstRadius¶
-
TrimTaskBuilder.
MatchCutFirstRadius
¶ Returns or sets the match cut first radius dimension of the trim task
-------------------------------------
Getter Method
Signature
MatchCutFirstRadius
Returns: first radius after notch Return type: float New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
MatchCutFirstRadius
Parameters: firstRadius (float) – first radius after notch New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
MatchCutNotchOffset¶
-
TrimTaskBuilder.
MatchCutNotchOffset
¶ Returns or sets the match cut notch offset dimension of the trim task
-------------------------------------
Getter Method
Signature
MatchCutNotchOffset
Returns: notch offset from trim line Return type: float New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
MatchCutNotchOffset
Parameters: notchOffset (float) – notch offset from trim line New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
MatchCutOffsetFromPlane¶
-
TrimTaskBuilder.
MatchCutOffsetFromPlane
¶ Returns or sets the match cut offset from plane dimension of the trim task
-------------------------------------
Getter Method
Signature
MatchCutOffsetFromPlane
Returns: offset from scrap cutter plane Return type: float New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
MatchCutOffsetFromPlane
Parameters: offsetFromPlane (float) – offset from scrap cutter plane New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
MatchCutOffsetLength¶
-
TrimTaskBuilder.
MatchCutOffsetLength
¶ Returns or sets the match cut offset length dimension of the trim task
-------------------------------------
Getter Method
Signature
MatchCutOffsetLength
Returns: length of offset piece Return type: float New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
MatchCutOffsetLength
Parameters: offsetLength (float) – length of offset piece New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
MatchCutScrapCutterLength¶
-
TrimTaskBuilder.
MatchCutScrapCutterLength
¶ Returns or sets the match cut scrap cutter length dimension of the trim task
-------------------------------------
Getter Method
Signature
MatchCutScrapCutterLength
Returns: entension line length Return type: float New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
MatchCutScrapCutterLength
Parameters: scrapCutterLength (float) – entension line length New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
MatchCutSecondRadius¶
-
TrimTaskBuilder.
MatchCutSecondRadius
¶ Returns or sets the match cut second radius dimension of the trim task
-------------------------------------
Getter Method
Signature
MatchCutSecondRadius
Returns: second radius after notch Return type: float New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
MatchCutSecondRadius
Parameters: secondRadius (float) – second radius after notch New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
MatchCutThirdRadius¶
-
TrimTaskBuilder.
MatchCutThirdRadius
¶ Returns or sets the match cut third radius dimension of the trim task
-------------------------------------
Getter Method
Signature
MatchCutThirdRadius
Returns: radius between offset piece and entension line Return type: float New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
MatchCutThirdRadius
Parameters: thirdRadius (float) – radius between offset piece and entension line New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
MatchCutType¶
-
TrimTaskBuilder.
MatchCutType
¶ Returns or sets the match cut type of the trim task
-------------------------------------
Getter Method
Signature
MatchCutType
Returns: Return type: NXOpen.Die.TrimTaskBuilderMatchCutTypes
New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
MatchCutType
Parameters: matchCutType ( NXOpen.Die.TrimTaskBuilderMatchCutTypes
) –New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
ReverseTrimSide¶
-
TrimTaskBuilder.
ReverseTrimSide
¶ Returns or sets the reverse trim side setting of the trim task.
True indicates that the trim side should be reversed.
-------------------------------------
Getter Method
Signature
ReverseTrimSide
Returns: Return type: bool New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
ReverseTrimSide
Parameters: reverse (bool) – New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
StartPlane¶
-
TrimTaskBuilder.
StartPlane
¶ Returns or sets the start plane of the trim task
-------------------------------------
Getter Method
Signature
StartPlane
Returns: Return type: NXOpen.ISurface
New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
StartPlane
Parameters: startPlane ( NXOpen.ISurface
) –New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
TippedProduct¶
-
TrimTaskBuilder.
TippedProduct
¶ Returns or sets the tipped product of the trim task
-------------------------------------
Getter Method
Signature
TippedProduct
Returns: The tip of the operation where the trim task resides. :rtype:
NXOpen.Features.Feature
New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
TippedProduct
Parameters: tippedProduct ( NXOpen.Features.Feature
) – The tip of the operation where the trim task resides.New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
TrimNewDieFace¶
-
TrimTaskBuilder.
TrimNewDieFace
¶ Returns or sets the trim new die face, from NX10.
0 new stamping output can import one new die face to die engineer process. If this trim task will trim this new die face, set newDieFace to true, or else set it to false.
-------------------------------------
Getter Method
Signature
TrimNewDieFace
Returns: if trim task performs on new die face, this will be true, or else this will be false. Return type: bool New in version NX10.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
TrimNewDieFace
Parameters: newDieFace (bool) – if set to true, trim task performs on new die face, or else it will perform on original die face. New in version NX10.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
Method Detail¶
CheckAndMovePlanes¶
-
TrimTaskBuilder.
CheckAndMovePlanes
¶ Move end planes if the position of Trim Task is changed.
Signature
CheckAndMovePlanes(origTip, targetTip, origStartPlaneTag, origEndPlaneTag)
Parameters: - origTip (
NXOpen.Features.Feature
) – Original Die Tip. - targetTip (
NXOpen.Features.Feature
) – Die Tip in the target operation. - origStartPlaneTag (
NXOpen.ISurface
) – Original start plane. - origEndPlaneTag (
NXOpen.ISurface
) – Original end plane.
Returns: a tuple
Return type: A tuple consisting of (targetStartPlaneTag, targetEndPlaneTag). targetStartPlaneTag is a
NXOpen.ISurface
. Start plane in target operation. targetEndPlaneTag is aNXOpen.ISurface
. End plane in target operation.New in version NX8.5.0.
License requirements: die_engineering (“DIE ENGINEERING”)
- origTip (
GetAssociativeObjects¶
-
TrimTaskBuilder.
GetAssociativeObjects
¶ Gets the associative objects of the trim task
Signature
GetAssociativeObjects()
Returns: Return type: list of NXOpen.DisplayableObject
New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
GetCameraLayerAndXmlp¶
-
TrimTaskBuilder.
GetCameraLayerAndXmlp
¶ Gets the camera layer settings and xmlp data
Signature
GetCameraLayerAndXmlp()
Returns: a tuple Return type: A tuple consisting of (layerSettings, xmlpData) layerSettings is a list of str. 1 layer setting string for each camera object. the string needs to be 256 characters long (one for each user layer) with either 0 for off or 1 for on. xmlpData is a list of str. xmlp data New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
GetCameraNames¶
-
TrimTaskBuilder.
GetCameraNames
¶ Gets the names of the camera
Signature
GetCameraNames()
Returns: each string contains the name of a camera object Return type: list of str New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
GetCameraViews¶
-
TrimTaskBuilder.
GetCameraViews
¶ Gets the camera views of the trim task
Signature
GetCameraViews()
Returns: Return type: list of NXOpen.View
New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
GetDetails¶
-
TrimTaskBuilder.
GetDetails
¶ Gets the detailed description of the trim task
Signature
GetDetails()
Returns: detail strings Return type: list of str New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
GetScrapCutters¶
-
TrimTaskBuilder.
GetScrapCutters
¶ Gets the scrap cutters of the trim task
Signature
GetScrapCutters()
Returns: Return type: list of NXOpen.ISurface
New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
GetTrimBounds¶
-
TrimTaskBuilder.
GetTrimBounds
¶ Gets the trim bounds of the trim task
Signature
GetTrimBounds()
Returns: a tuple Return type: A tuple consisting of (profileEntries, direction). profileEntries is a list of NXOpen.IProfile
. Profile entries that make up the boundary of the trim task direction is aNXOpen.Die.DirectionOption
. Profile directionNew in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
SetAssociativeObjects¶
-
TrimTaskBuilder.
SetAssociativeObjects
¶ Sets the associative objects of the trim task
Signature
SetAssociativeObjects(objects)
Parameters: objects (list of NXOpen.DisplayableObject
) –New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
SetCameraLayerAndXmlp¶
-
TrimTaskBuilder.
SetCameraLayerAndXmlp
¶ Sets the camera layer settings and xmlp data
Signature
SetCameraLayerAndXmlp(layerSettings, xmlpData)
Parameters: - layerSettings (list of str) – 1 layer setting string for each camera object. the string needs to be 256 characters long (one for each user layer) with either 0 for off or 1 for on.
- xmlpData (list of str) – xmlp data
New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
SetCameraNames¶
-
TrimTaskBuilder.
SetCameraNames
¶ Sets the names of the camera
Signature
SetCameraNames(strings)
Parameters: strings (list of str) – each string contains the name of a camera object New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
SetCameraViews¶
-
TrimTaskBuilder.
SetCameraViews
¶ Sets the camera views of the trim task
Signature
SetCameraViews(objects)
Parameters: objects (list of NXOpen.View
) –New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
SetDetails¶
-
TrimTaskBuilder.
SetDetails
¶ Sets the detailed description of the trim task
Signature
SetDetails(strings)
Parameters: strings (list of str) – detail strings New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
SetScrapCutters¶
-
TrimTaskBuilder.
SetScrapCutters
¶ Sets the scrap cutters of the trim task
Signature
SetScrapCutters(planes)
Parameters: planes (list of NXOpen.ISurface
) –New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
SetTrimBounds¶
-
TrimTaskBuilder.
SetTrimBounds
¶ Sets the trim bounds of the trim task.
Note -
Die.TrimTaskBuilder.TippedProduct()
needs to be called before this function.Signature
SetTrimBounds(direction, profileEntries)
Parameters: - direction (
NXOpen.Die.DirectionOption
) – Profile direction - profileEntries (list of
NXOpen.IProfile
) – Profile entries that make up the boundary of the trim task
New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
- direction (
Validate¶
-
TrimTaskBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.