RotorSectionBuilder Class¶
-
class
NXOpen.Die.
RotorSectionBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a Rotor Section sub feature.
This sub feature is created via the main feature builder.
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
BuildStatus | Returns the build status of the die rotor casting |
DesignStatus | Returns or sets the design status of the die rotor casting |
DisplayStatus | Returns or sets the display status of the die rotor casting |
MinimumCavityDepth | Returns the throat minimum cavity depth of the die rotor casting |
MinimumExtensionLength | Returns the throat minimum extension length of the die rotor casting |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetEndAttributes | Gets the end faces attributes |
GetFeature | Returns the feature currently being edited by this builder. |
GetFlangeWallAttributes | Gets the flange wall faces attributes |
GetFormingAttributes | Gets the forming faces attributes |
GetObject | Returns the object currently being edited by this builder. |
GetRotorAttributes | Gets the rotor faces attributes |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetEndAttributes | Sets the end faces attributes |
SetFlangeWallAttributes | Sets the flange wall faces attributes |
SetFormingAttributes | Sets the forming faces attributes |
SetMinimumCavityDepth | |
SetMinimumExtensionLength | |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
SetRotorAttributes | Sets the rotor faces attributes |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
BuildStatus¶
-
RotorSectionBuilder.
BuildStatus
¶ Returns the build status of the die rotor casting
-------------------------------------
Getter Method
Signature
BuildStatus
Returns: Return type: NXOpen.Die.DieBuildStatusOption
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
DesignStatus¶
-
RotorSectionBuilder.
DesignStatus
¶ Returns or sets the design status of the die rotor casting
-------------------------------------
Getter Method
Signature
DesignStatus
Returns: Return type: bool New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
DesignStatus
Parameters: designStatus (bool) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
DisplayStatus¶
-
RotorSectionBuilder.
DisplayStatus
¶ Returns or sets the display status of the die rotor casting
-------------------------------------
Getter Method
Signature
DisplayStatus
Returns: Return type: bool New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
DisplayStatus
Parameters: displayStatus (bool) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
MinimumCavityDepth¶
-
RotorSectionBuilder.
MinimumCavityDepth
¶ Returns the throat minimum cavity depth of the die rotor casting
-------------------------------------
Getter Method
Signature
MinimumCavityDepth
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
MinimumExtensionLength¶
-
RotorSectionBuilder.
MinimumExtensionLength
¶ Returns the throat minimum extension length of the die rotor casting
-------------------------------------
Getter Method
Signature
MinimumExtensionLength
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
Method Detail¶
GetEndAttributes¶
-
RotorSectionBuilder.
GetEndAttributes
¶ Gets the end faces attributes
Signature
GetEndAttributes()
Returns: a tuple Return type: A tuple consisting of (title, value, color) title is a str. title for attribute value is a str. value of attribute color is a int. color of end faces New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
GetFlangeWallAttributes¶
-
RotorSectionBuilder.
GetFlangeWallAttributes
¶ Gets the flange wall faces attributes
Signature
GetFlangeWallAttributes()
Returns: a tuple Return type: A tuple consisting of (title, value, color) title is a str. title for attribute value is a str. value of attribute color is a int. color of flange wall faces New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
GetFormingAttributes¶
-
RotorSectionBuilder.
GetFormingAttributes
¶ Gets the forming faces attributes
Signature
GetFormingAttributes()
Returns: a tuple Return type: A tuple consisting of (title, value, color) title is a str. title for attribute value is a str. value of attribute color is a int. color of forming faces New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
GetRotorAttributes¶
-
RotorSectionBuilder.
GetRotorAttributes
¶ Gets the rotor faces attributes
Signature
GetRotorAttributes()
Returns: a tuple Return type: A tuple consisting of (title, value, color) title is a str. title for attribute value is a str. value of attribute color is a int. color of rotor faces New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetEndAttributes¶
-
RotorSectionBuilder.
SetEndAttributes
¶ Sets the end faces attributes
Signature
SetEndAttributes(title, value, color)
Parameters: - title (str) – title for attribute
- value (str) – value of attribute
- color (int) – color of end faces
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetFlangeWallAttributes¶
-
RotorSectionBuilder.
SetFlangeWallAttributes
¶ Sets the flange wall faces attributes
Signature
SetFlangeWallAttributes(title, value, color)
Parameters: - title (str) – title for attribute
- value (str) – value of attribute
- color (int) – color of flange wall faces
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetFormingAttributes¶
-
RotorSectionBuilder.
SetFormingAttributes
¶ Sets the forming faces attributes
Signature
SetFormingAttributes(title, value, color)
Parameters: - title (str) – title for attribute
- value (str) – value of attribute
- color (int) – color of forming faces
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetMinimumCavityDepth¶
-
RotorSectionBuilder.
SetMinimumCavityDepth
¶ Signature
SetMinimumCavityDepth(minimumCavityDepth)
Parameters: minimumCavityDepth (str) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetMinimumExtensionLength¶
-
RotorSectionBuilder.
SetMinimumExtensionLength
¶ Signature
SetMinimumExtensionLength(minimumExtensionLength)
Parameters: minimumExtensionLength (str) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetRotorAttributes¶
-
RotorSectionBuilder.
SetRotorAttributes
¶ Sets the rotor faces attributes
Signature
SetRotorAttributes(title, value, color)
Parameters: - title (str) – title for attribute
- value (str) – value of attribute
- color (int) – color of forming faces
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
Validate¶
-
RotorSectionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.