DieBuildStatusOption Enumeration¶
-
class
NXOpen.Die.
DieBuildStatusOption
¶ Bases:
object
Settings for the build status of the die design sub features. Enum Members
Enum Member Enum Member Description Indeterminant Build status could not be determined since sub feature is not active. Unknown Build status is unknown since sub feature has not been built yet. Fail Sub feature build has failed. Valid Sub feature has built successfully. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-